- DynaGridCenter research project successfully completed with partners
- Dynamic control center indispensable to a successful energy transition
- Brings increasing grid dynamics under control and maintains grid stability
- Automated recommendations for action prevent blackouts and damage to plants
With the DynaGridCenter project, Siemens worked alongside partners in science and research to develop the next generation of grid control centers. For the first time, assistant systems visualize dynamic processes that bring the energy transition to the power grid and provide targeted recommendations for actions to optimize the grids and prevent blackouts. "In the future, we'll need control centers that can independently regulate the highly dynamic power grid with an autopilot functionality and keep it stable," said Prof. Dr. Rainer Krebs, head of the Consulting Unit for the Operation and Protection of Power Grids in the Siemens Energy Management Division. "The dynamic control center is therefore an indispensable part of a successful energy transition. It controls the increasing grid dynamics, maintains grid stability, and provides specific recommendations for action to prevent blackouts." The control center of the future will therefore become a key component of the power grid action plan that was introduced by the German federal government in August 2018.
Siemens and the company's Central Works Council have signed a reconciliation of interests based on the framework agreement reached in May. The goal is to increase the competitiveness of the Power and Gas Division (PG) and the Process Industries and Drives Division (PD). At PG alone, costs are to be reduced – as originally planned – by about €500 million worldwide, with €270 million of this amount to be saved in Germany. Around 2,900 jobs will be cut in Germany instead of the roughly 3,400 announced last November. This reduction in job cuts is due, above all, to the continuation of the location in Görlitz, Germany, and the retention of activities at the Dynamowerk, a Siemens production facility in Berlin. However, the measures are not restricted to capacity adjustments alone. Instead, they are primarily designed to achieve structural improvements and systematically sharpen the company's focus on the technologies of the future.
"The market for fossil power generation has contracted substantially. Against the backdrop of this structural change, the agreement we've reached is critical to improving our competitiveness. We now have to implement the measures quickly," said Lisa Davis, member of the Managing Board of Siemens AG.
"In the past few months, market forecasts have again worsened considerably. The job cuts agreed upon with the employee representatives are only one of the measures urgently necessary to improve our cost position. With the reconciliation of interests, we've also reached an agreement on structural changes and new opportunities for several locations," said Janina Kugel, Chief Human Resources Officer and member of the Managing Board of Siemens AG.
- Reconciliation of interests signed for Power and Gas Division and Process Industries and Drives Division in Germany
- Power and Gas to achieve cost savings of about €500 million worldwide, of which €270 million are to be saved in Germany
- Capacity and structure adjustments can now begin in Germany
Siemens and the company's Central Works Council have signed a reconciliation of interests based on the framework agreement reached in May. The goal is to increase the competitiveness of the Power and Gas Division (PG) and the Process Industries and Drives Division (PD). At PG alone, costs are to be reduced – as originally planned – by about €500 million worldwide, with €270 million of this amount to be saved in Germany. Around 2,900 jobs will be cut in Germany instead of the roughly 3,400 announced last November. This reduction in job cuts is due, above all, to the continuation of the location in Görlitz, Germany, and the retention of activities at the Dynamowerk, a Siemens production facility in Berlin. However, the measures are not restricted to capacity adjustments alone. Instead, they are primarily designed to achieve structural improvements and systematically sharpen the company's focus on the technologies of the future.
- Siemens Mobility provides intelligent road infrastructure including, Road Side Unit (RSU), communications networking and telematics for near-real-time exchange of information between vehicles and infrastructure
- Facility uses automated and connected vehicle technology to prepare for tomorrow's roads
Today, the city of Düsseldorf officially opened a cutting-edge automated and connected vehicle test track, which is a 20 km road dedicated to the advancement of connected and autonomous vehicle technology. Featuring Siemens Mobility technology, the digital test field highlights the latest intelligent traffic technologies, which is preparing the region for automated and autonomous traffic of the future.
Siemens and E.ON have reached a significant milestone in the area of 3D-printing for the energy sector. The world's first 3-D printed burner for an SGT-700 gas turbine has been in operation for one year at E.ON's combined cycle power plant in Philippsthal in the German state of Hessen and the results are impressive. The burner has been operating for over 8,000 hours with no reported issues.
- Siemens Mobility equips 30,000 freight cars with smart sensors
- Digitalization improves customer service and transport efficiency in rail logistics
DB Cargo AG, Europe's leading rail freight carrier, has commissioned Siemens Mobility to digitalize a large part of its freight car fleet. A total of 30,000 freight cars will be equipped with the CTmobile freight sensor solution. With this system, DB Cargo can directly and continuously determine the cars' location. The sensor also provides information about load conditions. The freight cars will be equipped over a period of three years. Siemens Mobility will operate the system for six years, monitoring data acquisition and data flows through its central in-house CT server. The contract includes an option to equip up to 50,000 freight cars.
Siemens showcased its comprehensive oil and gas solutions at the Turbomachinery & Pump Symposium (TPS), September 18 – 20, 2018 at the George R. Brown Convention Center in Houston, TX. Oil and gas companies have some of the most complex physical and technical operational challenges of any business on the planet. To manage risks, control costs and optimize asset performance, oil and gas operators increasingly rely on digital technologies and analytics to improve efficiencies and safety for all aspects of oil and gas production, distribution and use. Leveraging 170 years of technological and engineering expertise, with extensive experience in operational technology (OT) and information technology (IT), Siemens' suite of innovative technologies deliver cutting-edge hard and software capabilities for equipment and solutions that enhance efficiency, predictability, reliability and safety for its customers.
- New version SW 4.8 SP3 release for Sinumerik 828Dand Display Manager for Sinumerik 840D sI
- External PC remote control for 828D enables operation via external PC with Sinumerik Operate
- 828D operation simplified by multi-touch display and side screen
- Second control channel and Collision Avoidance Eco simplify handling
- New Display Manager for 840D sI enables integration of standard and machine-specific functions into user interfaces
Siemens has updated its proven Sinumerik 828D and 840D sI machine tool controls. For 828D, a software update SW 4.8 SP3 with Panel Processing Unit (PPU) 4 has now been released. Users benefit not only from exceptionally robust hardware but also improved connectivity through the ability to access central data and programs, increasing operating safety. Another feature of the update is an external PC remote control facility for the simplified connection of other authorized PCs via Virtual Private Computing (VPC). In addition, the application for MindSphere ManageMyMachines now enables connection of Sinumerik 828D controls to the cloud based open IotT operating system MindSphere. For exceptionally simple operation, Siemens offers Smart Operation, a robust multi-touch display used in conjunction with a side screen. The CNC Sinumerik 828D now also offers a second control channel for use during milling operations, making available additional integration and control possibilities for automation systems or handling robots. Another invaluable feature is the Collision Avoidance Eco, which works on the basis of protected areas and distances which can be configured by the user. There is also a new update designed to make life more convenient for users of the Sinumerik 840D sl. The new Sinumerik Operate Display Manager allows the operator to fully leverage the possibilities offered by larger widescreen monitors, as both standard and machine-specific functions can be integrated into the user interface. These innovations allow rapid and comprehensive access to all the relevant data and allow more efficient, simpler machine control, as well as speeding up and simplifying process workflows. This saves both time and costs throughout the entire milling process.
- At AMB, Siemens will be demonstrating new applications for Sinumerik Integrate
- Illustration of the whole tool cycle with Manage MyResources
- Optimize MyProgramming /NX CAM Editor revolutionizes CAM machine integration
- Consistent digitalization solutions increase efficiency, flexibility and competitiveness
Siemens is presenting two new applications for the open digitalization platform Sinumerik Integrate under the banner "Digitalization in Machine Tool Manufacturing – Implement now!" at AMB 2018. Using the Manage MyResources application, the complete tool cycle can be displayed for use in the CAD/CAM CNC chain. This provides the customer with a range of benefits including increased tool life. When combined with Manage MyResources, the user gains direct access to a set of NX CAM parameters using the second new application, Optimize MyProgramming /NX CAM Editor on Sinumerik, and can easily optimize and modify the NC programs generated there. The two new applications contribute to the highest possible level of tool availability and therefore to avoiding machine down time. Consistent digitalization solutions such as Sinumerik Integrate allow businesses in the machine tool industry to increase flexibility and production efficiency significantly, to reduce their development and launch times considerably, and thus to improve their competitiveness on the global market.
- Edge application Optimize MyMachining /Trochoidal allows real-time data processing for high availability and productivity
- Siemens Industrial Edge closes the gap between local and cloud computing in the industrial sector
- Sinumerik Edge facilitates high-frequency control data processing
As part of Siemens Industrial Edge, Siemens is launching applications for Sinumerik Edge, the machine-level platform specially designed for the machine tool industry, at AMB 2018 in Stuttgart. This is the first opportunity to see the Edge application Optimize MyMachining /Trochoidal for use in trochoidal milling.