Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release24 September 2018Siemens Mobility GmbHMunich/Düsseldorf
Siemens Mobility and the City of Düsseldorf jointly open digital automotive test track
"We are proud to be a partner with the City of Düsseldorf on this important project, which is laying the ground work for the future of road mobility in Germany. The test track is the first of its kind in Germany and our technologies will reduce traffic congestion, enhance safety and provide more availability of mass transit as we continue to move towards vehicle autonomy," said Manfred Fuhg, Head of Siemens Mobility Germany.
The project has four key Siemens Mobility components. The Road Side Units (RSU), communication units, allow for near-real-time information exchange between vehicles and infrastructure. These safety-critical network elements are installed and located at each of the four intersections with a signal. The second technology is an integrated SPAT (Signal Phase and Timing) unit, which forecasts green and red-light timing and transmits via RSU to vehicles. In addition, Siemens Mobility vehicle on-board units are used for vehicle-to-infrastructure communication. In the test field, these systems are used for public transport signal prioritization with 16 Rheinbahn buses. This Car-to-X (C2X) technology is the first of its kind in Germany. The Rheinbahn vehicles are also equipped with satellite positioning to test public transport privileges (i.e. right of way, designated lanes, etc.). When implemented in connected vehicle traffic settings, these technologies reduce traffic congestion, help improve safety and reduce environmental impact of traffic emissions.
For further information about Siemens Mobility GmbH, please see: www.siemens.com/mobility
For this press release
@SiemensMobility
Siemens Mobility is a separately managed company of Siemens AG. As a leader in transport solutions for more than 160 years, Siemens Mobility is constantly innovating its portfolio in its core areas of rolling stock, rail automation and electrification, turnkey systems, intelligent traffic systems as well as related services. With digitalization, Siemens Mobility is enabling mobility operators worldwide to make infrastructure intelligent, increase value sustainably over the entire lifecycle, enhance passenger experience and guarantee availability. In fiscal year 2017, which ended on September 30, 2017, the former Siemens Mobility Division posted revenue of €8.1billion and had around 28,400 employees worldwide. Further information is available at: www.siemens.com/mobility.