- Performance optimized, easy to use and future-proof servo drive system
- Flexible and compact – scalable depending on the application
- Easy engineering thanks to integration in TIA, integrated web server and one-button tuning function
With Sinamics S200, Siemens is launching a new servo drive system designed
for a variety of standard applications in the battery, electronics as well as other
industries. It consists of a precise servo drive, powerful servo motors and
easy-to-use cables and offers high dynamic performance. Applications that
require precision in speed and torque, such as winding and unwinding machines in
battery manufacturing and cell assembly, particularly benefit from the new
servo drive system. For this purpose, Sinamics S200 offers optimized speed
ripple, cogging torque compensation, 17/21-bit ST and 21-bit MT encoders, and
cycle-synchronous communication for optimized performance by
Profinet IRT in minimum 250us.
- New V6 software generation with new functions like a single positioner to reduce the load of the controller, and EtherNet/IP to allow third-party controllers to be connected
- Simulation via DriveSim Advanced enables virtual commissioning in advance, ensuring drive process requirements are met efficiently and cost-effectively
- New hardware architecture with functional enhancements like a second encoder interface and 3C3 (H2S and SO2) coating increases precision and robustness
Siemens is innovating the well-established Sinamics S210 servo drive system with a new hardware architecture and new V6 software generation that expand the system's range of applications. The servo drive system is especially suitable for applications with high dynamics in the power range between 50 W and 7 kW: for example, machines for packaging, pick & place applications, and digital printing.
- Siemens presents a new CNC for woodworking machines at the Ligna
- Sinumerik MC is the open CNC for customized processing machines
At the Ligna Woodworking Trade Fair 2019, Siemens is showcasing the Sinumerik MC control as a universal, open CNC system. Its optimized motion control, high-performance automation and the integrated Windows 10 operating system make it the ideal control, especially for wood, glass and stone cutting machines. With its open operating concept, the control system is also suitable for additive manufacturing, adhesive application, plate cutting, straightforward grinding, and laser or water jet cutting.
- New NCU 1740 for higher scalability of Sinumerik One
- Sinumerik Run MyRobot /Direct Control V2.0 and Run MyRobot /Direct Handling V2.0 available for Sinumerik One
- New functions for the Digital Twin in Create MyVirtual Machine and Run MyVirtual Machine
Siemens is expanding its offering for the "Digital Native" CNC Sinumerik One. Two years after its market launch, the technology company is presenting numerous innovations in hardware and software for the Sinumerik One at EMO Milano and the virtual Siemens Machine Tool Days. In this context, Siemens is demonstrating how the powerful machine tool controller can be used in a highly productive, flexible, and modular way and in the best possible way for digital transformation. In terms of hardware, the new NCU 1740 complements the existing NCU 1750 and 1760 as well as the PPU 1740, thus expanding its use in modular machines.
- Siemens supports BioNTech in converting to vaccine production at the Marburg plant
- Key parts of the new Manufacturing Execution System ready to use after only two and a half months
- Digitalization enables paperless documentation of production
The BioNTech SE biotechnology company based in Mainz has converted an existing facility in Marburg for the production of the Covid-19 vaccine in a record time with assistance from Siemens. The production plant has been producing the active substance since February and the vaccine BNT162b2 (also known as COMIRNATY®) since the end of March. BioNTech acquired a production facility for this in the fall of 2020 that was already equipped with capabilities for producing biotechnological substances. Through collaboration with Siemens and the team of experts on site in Marburg, the project timeline for converting the existing facility for the production of mRNA-vaccine was cut from around one year down to five months, whereby the implementation of key parts of the new Manufacturing Execution System (MES) was reduced to two and half months. The new system and end-to-end digitalization of production enable conversion to “paperless documentation of production”, which can immediately fulfill all documentation requirements.
- Sinumerik One is setting new standards in terms of productivity thanks to a new hardware platform and innovative technology functions
- Digital service offering supports machine users and machine manufacturers with the creation of a digital twin and with virtual commissioning
- Sinumerik One on show at EMO with more than 20 pilot customers
With the latest CNC generation, Sinumerik One, Siemens is presenting the essential component for the digital transformation of machine tools at EMO 2019. As a "digital native", the controller features versatile software for the creation of corresponding digital twins. Sinumerik One is setting new benchmarks in terms of productivity with its new hardware platform. A wide range of innovative technology functions help to improve processing speed, contour accuracy and processing quality.
- Process control system Simatic PCS neo version 4.0 ready for process plants of any size
- Extended functionalities for modular systems based on MTP standard
- New hardware platform: Siemens presents new Simatic S7-4100 controller generation and Simatic CN 4100 communication node
- Siemens presents Simatic PCS neo V4.0 together with the new hardware for the first time at the SPS trade fair from November 8 to 10, 2022 in Nuremberg
Digitalization, sustainability, shortage of skilled workers: Companies
in the process industry are currently facing major challenges. To prepare their
plants for the future, Siemens believes that operators must rely on a highly
flexible process control system. Against this backdrop, Siemens has now
launched both a new software version and new hardware components for its
Simatic PCS neo web-based process control system. With version 4.0, Simatic PCS
neo is now ready for plant capacities and large-scale projects of up to 64,000
process objects and 56 controllers – making it suitable for industrial plants
of all sizes.
- New Offering Seamlessly Combines Next-Generation Virtual Platform, Hardware Emulation, and FPGA Prototyping Technologies to Help Accelerate Verification Cycles
- Expansion of the Customer-Proven Veloce Family Sets New Standard in Hardware-assisted Verification
Siemens Digital Industries Software today unveiled its next-generation Veloce™ hardware-assisted verification system for the rapid verification of highly sophisticated, next-generation Integrated Circuit (IC) designs. This is the first complete, integrated offering that combines best-in-class virtual platform, hardware emulation, and Field Programmable Gate Array (FPGA) prototyping technologies, and paves the way to leverage the latest powerful hardware-assisted verification methodologies.
- Shorter development and commissioning times
- Software libraries enable standardization
- Commissioning tests on virtual test rack
The new Sinumerik One CNC generation is at the heart of digital transformation for machine tools. As a digital native, the controller features not only a new hardware platform, but also versatile software for the creation of a digital twin. It closes the gap between the virtual and the real world and helps to reduce development and commissioning times considerably.
- Sinumerik One Dynamics - three technology packages to increase the efficiency of CNC users when programming in the shopfloor and executing CAM-generated CNC programs
- Top Surface and Top Speed Plus for excellent motion control and perfect workpiece surfaces
With the software version NCU-SW 6.14, Siemens is launching three powerful technology packages exclusively for the CNC Sinumerik One. The Sinumerik One Dynamics packages are available in three different packages: One Dynamics Operate, One Dynamics 3-axis milling and One Dynamics 5-axis milling. The software functions contained in the technology packages support users from machine-oriented programming in the jobshop to high-performance machining of CAD-CAM-programmed workpieces with high surface quality.