Please use another Browser

It looks like you are using a browser that is not fully supported. Please note that there might be constraints on site display and usability. For the best experience we suggest that you download the newest version of a supported browser:

Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser

Continue with the current browser

Sinumerik One in the TIA Portal 

The central element for engineering the Sinumerik One is the TIA Portal. Both PLC (Programmable Logic Controller) and Safety are engineered in this engineering framework.

Sinumerik One as part of the engineering framework

The central element for engineering the Sinumerik One is the TIA Portal. Both PLC (Programmable Logic Controller) and Safety are engineered in this engineering framework with modern programming languages and a seamless data flow. The integration of Sinumerik One into the TIA Portal enables a consistent digital development process for machine tools, which makes all engineering tasks easier. With the integrated Simatic S7-1500F, machine manufacturers can make full use of the advantages of the TIA Portal with Sinumerik One. Uniform, centralized data handling enables efficient engineering and considerably reduces the potential for errors caused by inconsistent data. Drag and drop is used to network peripherals easily and to establish communication links with other machine components. In addition, machine manufacturers can create software libraries with ready-made hardware configurations and numerous function and software modules in the TIA Portal, thus standardizing the development of the machine tool.
Sinumerik One is based on Safety Integrated as the Siemens industry standard in the field of safety. The controller also supports the safety functions integrated in the drive. In addition, thanks to the integration of the Simatic S7 1500F PLC for implementation of the safety logic, only one failsafe program is required. This simplifies safety engineering and reduces safety commissioning time.

The digital twin as virtual test rack

With Create MyVirtualMachine software, machine manufacturers can use a digital twin of the controller and utilize it as a virtual test rack. In this way, engineering and software modules can be tested comprehensively without the use of hardware. Programming tasks which previously had to be performed successively can now be completed in parallel. This creates flexibility and reduces dependencies. Using the virtual image of the controller, logic functions in the safety environment can be virtually tested and commissioned in advance. Virtual commissioning with the digital twin helps to minimize commissioning time in the real world. Run MyVirtualMachine software also offers the machine user the option of using a digital twin to transfer tasks such as running in products and training employees into the virtual world.
Additional information about Sinumerik One can be found at
www.siemens.com/sinumerik-one
Additional information about TIA Portal can be found at
www.siemens.com/tia-portal
Siemens Digital Industries (DI) is an innovation leader in automation and digitalization. Closely collaborating with partners and customers, DI drives the digital transformation in the process and discrete industries. With its Digital Enterprise portfolio, DI provides companies of all sizes with an end-to-end set of products, solutions and services to integrate and digitalize the entire value chain. Optimized for the specific needs of each industry, DI’s unique portfolio supports customers to achieve greater productivity and flexibility. DI is constantly adding innovations to its portfolio to integrate cutting-edge future technologies. Siemens Digital Industries has its global headquarters in Nuremberg, Germany, and has around 76,000 employees internationally.
Read more
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 170 years. The company is active around the globe, focusing on the areas of power generation and distribution, intelligent infrastructure for buildings and distributed energy systems, and automation and digitalization in the process and manufacturing industries. Through the separately managed company Siemens Mobility, a leading supplier of smart mobility solutions for rail and road transport, Siemens is shaping the world market for passenger and freight services. Due to its majority stakes in the publicly listed companies Siemens Healthineers AG and Siemens Gamesa Renewable Energy, Siemens is also a world-leading supplier of medical technology and digital healthcare services as well as environmentally friendly solutions for onshore and offshore wind power generation. In fiscal 2019, which ended on September 30, 2019, Siemens generated revenue of €86.8 billion and net income of €5.6 billion. At the end of September 2019, the company had around 385,000 employees worldwide. Further information is available on the Internet at www.siemens.com .
Read more
Reference Number: PR201912135735en

Contact

Thomas Kießling

Digital Industries

+49 172 1564256