[{"name":"Home","site_name":"Press | Company | Siemens","description":"","url_str":"\/global\/","level":0,"image":"","base_root":"https:\/\/press.siemens.com","base_nid":"5","base_nodepath":"\/node\/5","base_path":"\/global\/","base_secure_url":"https:\/\/press.siemens.com\/global","children":null}]
[]
Please use another Browser
It looks like you are using a browser that is not fully supported. Please note that there might be constraints on site display and
usability.
For the best experience we suggest that you download the newest version of a supported browser:
Press Release27 October 2022Digital IndustriesNuremberg
Milestone
for the process industry: new version of the web-based Simatic PCS neo control
system available
Process control system Simatic PCS neo version 4.0 ready for process plants of any size
Extended functionalities for modular systems based on MTP standard
New hardware platform: Siemens presents new Simatic S7-4100 controller generation and Simatic CN 4100 communication node
Siemens presents Simatic PCS neo V4.0 together with the new hardware for the first time at the SPS trade fair from November 8 to 10, 2022 in Nuremberg
Digitalization, sustainability, shortage of skilled workers: Companies
in the process industry are currently facing major challenges. To prepare their
plants for the future, Siemens believes that operators must rely on a highly
flexible process control system. Against this backdrop, Siemens has now
launched both a new software version and new hardware components for its
Simatic PCS neo web-based process control system. With version 4.0, Simatic PCS
neo is now ready for plant capacities and large-scale projects of up to 64,000
process objects and 56 controllers – making it suitable for industrial plants
of all sizes.
Process control system Simatic PCS neo version 4.0 ready for process plants of any size
Extended functionalities for modular systems based on MTP standard
New hardware platform: Siemens presents new Simatic S7-4100 controller generation and Simatic CN 4100 communication node
Siemens presents Simatic PCS neo V4.0 together with the new hardware for the first time at the SPS trade fair from November 8 to 10, 2022 in Nuremberg
Digitalization, sustainability, shortage of skilled workers: Companies
in the process industry are currently facing major challenges. To prepare their
plants for the future, Siemens believes that operators must rely on a highly
flexible process control system. Against this backdrop, Siemens has now
launched both a new software version and new hardware components for its
Simatic PCS neo web-based process control system. With version 4.0, Simatic PCS
neo is now ready for plant capacities and large-scale projects of up to 64,000
process objects and 56 controllers – making it suitable for industrial plants
of all sizes.
Simatic PCS neo V4.0: Completely web-based process control system
"Whether
individual process modules or world-scale plants – Simatic PCS neo is the
control system of the future for the process industry," says Dr. Hartmut
Klocker, Vice President Automation and Engineering Systems at Siemens Process
Automation. "As the world's first and only completely web-based system,
the process control system enables location-independent teamwork – whether from
the home office or the office, on mobile devices or desktop computers. This is
a real milestone."
In version
4.0, Simatic PCS neo supports all parts of the MTP standard (Module Type
Package) defined and released jointly by NAMUR and ZVEI up to now. Plant
modules can thus be integrated even more easily into the process control system
and can be described, configured, and automated independently of the
manufacturer. In addition, version 4.0 offers workflow improvements that
further reduce the engineering effort. "With Simatic PCS neo, plant
operators are also pioneers in the MTP standard. Process plants can thus be
controlled even more efficiently than before," says Klocker.
New controller generation available
With the
Simatic S7-4100 automation system, Siemens is also presenting the new
generation of controllers for the process industry. The first release will be
available exclusively for Simatic PCS neo. Compared to the current model, which
will continue to be available in the long term, the new controller is 30 percent
smaller and thus saves space in the control cabinet. In addition, Simatic
S7-4100 offers extended communication options with up to six Profinet or
Profibus interfaces. The use of the latest Siemens chipsets reduces the energy
consumption of these controllers by up to 50 percent. In addition, the S7-4100
controller is absolutely robust and maintenance-free: When operating at ambient
temperatures of minus 25 to plus 70 degrees Celsius, no fan is necessary, and
no batteries are required to buffer the system data in the event of a power
failure. Klocker: "The controller is the brain of the process plant. With
the Simatic S7-4100 controller, we have taken our automation platform for the
process industry to a completely new level of performance."
Simatic S7-4100: New
generation of controllers for process automation
Simatic CN 4100 communication gateway for
maximum connectivity
Parallel to
Simatic PCS neo V4.0, Siemens is introducing the fully integrated Simatic CN
4100 communication gateway, which enables simple and secure process data
exchange with Simatic PCS neo both at the control level and in parallel at the
visualization level. It plays the role of a convenient data switch, which makes
it possible to configure data from the plant only once and then feed it to the
controller, the process control system, or both at the same time. Supported
protocols include Modbus TCP and OPC UA, and more protocols are planned. This
relieves process control, simplifies engineering, and increases plant security
by separating the networks.
Siemens will
be presenting Simatic PCS neo V4.0 together with the new hardware for the first
time at this year's SPS trade fair from November 8 to 10, 2022 in Nuremberg
(Hall 11).
Siemens Digital Industries (DI) is an innovation leader in automation and digitalization. Closely collaborating with partners and customers, DI drives the digital transformation in the process and discrete industries. With its Digital Enterprise portfolio, DI provides companies of all sizes with an end-to-end set of products, solutions and services to integrate and digitalize the entire value chain. Optimized for the specific needs of each industry, DI’s unique portfolio supports customers to achieve greater productivity and flexibility. DI is constantly adding innovations to its portfolio to integrate cutting-edge future technologies. Siemens Digital Industries has its global headquarters in Nuremberg, Germany, and has around 72,000 employees internationally.
Siemens AG (Berlin and Munich) is a technology company focused on industry, infrastructure, transport, and healthcare. From more resource-efficient factories, resilient supply chains, and smarter buildings and grids, to cleaner and more comfortable transportation as well as advanced healthcare, the company creates technology with purpose adding real value for customers. By combining the real and the digital worlds, Siemens empowers its customers to transform their industries and markets, helping them to transform the everyday for billions of people. Siemens also owns a majority stake in the publicly listed company Siemens Healthineers, a globally leading medical technology provider shaping the future of healthcare. In addition, Siemens holds a minority stake in Siemens Energy, a global leader in the transmission and generation of electrical power.
In fiscal 2021, which ended on September 30, 2021, the Siemens Group generated revenue of €62.3 billion and net income of €6.7 billion. As of September 30, 2021, the company had around 303,000 employees worldwide. Further information is available on the Internet at
www.siemens.com on the Internet.