Siemens AG is preparing to list its separately managed healthcare unit on the Prime Standard segment of the Frankfurt Stock Exchange's Regulated Market. This move, which the company's Supervisory Board approved at its meeting today, is planned for the first half of 2018. "For Siemens Healthineers, the public listing is the next logical step and the foundation for expanding our strong position as a leading global supplier of healthcare technology," said Michael Sen, Chairman of the Siemens Healthineers Supervisory Board and the member of Siemens' Managing Board responsible, among other things, for healthcare technology.
- Stand-alone Safety Instrumented System for use in critical areas in process industries
- Customized solution for functional safety for small to medium-sized plant projects
- Pre-configured packages based on proven Simatic components
- Connection to any process control system via Modbus/TCP
The Simatic SIS compact system from Siemens offers a new, stand-alone and flexible Safety Instrumented System for use in critical areas in the process industry. The combination of hardware and software components provides safety functions based on proven automation technology. The Simatic SIS compact system allows easy design of dedicated safety systems, the so called Safety Instrumented Systems (SIS), for monitoring potentially hazardous processes in the process industry and for protecting people, the environment, and the process plant. SIS monitor these processes and automatically intervene as soon as a permissible operating range is exceeded, such as too high pressure or temperature; alternatively, they can notify operating personnel to intervene. This minimizes the risk of potentially hazardous conditions.
Digitalization is changing our world – and the world of industry – in tangible ways. The digital transformation is creating new competitive advantages and business models in many companies in the manufacturing and process industry. Machine builders and plant engineers can also take advantage of this development and make it usable for their customers. For digital enterprises systems and processes can be comprehensively and uniformly optimized throughout the entire lifecycle of products and plants. At the SPS IPC Drives in Nuremberg, Germany, from November 28 to 30, 2017 – which took place this year under the motto "Discover the value of the Digital Enterprise" – Siemens presented in hall 11 specific examples of applications to show how this can be done.
- Faster processor and more memory space for complex applications
- Increased connectivity
- Efficient refrigeration control with inbuilt electronic expansion valves drivers
With the new Climatix C600 models the Siemens Building Technologies Division is extending its range of controllers for heating, ventilation and air conditioning (HVAC). These are designed for complex applications comprising up to 8,000 objects, for example a ventilation with integrated chiller unit. The new model series includes easy cloud connection for digitalized services for applications like chillers, heat pumps, district heating stations, air handling units and roof top units. Original equipment manufacturers (OEMs) are thereby enabled to develop new business fields or to increase service efficiency.
- New MindSphere Version 3.0 on Amazon Web Services (AWS) provides access to Siemens APIs and AWS cloud services for faster development
- Simotics IQ: New IoT concept for motors
- New partnership financing service to boost the implementation of Industrie 4.0
- Study affirms annual productivity increase due to digitalization of up to 9.8 percent
Increasing demands by consumers for individual, high-quality products at favorable prices are posing new challenges for industrial enterprises which can only be resolved by digitalization. "With the Digital Enterprise portfolio, the technical conditions have been created for Industrie 4.0. To ensure successful implementation of Industrie 4.0, what we now need is an extended model for cooperative partnership based on mutual respect: Large-scale corporations supply platforms and components, medium-sized enterprises develop their own solutions and business models on this basis, and end customers integrate these into their digital value chain," explained Klaus Helmrich, Member of the Managing Board of Siemens AG at the SPS IPC Drives. Siemens will be showcasing a range of innovations at the show designed to shorten the time to market and to improve flexibility, efficiency and quality in the process and manufacturing industries. They range from the new Version 15 of the Engineering Framework TIA Portal through the IoT concept for motors Simotics IQ to the new Version 3.0 of the open cloud-based IoT operating system MindSphere. Siemens is also offering financing services such as pay-per-use models designed to simplify the implementation of digital solutions, aimed in particular at medium-sized enterprises.
San Francisco is considered an especially environmentally friendly city. The urban environment is characterized by an extensive public transport system. In September 2014, San Francisco's Municipal Transportation Agency (SFMTA) has awarded Siemens a contract to deliver an initial 175 light rail cars at a value of USD648 million. The order included an option for additional 85 cars. One year later, SFMTA exercised its option for another 40 light rail vehicles for the public mass transit network. This is one of the biggest orders for light rail cars ever placed in the USA. The trains are being built in the Siemens plant in Sacramento. Today, every third tram or light rail vehicle in the USA is made by Siemens.
- Real-time transmission over Profinet and Pulse Train
- Absolute single-turn encoder with resolution of up to 21 bits for greater efficiency
- New motor design for better connectivity
The user-friendly servo drive system Sinamics V90 from Siemens is particularly suited as a solution for highly dynamic applications. The system comes not only in the form of a high-inertia variant with 400 volts (V) for applications requiring smooth operation, but also as a 200 V version with low inertia motors where highly dynamic performance is called for. Fitted with either Pulse Train (PTI) or Profinet, the motion/process data and diagnostic data can be transmitted in real time between Sinamics V90 and Simatic PLCs. The low inertia motor now features an additional absolute single-turn encoder with a resolution of up to 21 bits, allowing it to determine unequivocal position values and so ensure the great positioning accuracy in the applications.
- Sinamics G120 converter series in new frame size FSG
- Extended push-through heat sink variants for Power Module PM240-2
- Intelligent Operator Panel IOP-2 for Sinamics G series with added functions
Siemens is extending its portfolio of Sinamics G120 converters to include a new frame size, the FSG with voltage ranges from 380 to 480 volts (V) and from 500 to 690 V. This addition means that the innovative PM240-2 Power Modules now cover the entire power range up to 250 kilowatts (kW). The extremely compact design and standard integrated optional features such as integrated DC link reactor or integrated filter to achieve category C2, enable substantial space and cost savings in the control cabinet. The new frame size also allows cable lengths of up to 450 meters to be achieved without the need for additional options. Depending on the application, the Power Module can be configured individually to customer requirements using the correct control unit and matching components.
Siemens has developed new base holders for Neozed fuses in one-pole and three-pole designs and sizes D01 and D02. Made of heat-resistant plastic, the new bases replace the existing Siemens devices. Eight new variants for 16 A and 63 A rated currents were developed. The compact devices are especially safe to use and, thanks to new terminals, can be easily mounted in distribution boards. For the first time, the devices are available with LED indicators that clearly show whether the fuse has been tripped due to an overload or short circuit and must be replaced.