Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release27 November 2017Digital Factory Nuremberg
Sinamics V90 drive with Simotics S-1FL6 21-bit encoder version and new motor design

The presence of the additional absolute single turn encoder eliminates the need for advance referencing, as the values are available immediately after system start. The position tracking function allows you to generate a virtual multi turn encoder value from a single-turn encode and the position value to be stored in the drive. All of this takes place in running operation. It accelerates set-up times and reduces the time required for start-up after a machine stop. The Sinamics V90 is available in eight sizes and the SimoticsS-1FL6 in seven motor shaft heights, and covers the output range from 0.05 to 7.0 kilowatts for operation with single and three-phase supplies. Furthermore the design of the Simotics S-1FL6 high-inertia motor has been updated. The connections on the motor side are now angled, and connections on the cable side are standard connections. This makes the design of the motor more compact and the connectivity more convenient.
It is particularly suited for motion control applications such as positioning and winding.
For further information on the subject of Sinamics V90 please see www.siemens.com/sinamics-v90
Further information about Siemens at the SPS IPC Drives 2017 at www.siemens.com/sps-ipc-drives and www.siemens.com/press/sps2017
Siemens AG (Berlin and Munich) (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for 170 years. The company is active around the globe, focusing on the areas of electrification, automation and digitalization. One of the world's largest producers of energy-efficient, resource-saving technologies, Siemens is a leading supplier of efficient power generation and power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. The company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2017, which ended on September 30, 2017, Siemens generated revenue of €83.0 billion and net income of €6.2 billion. At the end of September 2017, the company had around 372,000 employees worldwide. Further information is available on the Internet at www.siemens.com.
Reference Number: PR2017110044DFEN
Contact
Katharina Lamsa
Siemens AG
Gleiwitzer Str. 555
90475 Nuremberg
Germany
90475 Nuremberg
Germany
+49 (911) 895-7975