- Optional I/O module for Sinamics V20 converters
- Sinamics V20 I/O module in Plug&Play design for greater flexibility
- Front and rear ports offer compatibility with additional components
For the smallest converter in its portfolio, the Sinamics V20, Siemens is now offering an extension module for the capture and output of digital and analog signals. The Sinamics V20 I/O extension module is mounted on the converter using Plug&Play technology, and provides two additional input and output interfaces, each for 400 volts., increasing both the flexibility and the scope of the Sinamics V20. Using connecting ports on the front and back, the extension module can also be combined with additional accessories from the Sinamics V20 portfolio. These include for instance the BOP (Basic Operator Panel) and the BOP interface module.
- Guided acceptance test for safety functions in the Sinamics Startdrive engineering tool
- Extremely user-friendly thanks to acceptance wizard
- Automatically generated and standard-compliant acceptance report supports documentation
With Sinamics Startdrive commissioning software, Siemens supports machine builders in the validation of safety functions for Sinamics frequency converters with a guided acceptance test. With Sinamics Startdrive, Siemens offers a tool for the integration of drive hardware into the TIA Portal engineering framework. The integrated guided acceptance test for safety functions is available for Sinamics G and S series frequency converters and complies with EN ISO 13849-2 and IEC 62061.
- Sinamics Startdrive V16 brings a single-axis version of Sinamics S120 to the TIA Portal.
- Innovative functions simplify safety approval, reduce commissioning times and increase user-friendliness.
Sinamics Startdrive commissioning software is the perfect tool for integrating drive hardware into the TIA Portal engineering framework. With the latest version Sinamics Startdrive V16, Siemens is expanding the hardware portfolio available on the automation platform. Following on from the integration of the Sinamics S120 multi-axis system, the single-axis version of this high-end servo drive system can now also be engineered in the TIA Portal. The drive control of the recently introduced Simatic Drive Controller is now also integrated in the commissioning tool. Drive-CliQ hubs, which increase the number of interfaces in the Sinamics S120 multi-axis group, as well as other add-on components, are now integrated in the TIA Portal, perfectly completing this hardware update.
- Smart connection panel with LAN link for cloud-based digitalization solutions
- Simple plug-and-play handling, also for use in legacy systems
- Analyze MyDrives now available on the latest MindSphere version
The new Sinamics Connect 300 from Siemens provides a simple plug-and-play solution for integrating converters of the Sinamics family into the IT world. The new solution is suitable for low-voltage converters and supports cloud-based digitalization solutions. MindSphere applications such as Analyze MyDrives can now be used directly via Sinamics Connect 300. Sinamics Connect 300 is an IoT gateway with its own dedicated LAN connection. The converter is connected directly to the Sinamics Connect 300 terminal block. Parameters, operating data and statuses are being transmitted over universal serial interface protocol and can be retrieved at any time. No modifications are necessary to the hardware or firmware of drives used with Sinamics Connect 300, nor do PLC programs need to be adjusted. Commissioning takes place conveniently and simply using a web server user interface. Sinamics Connect 300 does not bring about any changes to the data and signal flow of the machine automation, nor does it place any additional load on the field bus of the machine or plant. This makes the use of Sinamics Connect 300 completely independent of the automation and enables rapid, trouble-free and low-cost commissioning. The simultaneous connection of up to eight drives opens up outstanding economies of scale, and the Sinamics Connect 300 is also highly suited for machine users looking to directly upgrade heterogeneous legacy machine fleets in brown field projects.
- Bipole III is a 2,000 MW HVDC project enabling transmission of renewable energy via almost 1,400 kilometers
- Close collaboration enabled on time delivery of a highly complex project in a challenging environment
- The project significantly strengthens the reliability of Manitoba's electricity supply
The consortium of Siemens and Mortenson has successfully completed the ± 500-kilovolt (kV) Bipole III high-voltage direct-current (HVDC) power converter stations for customer Manitoba Hydro. The HVDC converter stations are an integral part of the Manitoba Hydro Bipole III transmission project. The entire transmission line will act as an "electricity highway", bolstering the reliability of Manitoba's electricity supply by reducing dependence on existing HVDC transmission lines, while also ensuring low-loss transport of renewable hydropower from northern generating stations to meet growing energy requirements. HVDC converter stations are specialized substations that support the conversion of electric power from high-voltage alternating-current (HVAC) to high-voltage direct-current (HVDC), or vice versa, a critical component to interconnecting separate power systems.
- New firmware V5.2 for even easier operation of Sinamics S120 drive systems
- Integration of the web server with new, responsive design and no special commissioning tools for diagnostics, maintenance and servicing
- Parallel connection of Active Line Modules (ALM) provides an extended performance range for booksize versions
- Users benefit from increased rated power without additional chassis unit and energy exchange in the DC link
Siemens offers new features in the firmware and hardware for the Sinamics S120 drive system. Operation is made much easier in firmware V5.2 through the integration of the web server. The web server in version V5.2 has a new, responsive design, which reacts via standard web browsers regardless of the end device used (notebook, PC, tablet or smartphone). For commissioning typical diagnostics and maintenance functions or servicing, no special tools are required. The web pages are available in six standard languages and feature error indicators and warning messages including meaningful help texts and suggestions for possible solutions. Users can intuitively create, manage and delete parameter lists - even across axes - and can perform firmware updates and system restores with the old firmware version. Backups of parameter settings can be stored on the clients using the web server and browser, and reloaded in the Sinamics converter using the Restore function. In order to test functions that are subject to license, it is possible to activate a temporary trial mode. In addition, a complete overview of all functions that are subject to license is clearly displayed in the web server. For optimum display on any Internet-capable end device, the best browsers are Microsoft Edge, Mozilla Firefox, Google Chrome and Safari. Navigation is via menu or breadcrumbs.
At SPS 2019, Siemens presents its latest solutions
for smart and networked drive technology. By networking entire drive systems, machine
and plant builders as well as users can simulate machines and plant more
accurately using digital twins, perform commissioning, reduce downtimes and therefore
increase productivity.
- First new frame size in 0.4 to one kilowatt output range
- New shared DC link coupling reduces waste heat during braking and increases traversing cycle of individual axes
- Higher-level control now possible with Simatic ET 200SP CPUs and Open Controllers or Simatic S7-1500 Software Controllers
- Engineering and commissioning using Sizer and Start Drive, engineering in TIA Portal V15.1
Siemens is extending its Sinamics S210 single-axis servo drive system for mid-range applications to include a number of additional output and connected voltage variants. In the first of the new frame sizes, the system is available with an output of 0.4 to one kilowatt with 3 AC 400 volts. The new Sinamics S210 device variants come with an optional busbar trunking system and a shared DC link coupling to enable their international application. The DC link coupling permits energy equalization during dynamic reversing operations by using the integrated braking resistor to reduce waste heat occurring during braking and increasing the traversing cycle of the individual axes. Alongside S7-1500 Advanced Controllers, higher-level control of the new devices is also possible using Simatic ET 200SP CPUs (Central Processing Units) and Open Controllers or Simatic S7-1500 Software Controllers, all of which are connected over time-synchronized Profinet IRT. The drive system can be simply engineered and commissioned using the integrated web server. Alternatively, engineering can now also be performed using Startdrive in the TIA (Totally Integrated Automation) Portal from Version V15.1.
- Sinamics G120 Smart Access Module for wireless commissioning of Sinamics G120 converter series
- Wireless commissioning, diagnostics and servicing using mobile devices
- Rapid installation with no need to download additional software
- Intuitive user interface and menu guidance simplify handling
Siemens has extended its Sinamics G120 converter series portfolio to include an option for wireless commissioning, diagnostics and servicing. The new Sinamics G120 Smart Access Module enables the wireless connection of mobile devices such as tablets, smartphones or laptops over WiFi to the Sinamics G120, Sinamics G120C and Sinamics G120P converter series, making for considerably simpler converter handling. The module is set up in a few simple steps using a conventional web browser and any standard operating system. The web server functionality eliminates the need to download any additional software. With its intuitively structured user interface and menu guidance, the module offers outstanding user convenience.
- Sinamics G120 converter series in new frame size FSG
- Extended push-through heat sink variants for Power Module PM240-2
- Intelligent Operator Panel IOP-2 for Sinamics G series with added functions
Siemens is extending its portfolio of Sinamics G120 converters to include a new frame size, the FSG with voltage ranges from 380 to 480 volts (V) and from 500 to 690 V. This addition means that the innovative PM240-2 Power Modules now cover the entire power range up to 250 kilowatts (kW). The extremely compact design and standard integrated optional features such as integrated DC link reactor or integrated filter to achieve category C2, enable substantial space and cost savings in the control cabinet. The new frame size also allows cable lengths of up to 450 meters to be achieved without the need for additional options. Depending on the application, the Power Module can be configured individually to customer requirements using the correct control unit and matching components.