Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release20 November 2018Digital Factory Nuremberg
Extended output and connected voltage variants for Sinamics S210

Extended output and connected voltage variants for Sinamics S210
The output spectrum of the Sinamics S210 devices is due to be supplemented by a number of new variants covering a range from 0.4 to seven kilowatts, alongside the matching Simotics S-1FK2 servomotors with shaft heights up to 100 millimeters. With an optional license, additional safety functions can be activated to supplement the standard safety package. Introduction of the new safety functions increases the resolution of the encoders installed in the Simotics motors to 22 bits. Depending on requirements, the servomotors come in a compact or highly dynamic version. In conjunction with the rapid sampling and control algorithms of the Sinamics S210, a high-grade feedback system and the combination of low rotor inertia and high overload capability, the servo motors achieve outstanding dynamic performance and precision. This makes them particularly suited to use in applications such as packaging machinery, handling, wood and ceramic processing as well as digital printing.
Siemens is extending its Sinamics S210 single-axis servo drive system for mid-range applications to include a number of additional output and connected voltage variants. In the first of the new frame sizes, the system is available with an output of 0.4 to one kilowatt with 3 AC 400 volts.
Siemens is extending its Sinamics S210 single-axis servo drive system for mid-range applications to include a number of additional output and connected voltage variants. In the first of the new frame sizes, the system is available with an output of 0.4 to one kilowatt with 3 AC 400 volts.
Additional information on the subject of Sinamics S210 is available at www.siemens.com/sinamics-S210
For this press release
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 170 years. The company is active around the globe, focusing on the areas of electrification, automation and digitalization. One of the largest producers of energy-efficient, resource-saving technologies, Siemens is a leading supplier of efficient power generation and power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. With its publicly listed subsidiary Siemens Healthineers AG, the company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2018, which ended on September 30, 2018, Siemens generated revenue of €83.0 billion and net income of €6.1 billion. At the end of September 2018, the company had around 379,000 employees worldwide. Further information is available on the Internet at www.siemens.com.
Reference Number: PR2018110038DFEN
Contact
Katharina Lamsa
Siemens AG
Gleiwitzer Str. 555
90475 Nuremberg
Germany
90475 Nuremberg
Germany
+49 (911) 895-7975