Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release14 March 2019,
updated19 March 2019Digital Factory Nuremberg
Sinamics S120 drive system - firmware and hardware updates increase user-friendliness
The picture shows the Sinamics S120 drive system.
By connecting the Sinamics S120 Active Line Modules (ALM) in parallel, the operator can now use the Booksize format continuously up to a rated power of 228kW. The parallel connection of the 55kW ALM also enables a higher peak power for high dynamic machines than a single 120kW ALM. The space-saving internal busbar can be used by suitable arrangement of the dc link components. 55, 80 and 120 kilowatts (kW) of ALM can be connected in two parallel circuits. This feature is supported by the new firmware version V5.2.
For further information regarding the Sinamics S120, please see www.siemens.com/sinamics
For further information on Siemens at the Hannover Messe 2019, please see www.siemens.com/press/hm19 and www.siemens.com/hannovermesse
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 170 years. The company is active around the globe, focusing on the areas of electrification, automation and digitalization. One of the largest producers of energy-efficient, resource-saving technologies, Siemens is a leading supplier of efficient power generation and power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. With its publicly listed subsidiary Siemens Healthineers AG, the company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2018, which ended on September 30, 2018, Siemens generated revenue of €83.0 billion and net income of €6.1 billion. At the end of September 2018, the company had around 379,000 employees worldwide. Further information is available on the Internet at www.siemens.com.
Contact
Katharina Lamsa
Siemens AG
Gleiwitzer Str. 555
90475 Nuremberg
Germany
90475 Nuremberg
Germany
+49 (911) 895-7975