Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release26 October 2017Digital Factory Nuremberg
I/O extension module for Sinamics V20 increases converter scope

The new module lends the Sinamics V20 converter additional functionalities such as the ability to control up to four pumps using only a single drive. It also allows the converter to be used for even more applications. Typical fields of application for the converter in combination with the I/O module include pump, fan and compressor applications and any applications involving additional input and output ports with an output of 0.12 to 30 kilowatts. The Sinamics V20 is a basic converter from the Siemens portfolio characterized in particular by its short commissioning times, simple handling, robust design and cost efficiency. The converter is available in seven different sizes.
For further information on the subject of Sinamics V20 please see www.siemens.com/sinamicsV20
For further information on Siemens at the SPS IPC Drives 2017 please see www.siemens.com/sps-ipc-drives and www.siemens.com/press/sps2017
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for 170 years. The company is active in more than 200 countries, focusing on the areas of electrification, automation and digitalization. One of the world's largest producers of energy-efficient, resource-saving technologies, Siemens is a leading supplier of efficient power generation and power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. The company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2016, which ended on September 30, 2016, Siemens generated revenue of €79.6 billion and net income of €5.6 billion. At the end of September 2016, the company had around 351,000 employees worldwide. Further information is available on the Internet at www.siemens.com.
Reference Number: PR2017100041DFEN
Contact
Katharina Lamsa
Siemens AG
Gleiwitzer Str. 555
90475 Nuremberg
Germany
90475 Nuremberg
Germany
+49 (911) 895-7975