Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release25 November 2019Digital IndustriesNuremberg
Analyze MyDrives V1.0 available as standard in MindSphere Store and Sinamics Connect 300 with new intelligent features
Analyze MyDrives V1.0
With
the new version V1.0 of the Analyze MyDrives MindSphere app, Siemens is providing
this proven app as standard in the MindSphere Store. The new version offers
users new powerful diagram libraries for faster visualization. The new “Pan
& Scan” function enables users to specify a precise time frame for
monitoring. The new version also features an improved e-mail notification
service, which is based on a simple IFTTT control mechanism. In addition, users
can freely configure trend analytics, for example for time series and scatter diagrams
to support even more powerful bivariate graphical correlation analysis. A new dashboard
provides the key status information for all relevant drive components at a
glance. If necessary, users have an overview of the integrated variables per
drive train component, including the last transmitted value, time of last
update, unit of measurement and link to the diagram used. Diagrams can be
exported with a single click. Statistical aggregate functions are integrated
into all diagram types.
New functions for Sinamics Connect 300
With Sinamics Connect 300, Siemens introduced a
simple plug and play solution for integrating Sinamics converters into the IT
world in 2018. The solution is designed for low-voltage converters and supports
cloud-based digitalization solutions. At SPS, Siemens presents the solution
with new features and improved usability. One new feature is expert mode, where
on request the user can individually differentiate the parameters of the Sinamics
drive which are to be stored in Mindsphere, the open, cloud based IoT operating
system. The new Sinamics Connect 300 device includes comprehensive
commissioning and service management with integrated web server, which
simplifies configuration even with very specific requirements. The web server enables
comprehensive management of the device, e.g. CA certificates, license management
and firmware updates. On the web server homepage, users can also view the MindSphere
connection status directly and therefore immediately check cloud connectivity. To
ensure that data is not lost even in the event of network failures, a data buffer
of up to 500 MB is provided. For secure data transfer, the transfer protocol
has been changed from HTTP to HTTPS and the security guidelines have been
updated to prevent unauthorized manipulation of the device. Sinamics Connect
300 adds to the existing Standard MindConnect portfolio and gives users the
opportunity to connect Sinamics converters that do not communicate via Profinet
directly to MindSphere. In addition, Sinamics Connect 300 enables the
connection of Sinamics drives in existing plants without the need for expensive
and time-consuming hardware or software modifications. Sinamics Connect 300 does
not use a proprietary data model, which means that uploaded converter data can
be provided to all Mindsphere apps without problems.

At SPS 2019, Siemens presents its latest solutions for smart and networked drive technology.
For further information regarding Siemens at the SPS, please see www.siemens.com/press/sps2019 and www.siemens.com/sps19
For further information regarding digitalization in drive technology, please see
www.siemens.com/digital-drives
For further information regarding digitalization in drive technology, please see
www.siemens.com/digital-drives
Siemens Digital Industries (DI) is an innovation leader in automation and digitalization. Closely collaborating with partners and customers, DI drives the digital transformation in the process and discrete industries. With its Digital Enterprise portfolio, DI provides companies of all sizes with an end-to-end set of products, solutions and services to integrate and digitalize the entire value chain. Optimized for the specific needs of each industry, DI’s unique portfolio supports customers to achieve greater productivity and flexibility. DI is constantly adding innovations to its portfolio to integrate cutting-edge future technologies. Siemens Digital Industries has its global headquarters in Nuremberg, Germany, and has around 76,000 employees internationally.
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 170 years. The company is active around the globe, focusing on the areas of power generation and distribution, intelligent infrastructure for buildings and distributed energy systems, and automation and digitalization in the process and manufacturing industries. Through the separately managed company Siemens Mobility, a leading supplier of smart mobility solutions for rail and road transport, Siemens is shaping the world market for passenger and freight services. Due to its majority stakes in the publicly listed companies Siemens Healthineers AG and Siemens Gamesa Renewable Energy, Siemens is also a world-leading supplier of medical technology and digital healthcare services as well as environmentally friendly solutions for onshore and offshore wind power generation. In fiscal 2019, which ended on September 30, 2019, Siemens generated revenue of €86.8 billion and net income of €5.6 billion. At the end of September 2019, the company had around 385,000 employees worldwide. Further information is available on the Internet at www.siemens.com
.
Reference Number: PR201911215701en
Contact
Katharina Lamsa
Digital Industries
Gleiwitzer Str. 555
90475 Nuremberg
Germany
90475 Nuremberg
Germany
+49 (911) 895-7975