- Integrated motor portfolio of Simotics reluctance motors from 0.55 to 45 kilowatts
- Additional shaft heights 90 and 225
- Encoderless closed-loop control down to a standstill
- Reluctance motor portfolio rounded off with rated speeds of 1500 and 3000 revolutions per minute
Siemens is extending its portfolio of Simotics synchronous-reluctance motors to include the two new shaft heights, AH90 and AH225. With these new additions, the company is addressing calls from renowned manufacturers of pumps, fans, compressors and machine builders in general for different shaft heights. The motors are available in a power range of 0.55 to 45 kilowatts (kW), and now also with rated speeds of 1500 and 3000 revolutions per min-1. In conjunction with the recently launched Sinamics Reluctance Control License, precise encoderless closed-loop torque control is possible down to a standstill. The license enables field-oriented (vector) closed-loop control even when at a standstill – reliably eliminating the possibility of the synchronous motor "stalling" at any time even if the load inertia is not known.
- Sidrive IQ improves drive systems along the entire life cycle up to the megawatt range
- Cloud-based application based on networked drive systems from Siemens
- Increased productivity, reliability and ease of maintenance
- Standardized link enabled by Sinamics Connect 500 and Simotics Connect 600 connectivity modules
Sidrive IQ from Siemens provides a digital platform enabling the evaluation and utilization of data gathered from drive systems. On the basis of networked drive systems from Siemens, this cloud-based application is now also available for motors and converters in the medium and high-voltage range. This opens up an array of benefits for plant and machine operators, from optimized maintenance activity and maximum availability to increased productivity, from low outputs through to the megawatt range across the entire life cycle. Connectivity modules such as Simotics Connect 600 and Sinamics Connect 500 enable high-voltage motors and medium-voltage converters to be simply linked up to Sidrive IQ. With the latest generation of its Remote Services and Condition Monitoring Services offered as part of the Sidrive IQ Services portfolio, Siemens is making available corrective measures for fixing faults, preventive maintenance offers and proactive services for optimized performance. The optimized drive systems are used in pumps, fans and compressors across different sectors of industry such as oil and gas, mining, food and beverage, water and wastewater, metals and cement.
- New software for omnidirectional control
- 360-degree freedom of movement for AGVs
- Innovative steering system implemented with ebm-papst
Siemens has expanded Simove, the scalable automation solution for Automated Guided Vehicle (AGV)
applications, to include functionality for omnidirectional control. The new software supports unrestricted freedom of movement for AGVs. Together with Simatic
Micro-Drive, the new member of the Siemens converter family specifically for
the safety extra-low voltage range, plant and machine builders can create universal
and flexible systems. Together with partner ebm-papst an initial application example has been realized: a steering system that uses Simatic Micro-Drive,
the universal Simatic controller and the new control software from Simove. The
compact steering system features a special gearbox where the speeds of both
motors in the steering system are overlaid. This means that the steering system
does not require moving cables. The result is 360-degree rotational movement of
the wheel and therefore of the system. In addition, the high transmission in the
driving and steering direction provides a high level of control accuracy for
the system. Thanks to the integrated safety functions of the Simatic Micro-Drive,
safe control and monitoring of the integrated motors is ensured at all times.
- Simatic S7-1500 controller with expanded motion control functionality and Sinamics S120 drive control in one device – thus saving space
- Powerful for high-end applications, with integrated safety functionality for the controller and drive
- Extensive communication interfaces, technology I/Os, as well as cross-PLC synchronous operation for an easy implementation of modular machine concepts
- Proven engineering in the TIA Portal
Siemens is expanding its product portfolio of technology CPUs with the Simatic Drive Controller. The new controller combines a Simatic S7-1500 controller with motion control, technology and safety functionality with a Sinamics S120 drive control in one device, thus saving space. This makes it easy to implement requirements for powerful, compact and flexible automation solutions. The high performance of the new controller is particularly beneficial for applications with many axes where a multi-axis drive system is used – for example in packaging, printing and textile machines.
- Voltage
regulation system for the Kusenhorst substation
- Two-thirds
of the multilevel STATCOMs installed worldwide are from Siemens
In handing over the converter for a state-of-the-art grid
stabilization system for voltage regulation to the German transmission grid
operator Amprion, Siemens is celebrating delivery of its one-hundredth STATCOM
(static synchronous compensator) from the SVC PLUS series. The turnkey
installation will be deployed in the important Kusenhorst node in North Rhine
Westphalia, Germany. STATCOM systems stabilize fluctuations in the grid by
absorbing or feeding in voltage-supporting reactive power, depending on the
requirements. This approach significantly reduces the risk of voltage drops and
blackouts. Two-thirds of the globally installed STATCOM systems with modular
multilevel converter technology (MMC) are from Siemens, making the company the
world market leader in this segment.
The VAG Verkehrs-Aktiengesellschaft Nuremberg has ordered 27 type G1 four-car metro trains from Siemens Mobility. The contract also includes an option for a total of a further 7 trains. These trains are earmarked for service on Nuremberg's U1 line. The trains will be built in the Siemens Mobility plant in Vienna. Core components of the G1 will be manufactured in the Nuremberg metropolitan area and include such products as the drive converters, traction motors, auxiliary converter units and control equipment. The project management, development and service support will be provided from Erlangen.
- TIA Portal V15.1: Practice-oriented functional expansions of the engineering framework along the entire value chain
- Spotlight on simulation and virtual commissioning
- Complete validation of machines with Simatic Machine Simulator V1.0 and NX Mechatronics Concept Designer
- Extended applications with redundant Simatic S7-1500R/H controllers and integration of the Sinamics S210 servo converter
With TIA Portal V15.1 (Totally Integrated Automation Portal) Siemens is enhancing its engineering framework with new practice-oriented functions for all phases, from planning to engineering to commissioning. Key topics in TIA Portal V15.1 include new simulation and virtual commissioning options which enable even better digital design of integrated work processes, as well as the expanded application focus with Simatic S7-1500R/H controllers, Sinamics S210 drive integration, Multiuser Engineering, software units and OPC UA functions.
- Siemens industrializes additive manufacturing with polymers with EOS and DyeMansion as partners
- Siemens and EOS support Hexr in the mass customization of additively manufactured bicycle helmets
- Digital Enterprise portfolio offers integrated software and automation solutions for the industrialization of additive manufacturing
- Additive Manufacturing Network – an online order-to-delivery collaboration platform for the industrial additive manufacturing community, helps streamline the AM production process
Siemens' Digital Enterprise portfolio consists of software and automation solutions that optimize process steps along the entire value chain of additive manufacturing. This holistic approach is unique in the field of the industrialization of additive manufacturing. "The automated chain of coordinated production steps from all suppliers, from design and printing to post-processing, as well as end-to-end IT integration, is crucial for high productivity and maximum flexibility. This applies to series parts as well as to a highly flexible lot-size-1 production for individualized products or spare parts," explains Dr. Karsten Heuser, Vice President Additive Manufacturing at Siemens Digital Industries.
- Early detection of anomalies in the drivetrain with the support of artificial intelligence
- Trend Prediction for optimized maintenance efficiency
- Higher productivity and reduced machine and system downtime
Siemens has supplemented the Mindsphere application Predictive Service Assistance with an AI-based module. The new Artificial Intelligence module identifies concrete fault patterns in motors at an early stage, such as misalignment or a defective bearing. The application thus helps users to reduce downtimes and further improve spare parts and maintenance processes. The new Artificial Intelligence module for motors uses a neural network to solve what was previously implemented using a defined KPI limit value. This enables the module to detect anomalies even before the defined limit value and provides clear indications of the type and severity of faults and their development. As soon as the application detects signs of an error, it warns the user and generates a due date that indicates when the error should ideally be corrected and what corrective action is recommended to prevent an unplanned downtime. Predictive Service Assistance with the new AI-based Artificial Intelligence module is offered as part of a Predictive Service Assessment. The package includes a customized configuration service that ensures that the Mindsphere application with the new AI-based module runs optimally according to the customer's requirements.