Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release19 November 2019Digital IndustriesNuremberg
Simatic Drive Controller – the new motion controller with integrated drive control

The controller is available in the two performance classes CPU 1504D TF and CPU 1507D TF. Thanks to integrated safety functionality for the controller and drive, even demanding requirements regarding operator and machine safety can be met.
The Simatic Drive Controller is equipped with extensive interfaces, including three Profinet interfaces and one Profibus interface for communication with, for example, HMI, I/O and other drive systems as well as on-board technology I/Os. This permits the efficient implementation of dynamic motion control applications.
With the "Cross-PLC synchronous operation" function, which is now available in all technology CPUs, it is also possible to implement gearing and camming across CPUs, so that there are virtually no limits to axis quantity structures. In addition to the performance distribution among several CPUs, modular automation concepts can also be easily implemented with cross-PLC synchronous operation. The engineering of the Simatic Drive Controller is carried out conveniently and efficiently in the TIA Portal Engineering Framework.
Background information:
Individual products require machines and production lines that can be quickly and easily adapted to different formats, sizes, product types, and production processes. Especially in production, maximum flexibility, efficiency, precision and availability are required. The reliable monitoring of all movements in producing machines also plays an essential role. Siemens offers suitable technological solutions based on the Simatic Advanced, Distributed and Drive Controllers.
Additional Information about Simatic Drive Controller can be found at
www.siemens.com/drive-controller
Additional information about Siemens at SPS 2019 can be found at
www.siemens.com/press/sps19 and www.siemens.com/sps19
www.siemens.com/drive-controller
Additional information about Siemens at SPS 2019 can be found at
www.siemens.com/press/sps19 and www.siemens.com/sps19
Siemens Digital Industries (DI) is an innovation leader in automation and digitalization. Closely collaborating with partners and customers, DI drives the digital transformation in the process and discrete industries. With its Digital Enterprise portfolio, DI provides companies of all sizes with an end-to-end set of products, solutions and services to integrate and digitalize the entire value chain. Optimized for the specific needs of each industry, DI’s unique portfolio supports customers to achieve greater productivity and flexibility. DI is constantly adding innovations to its portfolio to integrate cutting-edge future technologies. Siemens Digital Industries has its global headquarters in Nuremberg, Germany, and has around 76,000 employees internationally.
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 170 years. The company is active around the globe, focusing on the areas of power generation and distribution, intelligent infrastructure for buildings and distributed energy systems, and automation and digitalization in the process and manufacturing industries. Through the separately managed company Siemens Mobility, a leading supplier of smart mobility solutions for rail and road transport, Siemens is shaping the world market for passenger and freight services. Due to its majority stakes in the publicly listed companies Siemens Healthineers AG and Siemens Gamesa Renewable Energy, Siemens is also a world-leading supplier of medical technology and digital healthcare services as well as environmentally friendly solutions for onshore and offshore wind power generation. In fiscal 2019, which ended on September 30, 2019, Siemens generated revenue of €86.8 billion and net income of €5.6 billion. At the end of September 2019, the company had around 385,000 employees worldwide. Further information is available on the Internet at
www.siemens.com.
Contact
Andreas Friedrich
Digital Industries
Gleiwitzer Str. 555
90475 Nuremberg
Germany
90475 Nuremberg
Germany
+49 (1522) 2103967