Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release24 April 2018Process Industries and DrivesNuremberg
Siemens extends performance spectrum of synchronous-reluctance drive system

The image shows a Sinamics G120converter.
As digitalization is the key to fast, efficient working, Siemens has equipped the motors and converters with a data matrix code. Attached to the motor enclosure and the display or converter housing, this code provides users with access to technical data, spare part information and operating instructions at a glance. The data is accessed with the aid of a mobile terminal and the Simotics Digital Data App for motors, or alternatively the Siemens Industry Online Support App for converters.
The availability of 2D or 3D engineering data makes for shorter, more flexible design and engineering processes.
As an integrated drive system, Simotics reluctance motors and Sinamics converters are specifically coordinated to work together. Compared to induction motors, they offer highly efficient operation, particularly in the partial load range. The coordinated system comprising a Sinamics G120 converter and synchronous-reluctance motor enables the ideal closed-loop control of pumps, fans and compressors. By combining the Sinamics S120 converter and Sinamics Reluctance Control License, it is even possible to achieve encoderless closed-loop control down to a standstill, enabling applications in conjunction with coilers, servo pumps and extruders.
Proven system already in widespread operation
Synchronous-reluctance drive systems operate with exceptional energy efficiency, while also providing far greater power reserves than a comparable asynchronous drive. Particularly in comparison to conventional asynchronous technology, with its Simotics synchronous-reluctance motors Siemens enables extremely high efficiency to be achieved at the rated operating point and in the partial load range while at the same time ensuring high power density and dynamic performance. The result: savings in terms of costs and energy.
Synchronous-reluctance technology has proven highly successful in countless practical applications in the field. Customers such as machine builder Olbrich, plasterboard manufacturer Knauf and compressor manufacturer Kaeser Kompressoren have opted to use synchronous-reluctance drives due to their outstanding energy efficiency, their optimum operating behavior as a result of synchronous encoderless operation and their simple commissioning with the aid of the motor code.
Synchronous-reluctance technology has proven highly successful in countless practical applications in the field. Customers such as machine builder Olbrich, plasterboard manufacturer Knauf and compressor manufacturer Kaeser Kompressoren have opted to use synchronous-reluctance drives due to their outstanding energy efficiency, their optimum operating behavior as a result of synchronous encoderless operation and their simple commissioning with the aid of the motor code.
For further information on synchronous reluctance motors, please see www.siemens.com/reluctancedrivesystem
For this press release

Event: Siemens at the Hannover Messe 2018
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for 170 years. The company is active around the globe, focusing on the areas of electrification, automation and digitalization. One of the world’s largest producers of energy-efficient, resource-saving technologies, Siemens is a leading supplier of efficient power generation and power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. With its publicly listed subsidiary Siemens Healthineers AG, the company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2017, which ended on September 30, 2017, Siemens generated revenue of €83.0 billion and net income of €6.2 billion. At the end of September 2017, the company had around 377,000 employees worldwide. Further information is available on the Internet at www.siemens.com.
Reference Number: PR2018040244PDEN
Contact
Stefan Rauscher
Siemens AG
Gleiwitzer Str. 555
90475 Nuremberg
Germany
90475 Nuremberg
Germany
+49 (911) 895-7952