Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release22 March 2018Digital Factory Nuremberg
Optimum machine safety using Extended Safety Integrated functions

The picture shows the Sinamics S210 servodrive system from Siemens.
The Extended Safety functions are activated by a license in the converter and are triggered by the higher-level Simatic S7-1500F and/or S7-1500 TF controller via Profisafe. STO and SS1 are activated by terminals and/or Profisafe.
The Sinamics S210 servo drive system consists of a converter and the specially developed Simotics S-1FK2 servomotors, which are available in five performance classes from 50 to 750 watts. The motors are connected to the converters using a One Cable Connection (OCC). The Sinamics S210 is particularly suited for the dynamic control of motor axes, making sure that low loads can be moved particularly dynamically.
The converter is activated via a web server and one-button tuning.
The interaction between servomotors, quick sampling and smart control algorithms for the converters, a high-quality encoder system, low rotor inertia and high overload capacity provide this drive system with high dynamics and exceptional accuracy.
For further information on Sinamics S210, please see www.siemens.com/sinamics-S210
For this press release

Event: Siemens at the Hannover Messe 2018
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for 170 years. The company is active around the globe, focusing on the areas of electrification, automation and digitalization. One of the world's largest producers of energy-efficient, resource-saving technologies, Siemens is a leading supplier of efficient power generation and power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. The company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2017, which ended on September 30, 2017, Siemens generated revenue of €83.0 billion and net income of €6.2 billion. At the end of September 2017, the company had around 377,000 employees worldwide. Further information is available on the Internet at www.siemens.com.
Contact
Katharina Lamsa
Siemens AG
Gleiwitzer Str. 555
90475 Nuremberg
Germany
90475 Nuremberg
Germany
+49 (911) 895-7975