In March 2018, the Siemens Building Technologies Division joined buildingSMART International (bSI) as a member of the Strategic Advisory Council and several National Chapters. Siemens is the first building technology vendor to become part of this international not-for-profit organization. Created by bSI, the "openBIM" data format defines open, vendor-neutral international standards for BIM (Building Information Modeling). These standards are essential in order to promote rapid digitalization in the built asset sector.
- 50/50 joint venture for the maintenance of locomotives
- Company to be named Locomotive Workshop Rotterdam (LWR)
- Workshop to be built in the port of Rotterdam
Siemens and Mitsui Rail Capital Europe (MRCE), a full-service locomotive leasing company, have agreed to found a joint venture for the servicing and maintenance of locomotives. The agreement stipulates that Siemens and MRCE each will hold a 50-percent stake in the joint venture and jointly manage the new company. Founding of the firm, pending approval of antitrust authorities, is expected to be completed in the first half of calendar year 2018.
- DSB orders Vectron locomotives in AC configuration
- Option for 18 additional locomotives
- Delivery beginning at the end of 2020
Danish State Railways (DSB) and Siemens signed a contract for the delivery of 26 alternating-current (AC) Vectron locomotives. The locomotives will operate in Denmark and Germany. Delivery of the units is scheduled to begin at the end of 2020. The contract with DSB also includes maintenance of the locomotives for ten years and options for the delivery of an additional 18 units and an extension of the maintenance contract for a further five years. The locomotives will be built at the Siemens factory in Munich-Allach.
- Successful strategic cooperation with Atos, which started in 2011, to be further expanded
- Joint innovation and investment program extended by an additional €100 million, totaling €330 million
- Joint order intake of € 2.5 billion to date, overachieving all expectations
- Ambition to further accelerate joint business until 2020, driven by digital collaboration and joint go-to-market
Siemens and Atos today announce the reinforcement of their strategic co-operation, with plans to accelerate their joint business until 2020 through an ambitious joint go-to-market plan and the strengthening of their joint innovation and investment program. The program has been increased by €100 million, totaling €330 million – more than three times the original sum. This will further support the Siemens and Atos IoT MindSphere-Codex strategic co-operation as well as the joint go-to-market.
- Business Combination Agreement signed
- Siemens Alstom's future Board of Directors: Siemens Managing Board Member Roland Busch to be nominated as Chairman and Alstom Lead Director Yann Delabriere to be nominated as Vice-chairman
Siemens and Alstom have set the next key milestone for a champion in mobility. They have entered today into a Business Combination Agreement (BCA) regarding the proposed combination of Siemens' mobility business, including its rail traction drive business, with Alstom. This BCA follows the Memorandum of Understanding signed on 26 September 2017 and the conclusion of the required works council information and consultation process at Alstom regarding the proposed deal. The BCA sets forth the terms and conditions agreed upon by the two companies.
- Extended safety functions for Sinamics S210
- New firmware version V5.1 SP1 provides comprehensive protection of machine functions
- Encoders of Simotics S-1FK2 motors with new 22-bit resolution
Siemens extends the Sinamics S210 servo drive system to include the Extended Safety Integrated functions. The existing basic functions such as Safe Torque Off (STO), Safe Stop 1 (SS1) and Safe Brake Control (SBC) are now complemented by extended functions provided by the new firmware versions V5.1 SP1: Safe Stop 2 (SS2), Safe Operating Stop (SOS), Safely-Limited Speed (SLS), Safe Speed Monitor (SSM), Safe Direction (SDI), and Safe Brake Test (SBT). All of these functions ensure machine functions are provided with comprehensive protection. Also the encoders of the Simotics S-1FK2 motors have been updated, to support the new Extended Safety functions and provide an encoder resolution of 22 bits. The motors fitted with the new encoders can be used as replacement parts for previous models. Typical uses for the new drive system include in particular packaging machines, handling applications such as Pick & Place, wood and ceramic processing as well as digital printing.
Siemens expands its 3KF switch disconnector series with versions featuring Sitor fuses for semiconductor protection. Switch disconnectors are used to safely switch on and off electric equipment under load. They protect systems in the event of short circuit and prevent dangerous electrical shocks, e.g. during maintenance work. Compared to switch disconnectors with LV HRC fuses, the new versions with Sitor fuses are even faster. This prevents damage to very sensitive electronic components, e.g. in frequency converters, UPS systems and soft starters for motors. Moreover, the new series excels through streamlined heat dissipation. As a result, the switch disconnectors with Sitor fuses can be used even at high load currents.
Siemens was recently selected to supply another SGT-700 mechanical drive compression train for the Camisea gas-condensate asset located in Peru. The equipment, identical to that Siemens supplied in 2011, is essential to the continuing exploration and production of hydrocarbons in Block 88, operated by Pluspetrol Peru Corporation S.A. Due to the natural gas pressure decline of the reservoirs, the Camisea production plan includes a centralized wellhead compression system for all fields.
- Plant and process optimization based on a digital twin
- Cloud-based solutions for the efficient use of pumps
- Pre-configured sample solutions for the electrification, automation and drive systems of plants
At the IFAT 2018 trade show for environmental technologies, Siemens will be focusing on the digitalization of water and waste water plants. The solutions on display will cover the entire life cycle of plants - from planning through to operation and maintenance, helping to sustainably reduce energy consumption and lower the overall costs. Companies and municipalities are increasing both the efficiency and security of supply by, for example, planning, simulating and optimizing plants and processes using a digital twin. Innovations include new hardware concepts and industry-specific modules for the Simatic PCS 7 process control system, as well as automation over the TIA Portal using Simatic S7-1200 and S7-1500 and cloud-based solutions for the optimized use of pumps.
In a consortium with the general infrastructure contractor Per Aarsleff A/S, Siemens has received an order to build a light rail system in Copenhagen, Denmark, from urban transport development company Greater Copenhagen Light Rail I/S. The contract will be implemented as a turnkey project. Commissioning of the system is planned for 2024.