Bombardier Transportation, a subcontractor for the ICE 4 project, has determined within the framework of its quality management that individual welds on ICE 4 railcar bodies were not carried out as prescribed. This deviation is not safety relevant.
- 1.3-gigawatt turnkey combined cycle power plant
- Long-term service program and operation & maintenance (O&M) services included
- Largest LNG-to-power development in Latin America
- Total project volume of €1 billion
Siemens has secured an order for the turnkey construction of a new combined cycle power plant for the integrated LNG-to-Power project GNA 1 of Gás Natural Açu in the Port of Açu in the state of Rio de Janeiro, Brazil. Siemens is providing an equity investment and owns one-third of the project company Gás Natural Açu (GNA) together with Brazil logistics company Prumo Logística S.A. and BP. In addition, Siemens signed a long-term service agreement and will operate and maintain the plant to help ensure reliability, availability and operational performance. The order is the first application for the highly efficient and proven Siemens H-class gas turbine in Brazil. With a capacity of approximately 1.3 gigawatts (GW), the power plant will provide affordable and clean energy for Brazil. Total project volume for GNA 1 is approximately €1 billion (R$4.5 billion).
- Stimulating two senses through acoustic (EN 54-3) and optical (EN 54-23) alarm devices
- Voice messages can be emitted in two languages for faster evacuation
- High alarming reliability thanks to daily disturbance-free tests
Siemens Smart Infrastructure has launched new ceiling- and wall-mounted alarm devices. The expanded portfolio includes both acoustic and optical alarm devices in accordance with European Standards EN 54-3 / EN 54-23 and EN 54-17. One highlight of the expanded portfolio are the voice sounders with built-in voice messages because they improve the reaction time to alarms.
- Features signaling, communication and electrification technology
- Mass transit critical to the city's urban development
- With 65 kilometers of Blue line track, capacity is up to 30,000 passengers per hour
The latest expansion of Delhi Metro Rail Corporation's (DMRC) Blue Line signifies the city's commitment to modernizing mass rapid transit and features Siemens Mobility's signaling and electrification technology. As one of the world's largest metropolitan areas, India's National Capital Region of Delhi has grown from 6.2 million residents in 1981 to approximately 25 million residents in 2018. With more than 2 million riders per day, the network is expanding rapidly. From just 87 kilometers in 2010 to 375 kilometers today, the network continues to grow. The latest expansion adds 6.6 kms for a total of 65 kms. The signaling, electrification and automatic train control systems on this portion of the line ensure optimum headway between two consecutive trains on the same line during peak hours, resulting in capacity of up to 30,000 riders per hour on one line.
New research from Siemens Financial services explains how manufacturers are in a race against time to gain competitive advantage from Industry 4.0 investment, before the “tipping point” of majority adoption. A must-read for future focused manufacturing financial managers, the Whitepaper explains how Finance 4.0 solutions are providing practical methods of helping companies to urgently invest in Industry 4.0 and gain early mover advantage.
- Improving engineering and production processes
Siemens is intensifying its cooperation with the EDAG Group as a leading global independent engineering company for the automotive industry, in order to further promote industrial applications of additive manufacturing (AM) and to make engineering and production processes more efficient. Based on many years of successful project-specific collaboration in factory and production planning, in the field of engineering the innovative "NextGenerationSpaceframe 2.0" project will be presented at the Hannover Messe from April 1 to 5, 2019 at the Siemens booth (Hall 9, Booth D35) as the clear result of this successful cooperation.
- Services support first use of Siemens H-class turbine in an aluminum smelting facility globally
- Siemens' first long-term service agreement in the UAE for an H-class turbine
- Power services will ensure reliable operations for stable power production
Emirates Global Aluminum (EGA), the world's largest 'premium aluminum' producer, and Siemens announced the first power services agreement for an H-class gas turbine in the United Arab Emirates (UAE). With the new 20-year service agreement, Siemens will provide maintenance and repairs as well as onsite personnel support for the gas turbine and its generator at the planned over 600-megawatt (MW) combined cycle project feeding EGA's Jebel Ali power plant in Dubai.
- SensgearTM technology launch for digital connectivity of switchgear products
- New Sensformer® advanced with applications based on digital twin simulation of transformers
- Portfolio extension comes with comprehensive data analytics for added transparency, enhanced productivity, and advanced intelligence
Siemens is introducing Sensgear, its new digital switchgear portfolio, and the Sensformer advanced at this year's Hannover Messe. With the combination of the already well-established digitally connected transformer, the Sensformer, and the new Sensgear technology, all substation transmission assets are now fully connective, allowing operators to check their status via online applications in real time. Gas-insulated switchgear, circuit breakers, surge arresters, disconnectors, instrument transformers, and coil products will henceforth be equipped with Sensgear technology. All devices are connected via a smart and robust Internet of Things (IoT) gateway that securely transmits the required information to a cloud-based storage and visualization platform. All Sensgear products provide additional transparency with GPS and local weather information as well as product-specific measurement data that includes gas density, liquid temperature, gas leakage, and switching position.
- Integration into the digital workflow with data exchange via AutomationML
- Import and simulation of existing TIA Portal projects V15.1
- Configuration option of modular switches
- Simulation of broadcast with definition of broadcast limits
Siemens is launching a new version of the software tool for planning and simulating Profinet automation networks on the market. Sinetplan V2.0, the Siemens network planner, supports plant planners, builders and operators of automation systems and Profinet networks already in the planning phase and facilitates the professional and proactive simulation of a plant network. At the Hannover Messe 2019, Siemens is exhibiting the new features with which Sinetplan V2.0 is integrated into the digital planning and engineering workflow.
- New engineering portal speeds up plant engineering
- Object queries now editable in Comos web application
- Modular engineering with intelligent templates and central data storage
In the latest version 10.3 of its Comos CAE software solution for the process industry, Siemens is focusing on increasing efficiency in engineering. Using the Comos Engineering Portal included in this version, engineering processes can be significantly shortened. In addition to this, new developments and functional expansions are available for the current version in modular engineering and for mobile applications.