- New version 8.0 facilitates integration of Simatic S7-1500 controller as well as mixed operation with Simatic S7-400 controller operation with the Simatic S7-400 controller
- Improved production and batch transparency with new MES reporting options
- Enhanced safety concept with new functions
- Lean Edition for micro breweries and craft brewers
Siemens is presenting a new version of the Braumat brewery process control system at the BrauBeviale in Nuremberg: The latest version 8.0 is based on the Simatic S7-1500 controller and has been optimized in the areas of reporting, weighing systems and security. Already installed Simatic S7-400 controllers can still be used, including in mixed operation. Existing Braumat installations can be expanded or modernized with Simatic S7-1500 controller. Production downtimes caused by new installations are thus avoided.
- Highly compact design, up to 110 kiloamps
- Maintenance-free up to 10,000 interrupting cycles at current of 15 kA
- Based on proven HB3 generator platform with vacuum switching tech
Siemens is expanding its HB3 generator circuit-breaker portfolio with a new compact version. The HB3-Compact (HB3-C) offers the possibility for vertical or horizontal mounting and uses maintenance-free vacuum switching technology. These features make it especially valuable for retrofit applications in power plants, where the highest security of supply is crucial, and space is limited due to existing installations. The new system will be presented for the first time at the European Utility Week 2019, taking place in Paris from November 12 to 14.
We released our financial figures for the fourth quarter and fiscal year 2019 on November 7, 2019. The Press Conference and the Analyst Call were broadcast live.
- Efficient and future-proof maintenance with Predictive Services for Drive Systems
- New Mindsphere Predictive Service Assistance app provides digital support for the service portfolio, while also offering transparency and streamlined ordering processes
- Predictive Services for Drive Systems for increased productivity and reduced downtimes for machines and plants
With Predictive Services for Drive Systems, Siemens presents a standardized extension to the local service agreement at this year’s SPS. This is based on the new Mindsphere Predictive Service Assistance app. It makes maintenance more efficient for Sinamics drive systems and/or Simotics motors in the low voltage range.
- First soft starter series with integrated Safe Torque Off function
- Enhanced protection when shutting down electric motors
- High functional density saves space and decreases cost
Siemens Smart Infrastructure expanded its soft starters portfolio for motors, with the launch of Sirius 3RW55 Failsafe and Sirius 3RW50. Soft starters ensure electrical motors used in industry and infrastructure are protected during startup and ramp-down. The Sirius 3RW55 Failsafe soft starters are the first to feature the integrated Safe Torque Off (STO) function. As specified in safety standards, the protection function for electrical drive systems ensures that torque-generating energy stops acting when motors are turned off, preventing an unwanted restart. Control panel manufacturers no longer require using separate individual components to have this function, which reduces the time and effort for wiring and maintenance works and saves space in the control cabinet. In addition, the switching time of the integrated solution is significantly shorter than for conventional, electromechanical components.
- Ferraro to take on this role, effective
December 1, 2019, in addition to her position as Chief Financial Officer (CFO) at
Siemens Digital Industries
- In this role, she will report to Deputy
CEO and future Labor Director Roland Busch
Maria
Ferraro (46), Chief Financial Officer at Digital Industries, will become the
new Chief Diversity Officer (CDO) of Siemens AG, effective December 1, 2019. In
her capacity as CDO, she will be succeeding Janina Kugel, whose contract will
expire at the end of January 2020. Ferraro will take on the new position in addition
to her leadership role as CFO at the Digital Industries Operating Company. As
Chief Diversity Officer, she will report directly to Deputy CEO Roland Busch, who
will be succeeding Janina Kugel as Chief Human Resources Officer (CHRO) and
Labor Director, effective December 1, 2019.
- First order from Asia for HL-class gas turbine
- New power plant with a capacity of more than one gigawatt
- Efficiency rating of more than 63 percent
Siemens will set up a high-efficiency HL-class power island for a new combined cycle power plant (CCPP) in South Korea. This will be the first two state-of-the-art HL-class gas turbines that Siemens will supply to a customer in Asia. The new plant, which will be built in Yeoju, in South Korea’s Gyeonggi Province, will run on regasified liquefied natural gas (LNG) and offer a generating capacity of more than one gigawatt. With a maximum efficiency rating of more than 63 percent the gas turbine will allow the power station to get the most out of the valuable LNG for electricity generation, enabling especially economical and environmentally friendly operation. The customer is South Korean EPC SK Engineering & Construction Co., Ltd., which is constructing the entire plant for the independent power producer Yeoju Energy Services.
- New Simotics HV M slipring motors provide range of power up to 4.5 MW
- Easy integration into SIDRIVE IQ applications for highest availability, serviceability, productivity and efficiency
- Easy plant integration due to 3-D Motor models to speed up complete plant integration processes
- Certified and proven Siemens MICALASTIC® VPI insulation system with extreme long lifetime
Building on more than a century of experience in manufacturing slipring motors, Siemens today announces the new Simotics HV M slipring motor. Designed and engineered for applications mainly in the cement and mining industries, the newest slipring motor is implemented in a wide range of applications including but not limited to mills, crushers, conveyors and fans. The new platform motor with its power range up to 4.5 MW completes the Siemens slipring motor family which covers now the power range from 0.5 to 8.2 MW.
Bane NOR, the state-owned agency responsible for the Norwegian national railway infrastructure, has contracted Siemens to upgrade the signaling equipment of the entire Norwegian rail network to the European Train Control System (ETCS). Commissioning of the rollout lines is scheduled to be completed by 2034. The contract also includes services for 25 years and is worth around 800 million euros in total.