- Seamless redundancy and high precision time synchronization from a single device
- Easy migration to highly reliable networks with zero packet loss
- Minimal downtime and reduced risk of communication disruptions
- Specifically designed for modern digital substation applications
Siemens has introduced a new line module for the Ruggedcom RST2228 and RST2228P Layer 2 19” rack switches, the Ruggedcom RMM2972-2RNA. This module strengthens the Ruggedcom RST2228 19” rack switch offering to the electric power utilities by providing seamless redundancy with PRP/HSR (Parallel Redundancy Protocol/High-availability Seamless Redundancy), enhanced IEEE1588 implementation, high bandwidth uplinks, and traffic filtering and segmentation from a single device. This module eliminates network downtime due to single points of fault, resulting in high reliability and availability for modern digital substation applications as mandated by the IEC 61850 standard.
Kicking off 2020, Siemens Mobility will participate in the Consumer Electronics Show (CES), a preeminent gathering place for the most innovative minds and organizations, taking place in Las Vegas, January 6-10, 2020. Under the motto of “Connecting people through seamless mobility”, Siemens Mobility will be showcasing a variety of digital innovations from its intelligent traffic systems and intermodal solutions.
Siemens Mobility delivers innovative solution-driven technology that enhances quality of life: making communities more sustainable and better places to live, work and play. Contributing to the next mobility revolution, comprehensive traffic management systems are shaping an autonomous, connected, electric and shared mobility ecosystem.
- Partnership brings together leading-edge integrated circuit (IC) methodologies, processes and tools to help the automotive supply chain solve design and verification challenges
- Leveraging Arm automotive IP and software within Siemens’ PAVE360 digital twin environment enables collaboration and empowers automakers and suppliers to develop and validate differentiated safety enabled systems, ICs and software solutions in the context of the entire vehicle
- Siemens’ PAVE360, part of Siemens Digital Industries Software’s Xcelerator portfolio, helps automotive companies innovate and develop the complex electronic systems needed for today and tomorrow’s vehicles
Siemens Digital Industries Software today announced a partnership with global semiconductor IP leader Arm, that will bring leading edge IP, methodologies, processes and tools together to help automakers, integrators and suppliers collaborate, design and bring to market their next-generation platforms much faster. This partnership was formed to address the increasingly complex challenges facing the industry in developing platforms to realize active-safety, advanced driver assistance, in-vehicle infotainment, digital cockpits, vehicle-to-vehicle/vehicle-to-infrastructure and self-driving vehicles. Key advances in computing and sensor technology are enabling companies to redefine mobility beginning with the integrated circuits and software within automotive electronics systems. The combination of Siemens’ and Arm’s innovative technologies can help automakers and suppliers deliver tomorrow’s electronic design and automotive solutions, today.
- Voltage variant of Sinamics G120X for USA and Latin America
- Save space with new size for the Sinamics V20
- Adapter kit to physically and thermally separate power module and control unit for Sinamics G120
With numerous innovations, Siemens is extending its drive portfolio, improving user-friendliness and offering space-saving installation options. The Sinamics G120X converter, designed specifically for use in water/wastewater applications and in HVAC systems, is now also available in a three-phase 3AC 200V voltage variant in the power range up to 55 kW. This means that the converters can now be integrated seamlessly into applications in the USA and in Latin America. Due to its robust construction and the coating of the PCBs according to 3C3 standard the converter is suitable for harsh environments. The new module for extending the digital and analog inputs and outputs increases the flexibility and the optimal control of converter-guided applications. The Sinamics G120X now also supports the communication protocols Profibus, Modbus RTU, USS and BACnet MS/TP. It is equipped with extensive interfaces and can be easily integrated into existing or new systems.
- Intelligent infrastructure used on three bus routes in Manhattan and Brooklyn
- Helps ease congestion and improve efficiency
- Sophisticated solution identifies violations and length of stay
Siemens Mobility has successfully launched an Automatic Bus Lane Enforcement (ABLE) solution in New York City, representing the first-ever application of this technology to be mounted on buses. The ABLE systems are installed on M15 Select Bus Service buses that operate on bus lanes benefitting more than 44,000 daily customers. The technology is playing a key part in New York City’s drive to improve bus speed and efficiency and to keep traffic moving on the city’s congested streets.
- New power output module boosts HCS4300 heating control system performance
- HCS4200: space-saving solution for use in flat control cabinets with new CIM4210C central interface module
- Simple, convenient engineering and commissioning of industrial heating processes with TIA Portal
Siemens
has equipped the modular Siplus HCS heating control systems for
switching and controlling heater fields and elements with a new power output
module (POM) and a central interface module (CIM). With more power per output
and a space-saving solution for mounting in flat control cabinets, the flexible
heating control system is now even more versatile, and can be used for example
in applications with heat registers.
- Shorter development and commissioning times
- Software libraries enable standardization
- Commissioning tests on virtual test rack
The new Sinumerik One CNC generation is at the heart of digital transformation for machine tools. As a digital native, the controller features not only a new hardware platform, but also versatile software for the creation of a digital twin. It closes the gap between the virtual and the real world and helps to reduce development and commissioning times considerably.
- Siemens announces projects to be supported in the Third Funding
Round
- Up to US$ 30 million in funding to be awarded
- Siemens Integrity Initiative's
funding volume exceeds US$ 100 million
As part of the Siemens Integrity Initiative, which has a funding volume
of more than US$ 100 million, Siemens AG has named new projects to receive
funding in order to promote corruption-free markets.
- Seven four-car Desiro Mainline trainsets ordered
- To serve in the Verkehrsgesellschaft Mecklenburg-Vorpommern rail network
- Subsequent capacity expansion to four-car trainsets ensures sustainable value creation over the entire lifecycle
Alpha Trains, the European continent’s largest leasing company for rail rolling stock, has ordered seven Desiro Mainline (ML) regional trains from Siemens Mobility. Ostdeutsche Eisenbahn GmbH (ODEG) will lease the trains for service in the rail network Baltic coast east operated from December 2019 onwards by the ODEG on behalf of Verkehrsgesellschaft Mecklenburg-Vorpommern (VMV). The production has already started at the Siemens Mobility train manufacturing facility in Krefeld. “Alpha Trains ordered the Desiro ML as its first customer many years ago and we are pleased that this proven and reliable platform is also used for this project” said Thomas Schmidt, Managing Director of Alpha Trains Europa GmbH.
- ETCS approval for Baseline 3 in Germany and Sweden
- Improved availability thanks to intelligent infrastructure
- Approval for other countries to follow
Germany’s Federal Railway Authority (EBA) has approved the Vectron locomotive for operating in Germany with the European Train Control System (ETCS) Baseline 3. Approval for Sweden has already been received. Additional countries will follow.