Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release16 December 2019Digital IndustriesNuremberg
Siplus HCS4300 and HCS4200: space-saving, high-performance heating solution

With
the new POM4320 Highend power output module for 230/277 and
400/480 V power
supply networks, the Siplus HCS4300 heating control system can now control
electrical heating elements up to 60 A. Three outputs per module can be used at
60 A, six outputs at 30 A. Integrated current measurement for each output
enables heating elements connected in parallel to be monitored so faults can be
diagnosed. Three-phase heating elements in a closed triangle, as are typically
used in applications with higher power ratings can now also be controlled.
For small heating applications with up to 32 heating elements, the
HCS4200 heating control system offers a particularly space-saving solution with
the compact CIM4210C central interface module, which is just 104 mm wide. As a
result, this HCS solution is also particularly well-suited for use in flat
control cabinets. All POMs of the HCS4200 can be used in the two slots of the
compact CIM.
The Siplus heating control system can be integrated particularly easily
into the automation environment via the engineering framework Totally
Integrated Automation Portal (TIA) – with minimal cabling effort and fast
commissioning. An HCS program library and user examples simplify engineering
even further. Smart control routines ensure that the load is distributed evenly
across the network, while integrated diagnostic functions enable faults to be
detected and localized rapidly.
Heating
control systems from Siemens can be found in a range of sectors and
applications all over the world: for example, in the drying of paint and
coatings, in the molding of plastics and lightweight construction materials, in
plastic welding, and in infrared oven baking.
For this press release
Links
Siemens Digital Industries (DI) is an innovation leader in automation and digitalization. Closely collaborating with partners and customers, DI drives the digital transformation in the process and discrete industries. With its Digital Enterprise portfolio, DI provides companies of all sizes with an end-to-end set of products, solutions and services to integrate and digitalize the entire value chain. Optimized for the specific needs of each industry, DI’s unique portfolio supports customers to achieve greater productivity and flexibility. DI is constantly adding innovations to its portfolio to integrate cutting-edge future technologies. Siemens Digital Industries has its global headquarters in Nuremberg, Germany, and has around 76,000 employees internationally.
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 170 years. The company is active around the globe, focusing on the areas of power generation and distribution, intelligent infrastructure for buildings and distributed energy systems, and automation and digitalization in the process and manufacturing industries. Through the separately managed company Siemens Mobility, a leading supplier of smart mobility solutions for rail and road transport, Siemens is shaping the world market for passenger and freight services. Due to its majority stakes in the publicly listed companies Siemens Healthineers AG and Siemens Gamesa Renewable Energy, Siemens is also a world-leading supplier of medical technology and digital healthcare services as well as environmentally friendly solutions for onshore and offshore wind power generation. In fiscal 2019, which ended on September 30, 2019, Siemens generated revenue of €86.8 billion and net income of €5.6 billion. At the end of September 2019, the company had around 385,000 employees worldwide. Further information is available on the Internet at www.siemens.com
.
Reference Number: PR201912135738en