Ostdeutsche Eisenbahn GmbH (ODEG) has ordered 23 Desiro HC regional trains from Siemens for service on the Elbe-Spree network. The order is worth around €300 million. Delivery of the 21 six-car and two four-car trains is scheduled to begin in the summer of 2022. In January 2019, ODEG was awarded the contract to operate these lines following a Europe-wide tender by Verkehrsverbund Berlin-Brandenburg (VBB).
The Desiro trainsets will be used on the regional express line RE1 (lot 1) connecting Magdeburg with Cottbus via Berlin and Frankfurt (Oder). During rush hours, trains will operate three times an hour between Brandenburg a. d. Havel and Frankfurt (Oder). The four-car Desiros are planned for service on the RE8 line connecting Wismar and Wittenberge with Baruth and Elsterwerda/Finsterwalde via Berlin, as well as on the RB17 line connecting Wismar and Ludwigslust.
The trains have generous space available for bicycles, strollers and wheelchairs and a multipurpose car with a barrier-free WC. Sliding steps enable barrier-free access at stations with 550 mm and 760 mm platform heights. Wider doors than in older trains speed and ease passenger boarding and exiting. Free WLAN on board enhances passenger convenience. A passenger safety system provides live camera coverage of activities in the cars. In case of a conflict or problem, supervisors at the operations control center can communicate directly with the car via loudspeakers. The cars are equipped inside and outside with real-time capacity displays, and this information can also be accessed via the VBB app.
- First new gas-fired power plant project in Afghanistan since the 1970s
- Electricity generation planned for summer 2019
Siemens has received the first order for its SGT-A45 mobile unit from Bayat Power, a company of the Bayat Group. A few months from now, a complete gas-fired power plant, centered around the SGT-A45 trailer-mounted unit, will begin to provide electricity for the Jowzjan Province in northern Afghanistan. The mobile solution utilizes an aeroderivative gas turbine, which can provide capacity of up to 41 Megawatts (MW) of power at 50 Hertz (Hz). The SGT-A45 mobile unit is fully tested and pre-commissioned in the factory, and its trailer-mounted design minimizes the amount of construction work required on site. As a result, the plant can begin producing electricity in only a few months and will be capable of supplying power for approximately 200,000 homes. As the first new gas-fired power plant project in Afghanistan since the 1970s, Bayat Power Phase 1 will supply clean and reliable electricity, a first step to energy independence for the country.
- Higher reading rates and reading reliability
- Additional Gigabit Ethernet interface for diagnostic and service purposes
- Easy connection to cloud applications via Simatic S7-1500 and CP 1545-1
- Powerful, flexible accessories and easy handling
Siemens has introduced the Simatic MV550, the second optical reader in its new high-end Simatic MV500 series. The device is characterized by higher computing power, which allows a fast reading process and increased reading reliability – even under difficult conditions. It has an additional Gigabit Ethernet interface for diagnostic and service purposes. The Simatic MV500 can be easily and securely connected to cloud applications. This enables users to optimize production processes and supply chains, and to increase the efficiency and quality of production, logistics and asset management.
- New CP 1545-1 communications processor for use with Simatic S7 1500
- New Simatic CloudConnect 7 Industrial IoT Gateway for existing systems
- Event-driven communication reduces network load and costsStandardized MQTT protocol enables transmission to various cloud platforms
The Siemens CloudConnect portfolio simplifies data transfer within the IIoT (Industrial Internet of Things) to cloud-based solutions. To this end, Siemens is offering the new Simatic CP 1545-1 communications processor, designed for use with Simatic S7-1500 in modern automation environments. For the cloud connection of existing systems, Siemens is now also offering the new Simatic CloudConnect 7 Industrial IoT Gateway. With CloudConnect, it is even easier for users to benefit from cloud-based data analyses. They can enhance machine availability by evaluating data for predictive maintenance purposes, for example, or machine manufacturers can offer new marketing models such as pay-per-use.
- New firmware V5.2 for even easier operation of Sinamics S120 drive systems
- Integration of the web server with new, responsive design and no special commissioning tools for diagnostics, maintenance and servicing
- Parallel connection of Active Line Modules (ALM) provides an extended performance range for booksize versions
- Users benefit from increased rated power without additional chassis unit and energy exchange in the DC link
Siemens offers new features in the firmware and hardware for the Sinamics S120 drive system. Operation is made much easier in firmware V5.2 through the integration of the web server. The web server in version V5.2 has a new, responsive design, which reacts via standard web browsers regardless of the end device used (notebook, PC, tablet or smartphone). For commissioning typical diagnostics and maintenance functions or servicing, no special tools are required. The web pages are available in six standard languages and feature error indicators and warning messages including meaningful help texts and suggestions for possible solutions. Users can intuitively create, manage and delete parameter lists - even across axes - and can perform firmware updates and system restores with the old firmware version. Backups of parameter settings can be stored on the clients using the web server and browser, and reloaded in the Sinamics converter using the Restore function. In order to test functions that are subject to license, it is possible to activate a temporary trial mode. In addition, a complete overview of all functions that are subject to license is clearly displayed in the web server. For optimum display on any Internet-capable end device, the best browsers are Microsoft Edge, Mozilla Firefox, Google Chrome and Safari. Navigation is via menu or breadcrumbs.
- Real-time data analysis from 29 gas turbines across multiple locations will increase availability, reduce forced outages and enable proactive, prescriptive maintenance
- Digitalization to improve availability, efficiency, productivity and flexibility
Siemens will install state-of-the-art Remote Diagnostic Services (RDS) for GAIL (India) Limited covering 29 gas turbines operating across the Hazira-Vijaipur-Jagdishpur (HVJ) pipeline and the Vijaipur C2/C3 Plant. The scope includes the supply of RDS hardware, site installation and commissioning including remote Operational Service Desk (OSD) and helpdesk services. The OSD will be accessible 24/7, equipped with machine learning tools and manned by technical experts to provide faster, high quality troubleshooting and guidance for problem resolution.
- 61 Vectron MS locomotives
- Deliveries beginning in March 2020
Austrian Federal Railways (ÖBB) has ordered 61 Vectron MS locomotives from Siemens Mobility. With this order, ÖBB is calling a further option from the framework contract signed in January 2017 for the delivery of up to 200 Vectron locomotives. This now brings the total number of locomotives ordered to date to 108. The locomotives will be operated by the Rail Cargo Group, the freight division of ÖBB, and are planned for cross-border freight service in several European countries. The locomotives will be built at Siemens Mobility's factory in Munich-Allach, and deliveries will begin in March 2020.
- Company awards free shares worth nearly €68 million
- High number of employee shareholders – 300,000 – constant since last year
- For the first time, Siemens employees worldwide donate share dividends to social projects
Today is "Share Day" in Germany, and Siemens is marking the occasion by highlighting its firmly anchored ownership culture: some 300,000 of the company's 379,000 employees worldwide are also Siemens shareholders. This means that nearly 80 percent of all Siemens employees are simultaneously co-owners of their company. The number of employee shareholders at Siemens has remained constant since last year. No comparable company can point to such a high number of employee shareholders.
- Initial call for four Smartron locomotives includesmaintenance contract with Siemens Mobility
- Deliveries to begin in October 2019
Siemens Mobility and Paribus Holding GmbH & Co. KG, a Hamburg-based investment and asset management firm for rail rolling stock and real estate, have signed a framework agreement for the delivery of 25 Smartron locomotives. The deal was arranged and structured by Paribus for Paris-based RIVE Private Investment. The asset management of the locomotives will be handled by northrail GmbH, the rail asset management subsidiary of Paribus. Four locomotives valued at €2.5 million each have already been ordered. Three of these will be leased by northrail GmbH to TX Logistik AG. The locomotives are intended for freight transport in Germany. Deliveries are scheduled to begin in October 2019. Siemens Mobility will also be responsible for maintenance of the locomotives for a period of eight years.