Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release21 March 2019Process Industries and DrivesNuremberg
Siemens CloudConnect simplifies IIoT data transfer to cloud-based solutions

Siemens CloudConnect simplifies IIoT data transfer to cloud-based solutions.
Instead of every single sensor having to be connected to the cloud, the Simatic S7-1500 enables field data aggregation and subsequent linking to additional process-relevant information if required. The CP 1545-1 then transfers the data to the cloud platform. The communications processor also features an integrated Stateful Packet Inspection (SPI) firewall for protecting the S7-1500 against unauthorized access. The CloudConnect functionality is easy to project in the TIA Portal using just a few input screens.
There are two ways to connect existing systems with the Industrial IoT Gateway CloudConnect 7: Simatic CC712 facilitates connection of one Simatic S7-300 or S7-400 via Industrial Ethernet by means of the S7 protocol. With Simatic CC716, on the other hand, up to seven Simatic S7 controllers can be connected via Industrial Ethernet or Profibus/MPI interfaces.
The existing automation program does not have to be changed in order to select and transfer the essential information. In addition, the data read by CloudConnect 7 from lower-level S7 stations can be made available as OPC UA variables (server). This enables standardized data exchange, for example with MES systems or HMI and third-party controllers.
The open Message Queuing Telemetry Transport (MQTT) cloud protocol is used in all cases. This established standard also makes it possible to transfer data to MindSphere, the IoT operating system from Siemens, as well as to other cloud platforms.
For further information on this topic please go to www.siemens.com/cloudconnect
More information on Siemens at the Hannover Messe 2019 is available at www.siemens.com/press/hm19 and www.siemens.com/hannovermesse
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 170 years. The company is active around the globe, focusing on the areas of electrification, automation and digitalization. One of the largest producers of energy-efficient, resource-saving technologies, Siemens is a leading supplier of efficient power generation and power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. With its publicly listed subsidiary Siemens Healthineers AG, the company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2018, which ended on September 30, 2018, Siemens generated revenue of €83.0 billion and net income of €6.1 billion. At the end of September 2018, the company had around 379,000 employees worldwide. Further information is available on the Internet at www.siemens.com.
Contact
David Petry
Siemens AG
Werner-von-Siemens-Str. 65
91052 Erlangen
Germany
91052 Erlangen
Germany
+49 (9131) 17-35398