- Simotics SD motor series from Siemens is now consistently available in efficiency class Super Premium Efficiency (IE4)
- Exceeds increasingly stringent requirements of ErP Directive 2019/1781, which takes effect in two steps in July 2021 and July 2023
- Users can meet long-term efficiency standards, save energy, lower operating costs, and reduce CO2 emissions
Siemens is presenting the Simotics SD motor series as part of the Digital Enterprise Virtual Experience at the Hannover Messe 2021. The standard version of Simotics SD is offered in the efficiency class Super Premium Efficiency (IE4) across the entire power spectrum from 2.2 to 1,000 kW and for the number of poles 2, 4, as well as from 75 kW for 6 poles and from 55 kW for 8 poles. Simotics SD in IE4 thus exceeds the so-called ErP Directive 2019/1781 (energy-related products) – both the first stage, which will be valid by July 2021, as well as the next, which will apply from July 2023. The directive defines the eco-design requirements for electric motors and speed control systems.
- Simotics XP motors from 0.25 to 460 kW available in gas groups IIB
und IIC
- Premium efficiency class for all motors
- Chemstar: motor solution tailored for the chemical industry
The flameproof Siemens low-voltage motor series Simotics XP is now available across the entire power spectrum from 0.25 to 460 kW in gas groups IIB and IIC. Furthermore, with the availability of premium IE3 efficiency, the low-voltage motors are ready for future energy efficiency requirements. In addition, Siemens offers motors with Chemstar technology, which provide a tailored motor solution for the chemical industry with pre-configured, chemical-specific options.
- Simotics S-1FS2 in stainless steel housing with specific features for use in the pharmaceutical and F&B industries
- Servo planetary gearmotors Simotics S-1FK2 for optimum adjustment of speed, torque and mass inertia
- Simotics S-1FT2 in protection class IP67 with 26 bit encoder, higher rated speed and other selectable features
Siemens is adding new servo motors to its proven Sinamics S210 single-cable servo drive system, thereby expanding its range of applications. Specifically, for use in the pharmaceutical and food industries, the company is launching the Simotics S-1FS2, a motor version with a stainless-steel housing, the highest degree of protection IP67/IP69, and high-resolution 22-bit absolute multiturn encoders. The servo motor thus meets all hygienic conditions and can be used for mixing and stirring, air conditioning and ventilating, dosing and filling, as well as conveying, packaging and storing a wide variety of end products in the food and beverage sector and in the pharmaceutical industry.
- Siemens Large Drives Applications (LDA) to deliver a high voltage (HV) motor with 105 MW and a 40 MW starting frequency converter for an energy storage project in China
- The motor will have an efficiency of beyond 98 percent
Siemens LDA has received an order from a Chinese customer to deliver a special machine with dual shaft extension. It can be used in motor operation with a power of 105 MW and as generator with up to 129 MVA in power generation mode. The motor will have an efficiency of beyond 98 percent and will be a world-leading 2-pole electric motor.Beside the motor, the contract includes the delivery of a 40 MW Sinamics GL150 starting frequency converter. This LCI-converter (load commutated inverter) is designed for single-motor applications with variable and constant torque characteristics. As a result of the low switching losses and the low loss thyristor technology, the efficiency of the LCI converter is extremely high and lies at 99 percent.
- Analyze MyDrives Edge with new feature to optimize energy consumption
- Analyze MyDrives Edge is part of Siemens Xcelerator
- New compact DC/DC converter Sinamics DCP 250 kW
In the field of
energy-efficient and sustainable drive technology, Siemens is bringing two
innovations to this year's Smart Production Solutions (SPS) trade fair in
Nuremberg. The first innovation relates to the Analyze MyDrives Edge
application, which is already established on the market. This is equipped with
a new feature that ensures transparency regarding the energy consumption of the
entire drive system. The AI-based feature of the Edge app calculates all data
without the need for additional sensors and special measuring devices. The app
shows how efficiently the drive runs, how high energy consumption and operating
costs are and what carbon footprint the drive leaves behind. Drive settings can
thus be optimized even better to customer needs.
- Sinamics DriveSim Advanced expands the Industrial Operations X offering, part of the Siemens Xcelerator digital business platform
- Sinamics DriveSim Advanced simulation software for virtual engineering and commissioning of drive constellations
- Complete digital twin of Sinamics drives with all parameters and configurations
- Extending digitalization of drive technology continuously enables machine builders to reduce resource consumption and optimize energy efficiency
At this year's Hannover
Messe, Siemens is presenting Sinamics DriveSim Advanced, an extended simulation
software for drive constellations that can be used for both engineering and
commissioning on the basis of a digital twin. Sinamics DriveSim
Advanced thus expands the simulation portfolio for motion control drives at
Siemens, which was introduced to the market in 2021 with Sinamics DriveSim
Basic. At the same time, Sinamics DriveSim Advanced adds to the Industrial Operations X offering. With Industrial Operations X, Siemens offers a continuously growing interoperable portfolio of products and services for production engineering, execution, and optimization. This offering brings more information technology (IT) and software capabilities to automation and production operations, making industrial operations more adaptable. The Industrial Operations X portfolio is characterized by supporting an open ecosystem, being flexible with modular and scalable functions, and enabling interoperable, seamless, holistic production value chains.
- Predictive Service Analyzer provides information about anomalies in the drive system
- Increased plant availability by up to 30 percent through reduced production downtime
- AI-based algorithm for drive systems
As part of Predictive
Services for Drive Systems, Siemens is expanding its offering at the Hannover
Messe with an edge application. The Predictive Service Analyzer indicates
defects in the drive system at an early stage before they affect the entire
production. As a result, unplanned production downtime can be avoided and
maintenance times can be scheduled in good time, increasing plant availability
by up to 30 percent. By scheduling maintenance and servicing activities based
on actual demand, this increases productivity by up to 10 percent. The Predictive
Service Analyzer's AI-based solution detects early signs of anomalies, such as
those indicating mechanical damage in the motor, including bearing damage,
imbalance, and misalignment, as well as critical operating conditions of the
frequency converter. The app assesses the severity of the defect and the
expected remaining runtime and can thus predict potential future failures.
- Focus on combining the real and the digital worlds
- IIoT: Data-based algorithms increase operational efficiency of plants
- Process optimization and modularization as the key to success
At the "Achema Pulse" live digital event, Siemens will be demonstrating how the combination of the real and the digital worlds empowers industrial companies to act in a versatile and sustainable manner. Companies in the process industry are facing urgent and rapidly changing challenges. The Covid-19 pandemic in particular has transformed demand patterns and global supply chains virtually overnight. At the same time, industry-specific regulations and standards are creating new framework conditions for production. Digitalization and automation are the levers for mastering these changes. Industrial IoT solutions can exploit the resulting data to secure a competitive advantage since the intelligent analysis, understanding and utilization of the data allows companies to adapt their processes faster to changing requirements. The Siemens Digital Enterprise portfolio makes this possible by combining the real world with the digital world, thus enabling solutions for simulation, virtual processes, remote access and connectivity as well as presenting service offerings for digital transformation. Thanks to the corresponding industry-specific know-how, individual sector requirements can be taken into account.
- Siemens industrializes additive manufacturing with polymers with EOS and DyeMansion as partners
- Siemens and EOS support Hexr in the mass customization of additively manufactured bicycle helmets
- Digital Enterprise portfolio offers integrated software and automation solutions for the industrialization of additive manufacturing
- Additive Manufacturing Network – an online order-to-delivery collaboration platform for the industrial additive manufacturing community, helps streamline the AM production process
Siemens' Digital Enterprise portfolio consists of software and automation solutions that optimize process steps along the entire value chain of additive manufacturing. This holistic approach is unique in the field of the industrialization of additive manufacturing. "The automated chain of coordinated production steps from all suppliers, from design and printing to post-processing, as well as end-to-end IT integration, is crucial for high productivity and maximum flexibility. This applies to series parts as well as to a highly flexible lot-size-1 production for individualized products or spare parts," explains Dr. Karsten Heuser, Vice President Additive Manufacturing at Siemens Digital Industries.
- Early detection of anomalies in the drivetrain with the support of artificial intelligence
- Trend Prediction for optimized maintenance efficiency
- Higher productivity and reduced machine and system downtime
Siemens has supplemented the Mindsphere application Predictive Service Assistance with an AI-based module. The new Artificial Intelligence module identifies concrete fault patterns in motors at an early stage, such as misalignment or a defective bearing. The application thus helps users to reduce downtimes and further improve spare parts and maintenance processes. The new Artificial Intelligence module for motors uses a neural network to solve what was previously implemented using a defined KPI limit value. This enables the module to detect anomalies even before the defined limit value and provides clear indications of the type and severity of faults and their development. As soon as the application detects signs of an error, it warns the user and generates a due date that indicates when the error should ideally be corrected and what corrective action is recommended to prevent an unplanned downtime. Predictive Service Assistance with the new AI-based Artificial Intelligence module is offered as part of a Predictive Service Assessment. The package includes a customized configuration service that ensures that the Mindsphere application with the new AI-based module runs optimally according to the customer's requirements.