Please use another Browser

It looks like you are using a browser that is not fully supported. Please note that there might be constraints on site display and usability. For the best experience we suggest that you download the newest version of a supported browser:

Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser

Continue with the current browser

New motors extend the application range of the Sinamics S210 servo drive system

The new Simotics S-1FK2 servo planetary gearmotors complement the Sinamics S210 servo drive system.

The new Simotics S-1FK2 servo planetary gearmotors also complement the Sinamics S210 drive system. They are used when high cycle rates need to be achieved with a lightweight and low-inertia gear design, or when inertia matching is required to move heavy loads precisely. The motors are ready mounted and as a unit available in a wide range of gear ratios and sizes, allowing them to be optimally adapted to different applications. Thermal dimensioning is done via the digital twin in the TIA (Totally Integrated Automation) Selection Tool. 
With the new Simotics S-1FT2, Siemens is launching a servo motor that offers a wide range of different options for the Sinamics S210 servo drive system. For example, encoders with a resolution of up to 26 bits improve system accuracy, and the high IP67 protection rating and various motor coatings make the solution suitable for use in harsher environments. In addition, new machine options, such as higher rated speeds, are available for extended use.
The Sinamics S210 servo drive system consists of a servo converter and servo motor. All motors of the servo system are connected via a single cable that combines power wires, encoder signal and brake in one line. The range of applications includes highly dynamic servo solutions such as those found in handling systems, packaging machines and machine building applications. To meet the high demands on motion control functionality in these applications, for example dynamic positioning, gear synchronization or cams with multiple axes, the system works perfectly with the Simatic S7-1500 controller via Profinet IRT.
For further information regarding the Siemens Digital Enterprise Virtual Experience at Hannover Messe 2021 please see www.siemens.com/press/hm21
For further information regarding Sinamics S210 please see
www.siemens.com/sinamics-s210

For this press release

Press Folders

Follow us on Social Media

Siemens Digital Industries (DI) is an innovation leader in automation and digitalization. Closely collaborating with partners and customers, DI drives the digital transformation in the process and discrete industries. With its Digital Enterprise portfolio, DI provides companies of all sizes with an end-to-end set of products, solutions and services to integrate and digitalize the entire value chain. Optimized for the specific needs of each industry, DI’s unique portfolio supports customers to achieve greater productivity and flexibility. DI is constantly adding innovations to its portfolio to integrate cutting-edge future technologies. Siemens Digital Industries has its global headquarters in Nuremberg, Germany, and has around 76,000 employees internationally.
Read more
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 170 years. Active around the world, the company focuses on intelligent infrastructure for buildings and distributed energy systems and on automation and digitalization in the process and manufacturing industries. Siemens brings together the digital and physical worlds to benefit customers and society. Through Mobility, a leading supplier of intelligent mobility solutions for rail and road transport, Siemens is helping to shape the world market for passenger and freight services. Via its majority stake in the publicly listed company Siemens Healthineers, Siemens is also a world-leading supplier of medical technology and digital health services. In addition, Siemens holds a minority stake in Siemens Energy, a global leader in the transmission and generation of electrical power that has been listed on the stock exchange since September 28, 2020. In fiscal 2020, which ended on September 30, 2020, the Siemens Group generated revenue of €57.1 billion and net income of €4.2 billion. As of September 30, 2020, the company had around 293,000 employees worldwide. Further information is available on the Internet at www.siemens.com.
Read more
Reference Number: HQDIPR202104076168EN

Contact

Katharina Lamsa

Siemens AG

+49 172 8413539