Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release31 March 2021Digital IndustriesNuremberg
High-efficiency motor series from Siemens now consistently available in efficiency class IE4
Simotics SD is offered in Super Premium Efficiency (IE4)
This European directive comes into force in two phases. From July 2021, it requires the efficiency class Premium Efficiency (IE3) for 2- to 8-pole electric motors from 0.75 kW to 1,000 kW. From July 2023, it requires the efficiency class Super Premium Efficiency (IE4) for 2- to 6-pole motors of medium power from 75 kW to 200 kW. In accordance with the regulation, Siemens offers the Simotics SD motor series consistently in IE4 for all affected motors. In addition, however, also for motors with an output of up to 1,000 kW as well as for 8-pole motors from 55 kW, which are still exempt from the second stage from 2023. Users of Simotics motors can thus meet the increasing requirements for energy efficiency and environmental compatibility in the long term.
Highly efficient motors also allow users to save energy, lower their operating costs and reduce CO2 emissions. Such motors are typically used in the process industry for pumps, fans, compressors, extruders, mixers, agitators, centrifuges, rollers, or winders. This applies primarily to the Water, Wastewater, Chemical, Oil & Gas, Cement, Paper, Marine and Metal processing industries.
The motors of the explosion proof Simotics XP series also exceed the currently required efficiency standards. They are also offered in IE3 and IE4. IE3 is standard in the increased safety (Ex eb) type of protection. This means that the requirements that come into force in 2023 and demand efficiency class High Efficiency (IE2) are also exceeded here. Another example from the Simotics portfolio is the Simotics reluctance motor. This motor is characterised by the highest efficiency levels, comparable to IE4, even in the partial load range. In the system with a Sinamics converter, it exceeds the minimum requirements of the highest defined system efficiency class IES2.
Highly efficient motor technologies can sustainably reduce the energy demand of industry and contribute to lowering global CO2 emissions. After all, according to the German Electrical and Electronic Manufacturers' Association (ZVEI), around 70 percent of the energy demand in industry is required by electric motors.
For further information regarding the Siemens Digital Enterprise Virtual Experience at Hannover Messe 2021 please see
www.siemens.com/press/hm21
www.siemens.com/press/hm21
For further informaiton regarding the ErP Directive please see
https://new.siemens.com/global/en/products/drives/topic-areas/energy-efficiency.html
https://new.siemens.com/global/en/products/drives/topic-areas/energy-efficiency.html
For this press release
Follow us on Social Media
Siemens Digital Industries (DI) is an innovation leader in automation and digitalization. Closely collaborating with partners and customers, DI drives the digital transformation in the process and discrete industries. With its Digital Enterprise portfolio, DI provides companies of all sizes with an end-to-end set of products, solutions and services to integrate and digitalize the entire value chain. Optimized for the specific needs of each industry, DI’s unique portfolio supports customers to achieve greater productivity and flexibility. DI is constantly adding innovations to its portfolio to integrate cutting-edge future technologies. Siemens Digital Industries has its global headquarters in Nuremberg, Germany, and has around 76,000 employees internationally.
Siemens AG (DI) (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 170 years. Active around the world, the company focuses on intelligent infrastructure for buildings and distributed energy systems and on automation and digitalization in the process and manufacturing industries. Siemens brings together the digital and physical worlds to benefit customers and society. Through Mobility, a leading supplier of intelligent mobility solutions for rail and road transport, Siemens is helping to shape the world market for passenger and freight services. Via its majority stake in the publicly listed company Siemens Healthineers, Siemens is also a world-leading supplier of medical technology and digital health services. In addition, Siemens holds a minority stake in Siemens Energy, a global leader in the transmission and generation of electrical power that has been listed on the stock exchange since September 28, 2020. In fiscal 2020, which ended on September 30, 2020, the Siemens Group generated revenue of €57.1 billion and net income of €4.2 billion. As of September 30, 2020, the company had around 293,000 employees worldwide. Further information is available on the Internet at
www.siemens.com.