[{"name":"Home","site_name":"Press | Company | Siemens","description":"","url_str":"\/global\/","level":0,"image":"","base_root":"https:\/\/press.siemens.com","base_nid":"5","base_nodepath":"\/node\/5","base_path":"\/global\/","base_secure_url":"https:\/\/press.siemens.com\/global","children":null}]
[]
Please use another Browser
It looks like you are using a browser that is not fully supported. Please note that there might be constraints on site display and
usability.
For the best experience we suggest that you download the newest version of a supported browser:
Press Release09 June 2021Digital IndustriesNuremberg
Siemens expands motor portfolio for the
process industry
Simotics XP motors from 0.25 to 460 kW available in gas groups IIB
und IIC
Premium efficiency class for all motors
Chemstar: motor solution tailored for the chemical industry
The flameproof Siemens low-voltage motor series Simotics XP is now available across the entire power spectrum from 0.25 to 460 kW in gas groups IIB and IIC. Furthermore, with the availability of premium IE3 efficiency, the low-voltage motors are ready for future energy efficiency requirements. In addition, Siemens offers motors with Chemstar technology, which provide a tailored motor solution for the chemical industry with pre-configured, chemical-specific options.
Simotics XP motors from 0.25 to 460 kW available in gas groups IIB
und IIC
Premium efficiency class for all motors
Chemstar: motor solution tailored for the chemical industry
The flameproof Siemens low-voltage motor series Simotics XP is now available across the entire power spectrum from 0.25 to 460 kW in gas groups IIB and IIC. Furthermore, with the availability of premium IE3 efficiency, the low-voltage motors are ready for future energy efficiency requirements. In addition, Siemens offers motors with Chemstar technology, which provide a tailored motor solution for the chemical industry with pre-configured, chemical-specific options.
The flameproof motors of the Siemens Simotics XP low-voltage motor series are now available across the entire power spectrum from 0.25 to 460 kW in gas groups IIB and IIC.
According to explosion protection in zone 1
gas, the use of Simotics XP motors in the IIB version is possible. If hydrogen or acetylene are present, the IIC version is required. Both versions, IIB and IIC, are characterized by robustness, high
availability, and a consistent platform concept. In addition, further options
are available for the motors: Premium insulation enables speed-controlled
operation with any converter with output voltages up to 690 V without any
filter. Variants with reduced starting currents and the availability of the
wide range of options with monitoring by PTC sensors (PTC thermistors) and
PT100 (thermometers), with specific painting systems and modular attachments,
such as speed encoders and brakes, complete the portfolio.
All common types of protection are covered by the consistent and integrated Simotics XP platform for explosion-proof motors and can be easily configured and adapted using the Drive Technology Configurator provided by Siemens. Simotics XP motors offer plant operators and machine builders a simple spare parts inventory, standardized tools, and ordering processes.
They run reliably and trouble-free under extreme operating conditions in aggressive atmospheres, both on the mains and on the frequency converters, and meet the requirements of the new, stricter EU Ecodesign Directive (ErP). From July 2021, the high energy efficiency class IE3 is also required for explosion-proof motors. The Simotics XP portfolio is available in energy efficiency class IE3 and in major parts also in energy efficiency class IE4. Motors with increased safety in the Ex eb version must meet energy efficiency class IE2 from July 1, 2023. IE3 is already standard for Simotics XP motors in the Ex eb version.
Chemstar concept – Tailord to the chemical and oil & gas industry
As a specific offering for the chemical and oil & gas industries, Siemens offers not only the explosion-proof motors of the Simotics XP series, but also motors of the Simotics SD series for environments without explosion hazard in the Chemstar version. They are equipped with pre-configured chemical-specific options, for example, fan shroud in steel plate, reinforced bearing, external grounding, IP66 protection, premium insulation system, VIK design and painting up to class CX according to ISO12977-2:2018 for the complete color spectrum including non-standard shades. Both motor series, available with options, operate reliably and energy-efficiently even under extreme conditions and offer all relevant certificates.
Siemens Digital Industries (DI) is an innovation leader in automation and digitalization. Closely collaborating with partners and customers, DI drives the digital transformation in the process and discrete industries. With its Digital Enterprise portfolio, DI provides companies of all sizes with an end-to-end set of products, solutions and services to integrate and digitalize the entire value chain. Optimized for the specific needs of each industry, DI’s unique portfolio supports customers to achieve greater productivity and flexibility. DI is constantly adding innovations to its portfolio to integrate cutting-edge future technologies. Siemens Digital Industries has its global headquarters in Nuremberg, Germany, and has around 76,000 employees internationally.
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 170 years. Active around the world, the company focuses on intelligent infrastructure for buildings and distributed energy systems and on automation and digitalization in the process and manufacturing industries. Siemens brings together the digital and physical worlds to benefit customers and society. Through Mobility, a leading supplier of intelligent mobility solutions for rail and road transport, Siemens is helping to shape the world market for passenger and freight services. Via its majority stake in the publicly listed company Siemens Healthineers, Siemens is also a world-leading supplier of medical technology and digital health services. In addition, Siemens holds a minority stake in Siemens Energy, a global leader in the transmission and generation of electrical power that has been listed on the stock exchange since September 28, 2020.
In fiscal 2020, which ended on September 30, 2020, the Siemens Group generated revenue of €57.1 billion and net income of €4.2 billion. As of September 30, 2020, the company had around 293,000 employees worldwide. Further information is available on the Internet at
www.siemens.com.