Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release13 April 2023Digital IndustriesNuremberg
Siemens to add new simulation software for drives to Industrial Operations X offering

Siemens is presenting Sinamics DriveSim Advanced, an extended simulation software for drive constellations that can be used for both engineering and commissioning on the basis of a digital twin.
In this context, Siemens
offers Sinamics DriveSim Advanced, a comprehensive solution for the simulation
of drives that offers a
realistic simulation of the new Sinamics converters with all their functions. Users
can create a digital twin of the drive in a virtual environment with all the
parameters and configurations that correspond to a real drive. The innovative
technology and user-friendly interface allow users to simulate, commission and
optimize the behavior of drive systems in a virtual environment before building
them in the real world. This significantly increases efficiency and productivity
when optimizing drive systems and machines. With Startdrive, simulation is
integrated directly into TIA Portal, so no additional software tools are
required. Using the digital twin, the logical and functional aspects of the
drive system can be simulated identically to the real Sinamics drives, while
electrical, magnetic, and mechanical aspects are partially modeled in a
simplified way. The use of virtual commissioning and engineering tools such as
Sinamics DriveSim Advanced thus enables machine builders to reduce resource
consumption and optimize energy efficiency, leading to a more sustainable
approach to machine building.
Shaping the future of production sustainably with energy-efficient drives
With the continuous
expansion of its digitalization portfolio in the area of drive technology,
Siemens is responding to the current needs of industry for greater
sustainability. Electric motors are responsible for over 70 percent of
industrial energy demand. Simotics SD IE4 motors and IE5 motors are already
very energy-efficient with an efficiency of up to over 96 percent and are
therefore also optimally designed for operation directly on the grid. By using
motors of the very high efficiency classes IE4 and IE5, savings of 6 percent of
electrical energy on average are possible. Using perfectly matched motor and
drive systems for variable-speed operation of pumps, fans and compressors,
energy savings of 30 percent on average can be achieved, and in some cases even
more. The real key to greater energy efficiency, however, lies in the overall
system: In the interaction of all individual measures - from more efficient
motors with variable-speed control, to digital system components and tools, to
the use of electrically buffered energy in the motor network - savings of 60
percent on average can be achieved in the system network.
Further
information on Siemens at Hannover Messe 2023 at
www.siemens.com/press/hm23 and www.siemens.com/hannover-messe
www.siemens.com/press/hm23 and www.siemens.com/hannover-messe
For this press release
Follow us on our social media channels
Siemens Digital Industries (DI) is an innovation leader in automation and digitalization. Closely collaborating with partners and customers, DI drives the digital transformation in the process and discrete industries. With its Digital Enterprise portfolio, DI provides companies of all sizes with an end-to-end set of products, solutions, and services to integrate and digitalize the entire value chain. Optimized for the specific needs of each industry, DI’s unique portfolio supports customers to achieve greater productivity and flexibility. DI is constantly adding innovations to its portfolio to integrate cutting-edge future technologies. Siemens Digital Industries has its global headquarters in Nuremberg, Germany, and has around 72,000 employees internationally.
Siemens AG (Berlin and Munich) is a technology company focused on industry, infrastructure, transport, and healthcare. From more resource-efficient factories, resilient supply chains, and smarter buildings and grids, to cleaner and more comfortable transportation as well as advanced healthcare, the company creates technology with purpose adding real value for customers. By combining the real and the digital worlds, Siemens empowers its customers to transform their industries and markets, helping them to transform the everyday for billions of people. Siemens also owns a majority stake in the publicly listed company Siemens Healthineers, a globally leading medical technology provider shaping the future of healthcare. In addition, Siemens holds a minority stake in Siemens Energy, a global leader in the transmission and generation of electrical power.
In fiscal 2022, which ended on September 30, 2022, the Siemens Group generated revenue of €72.0 billion and net income of €4.4 billion. As of September 30, 2022, the company had around 311,000 employees worldwide. Further information is available on the Internet at www.siemens.com.
In fiscal 2022, which ended on September 30, 2022, the Siemens Group generated revenue of €72.0 billion and net income of €4.4 billion. As of September 30, 2022, the company had around 311,000 employees worldwide. Further information is available on the Internet at www.siemens.com.
Reference Number: HQDIPR202304116676EN