- Continuous dimming of LEDs and other lamps
- Powerful lighting control of up to 1000 volt-amperes (VA) and adjustable dimming sequences
- KNX DIN rail-mounted device with integrated front operating panel
The Siemens Building Technologies Division has updated its GAMMA instabus product line with the powerful new KNX based universal dimmer N 554. This universal dimmer can be used to control LED and other lamps up to a total 1000 VA, making it perfect for advanced lighting solutions in cinemas, theaters, opera houses, museums and hotels. The device features continuous dimming, the dimming sequences can be adjusted to the behaviors of the different lamps. Manual testing of the lighting installation from the integrated panel saves time.
- Siemens to design, supply and build onshore substation and offshore transformer modules (OTM®)
- Triton Knoll is the 10th UK offshore wind farm Siemens has connected to the mainland
- After completion Triton Knoll would be able to provide sufficient clean and sustainable power for the equivalent of 800,000 British homes
Siemens Energy Management has received an order to design, supply and build the grid connection for the Triton Knoll offshore wind farm by German customer Innogy SE. The wind farm, 32 kilometers (km) off the Lincolnshire coast, will have an installed generation capacity of circa 860 megawatts (MW) after its completion. Triton Knoll will be capable of providing sufficient clean and sustainable power for the equivalent of at least 800,000 British homes, making a significant contribution to the UK's renewable energy targets. Siemens will lead on the construction of a new four-hectare onshore substation at Bicker Fen, as well as offshore infrastructure, including two Offshore Transformer Modules (OTM ®). The Siemens OTM® is significantly smaller in size and weight compared to conventional alternating current platforms and highlight Siemens' commitment to helping power developers improve efficiencies and the delivery program.
- Service on non-electrified rail lines
- Passenger tests planned in second half of 2019
- Eco-friendlier operation with up to 50 percent less CO2 emissions than with diesel engines
Austrian Federal Railways (ÖBB) and Siemens Mobility are jointly investing in the future of passenger transport and are developing an electro-hybrid battery drive for trains. Today, both companies presented in Vienna the first result of this innovative pilot project, the prototype of the Desiro ML Cityjet eco. Operating as a battery-powered train, the Cityjet eco is an alternative for non-electrified rail lines primarily served at present with diesel-powered passenger trains. Battery operation can reduce CO2 emissions by up to 50 percent compared to diesels. Following extensive testing of the train, it is expected to first be used in passenger service in the second half of 2019. The prototype will be presented on track 1/400 in the outdoor exhibition area at the InnoTrans 2018, the leading international trade fair for transport technology, being held in Berlin on September 18-21.
- Siemens Intelligent Traffic Systems will provide connected vehicle technology and smart traffic control infrastructure to the American Center for Mobility for automated and connected vehicle testing.
The American Center for Mobility (ACM) is excited to announce its second partnership with Siemens. Siemens Intelligent Traffic Systems (ITS) will now provide approximately $1 million in state-of-the-art ITS infrastructure, software, and engineering support to aid ACM in developing real-world testing and validation of connected and automated vehicles (CAVs). The newest agreement between Siemens and ACM adds physical infrastructure, software applications, and analytics to the Virtual Simulation and Testing solutions provided by Siemens PLM, announced earlier this year. Under the terms of this new agreement Siemens ITS will also have a seat on ACM’s Industry Advisory Board (IAB).
- Rail Service Center inaugurated in Dortmund-Eving, Germany
- Digitalized service and maintenance of RXX trainsets for 32 years
- Contract specifies over 99 percent availability of RRX trains
Today, after one-and-a-half years of construction, Siemens Mobility is officially inaugurating the new maintenance depot for the Rhine-Ruhr Express (RRX). In the future, 75 employees in the Rail Service Center in Dortmund-Eving will service and maintain the 82 electric RXX Desiro HC multiple-unit trains for a period of 32 years. The digitalized and paperless concept ensures that the trains' contractually agreed availability of over 99 percent can be guaranteed.
- Demand for bonds with a total value of €2.75 billion and maturities of five, nine and twelve years 2.5 times higher than issue volume
- Placement directly after summer lull secures favorable financing conditions
After a five-year absence, Siemens has made an impressive return to the euro capital market. For its new bonds, the company generated very strong demand of €6.8 billion. Siemens issued bonds with a total value of €2.75 billion and maturities of five, nine and twelve years. The high demand enabled Siemens to obtain very good interest-rate conditions over all maturities. At the time of price fixing, the average issue yield for all three maturities was 20 basis points (0.2 percentage points) below the initial indications.
- Scalable uniform-topology power supply and drive solutions
- Customized configuration based on practically tested, standardized components such as Sinamics
- High level of resilience, availability and service friendliness
- Up to zero emissions depending on drive configuration
Siemens is expanding its portfolio of green ship propulsion systems by adding a new member to the Siship BlueDrive Family: Siship BlueDrive Eco. Besides by integrating battery systems produced in-house, the company is now able to offer a scalable and flexible solution to cover every propulsion requirement, with different power graduations for small to medium-sized propulsion systems from 5 kilowatts (kW) in auxiliary mode up to 5.5 megawatts (MW) for the main drive – from Siship BlueDrive Eco through to Siship BlueDrive PlusC. The solutions can be configured to individual customer specifications and are based on practically tested standardized components such as Sinamics converters. With its Siship BlueDrive, Siemens provides an efficient, environmentally friendly propulsion solution providing a high level of reliability, availability and service friendliness, with emissions down as low as zero depending on the drive configuration.
- Joint research and development project with ViP Verkehrsbetriebe Potsdam GmbH
- World premiere at InnoTrans 2018
- Demonstration runs in real traffic
Siemens Mobility, together with ViP Verkehrsbetrieb Potsdam GmbH, will be presenting their research project on the world's first autonomous tram at InnoTrans 2018. On a six-kilometer section of the tram network in Potsdam, Germany, Siemens Mobility will be demonstrating a test tram driving autonomously in real traffic on September 18 through 21.
- Around 2,170 apprentices and work-study program participants begin their professional life at 20 Siemens locations
- Training further aligned to the requirements of digitalization
- 27 participants in international training program in Berlin
Around 2,170 young people will begin their vocational training next Monday at 20 Siemens locations in Germany alone. Siemens will be training about 1,530 for careers at the company, while a further 640 are from external partners. The ongoing digitalization of the work environment is playing an increasingly important role at Siemens – and in the company's training programs as well. What began in "apprentice corners" back in 1891 is being continued today at advanced, innovative training centers.