- Efficient power transmission in the range from 30 to 150 megawatts
- Functions as direct-current transmission line (DC) to control, optimize, and regulate load flows in medium-voltage alternating current grids (AC)
- Based on Siemens high-voltage direct-current transmission (HVDC) technology
With MVDC PLUS (Medium Voltage Direct Current Power Link Universal System), Siemens is introducing a new direct-current transmission system to the market that will be serve as an efficient transmission route in medium-voltage AC grids from 30 to 150 kilovolts (kV). Siemens has developed the transmission system for grid operators who need to enlarge their infrastructure to handle the increasing volumes of power fed into the distribution system from distributed and renewable energy sources and also keep their network stable. Distances of up to 200 kilometers can be bridged with MVDC PLUS. Siemens offers the medium-voltage DC transmission system as a compact system in three variants: for a transmission capacity of approximately 50, 100, and 150 megawatts (MW) at DC transmission voltages of 20 to 50 kV.
- MindSphere interface offers value added by using recorded data over and above its actual protection and automation functions
- Data is fed to MindSphere applications through a separate communications channel, for example, to be used in asset management
Today's digital protection devices like those in the Siemens Siprotec 5 series record a multitude of different measured values and network condition quantities. Adding to the devices' actual protection and automation functions, these values can be extremely useful for utilities and grid operators, for example for asset management. That's why Siemens will equip its Siprotec 5 devices with a MindSphere interface, which will be available approximately in the middle of 2018. Through this integrated interface data can be fed, for instance, to a MindSphere application for asset management. Siprotec 5 uses a separate communications path for data read-out and transmission in addition to communications with the power station's automation and control system. There's only one data read access, and it doesn't affect the function of the protection device.
Sabrina Soussan (48) and Michael Peter (51) have been appointed to succeed Jochen Eickholt (55) as head of Siemens' Mobility Division, effective October 1, 2017. Eickholt has been appointed integration manager for the announced merger of Siemens' and Alstom's mobility businesses, effective the same date.
- Siemens to supply power island with highly-efficient H-class gas turbines
- Around 1.3 gigawatts power generation capacity
- Fast track power generation project to boost capacity in Punjab Province
Siemens has received an order from Pakistan for a complete power island for the new combined cycle Punjab Power Plant Jhang. The order was placed by the China Machinery Engineering Corporation (CMEC). As EPC contractor the Chinese company is building the project for the independent energy provider Punjab Thermal Power (Pvt) Ltd (PTPL). The liquefied natural gas (LNG)-operated plant is being built 250 kilometers southwest of Lahore and will provide a power generating capacity of 1.3 gigawatts.
- Digitalization of low-flow measurement
- Sensor program expansion with DN100 and DN150
- Transmitter with Modbus and Profibus PA profile 4.0 communication
- Suitable for new applications in oil and gas, marine, and chemical
To extend the numerous process-optimizing advantages of the digital Coriolis flowmeter platform to low-flow applications such as batching, dosing and filling of both liquids and gases, the Sitrans FCT030 and FCT010 digital transmitters can now be paired with the Sitrans F C MASS 2100 and Sitrans FC300 Coriolis sensors for small line sizes from DI 1.5 to DN 15. With this major enhancement to the product line, a broad range of users from chemical to automotive applications can benefit from market-leading mass flow accuracy of 0.1%, density accuracy of 0.5 kg/m3 and 100 Hz signal processing. The high-speed update rate ensures the highest precision for applications such as the filling of beverage bottles.
- Signed Memorandum of Understanding grants exclusivity to combine mobility businesses in a merger of equals
- Listing in France and group headquarters in Paris area; led by Alstom CEO with 50 percent shares of the new entity owned by Siemens
- Business headquarter for Mobility Solutions in Germany and for Rolling Stock in France
- Comprehensive offering and global presence will offer best value to customers all over the world
- Combined company's revenue €15.3 billion, adjusted EBIT of €1.2 billion
- Annual synergies of €470 million expected latest four years after closing
Today, Siemens and Alstom have signed a Memorandum of Understanding to combine Siemens' mobility business including its rail traction drives business, with Alstom. The transaction brings together two innovative players of the railway market with unique customer value and operational potential. The two businesses are largely complementary in terms of activities and geographies. Siemens will receive newly issued shares in the combined company representing 50 percent of Alstom's share capital on a fully diluted basis.
China's largest acrylic producer, Zhejiang Satellite Energy Co., Ltd, recently selected Siemens to provide a reactor effluent compressor train for Phase II of its propane dehydrogenation (PDH) plant in Pinghu City in China's Zhejian province. The dual-casing compressor train, scheduled for installation in late 2018, consists of two Siemens STC-SH single-shaft compressors driven by a Siemens SGT-750 industrial gas turbine. Plant commissioning is scheduled for early 2019.
- Digitalization allows machine manufacturers to develop new business models
- Openness of MindSphere has an important role to play for machine manufacturers
- Siemens connects 240 machine tools with "Manage MyMachines" on MindSphere across the whole exhibition site
At the EMO 2017, Siemens is demonstrating the various connection and installation options of its high-performance and open cloud-based IoT operating system MindSphere for applications in the machine tool sector. The company is connecting over 240 different machine tools from over 140 manufacturers across the whole exhibition site using its "Manage MyMachines" app on MindSphere. In addition to this, machine manufacturers such as Heller are presenting new services and business models based on MindSphere to, for example, increase efficiency and productivity.
- System offers data transmission rates of up to 2.5 megabit per second
- Replaces traditional systems and can be seamless integrated into existing power line carrier infrastructure
Siemens launches PowerLink IP, a new power line carrier (PLC) system for digital high-voltage substations. This brand new PLC system uses the high-voltage lines between the substations as a channel by overlaying a modulated carrier frequency on the frequency of the transmission voltage in the overhead lines. State-of-the-art, digital substations generate ever-increasing volumes of data that are used to ensure reliable network operation. With PowerLink IP, power grid operators can enjoy the benefits of digitalization for Ethernet/IP communication via overhead lines. Siemens provides proven PLC technology for this purpose – technology which meets the demand for more bandwidth and ensures that the constantly growing volumes of data in high-voltage substations can be used for efficient grid operation.
- Greatly expanded product line of GAMMA instabus switching actuators for lighting and electrical loads
- Numerous control, override and diagnostic functions
- Much shorter installation time, simplified commissioning, lower maintenance costs
The Siemens Building Technologies Division has updated its GAMMA instabus product line with new switching actuators, greatly expanding its range of products for lighting control. The new actuators are available with switching capacities of 6, 10 and 16 or 20 amperes and four, eight and twelve channels each.