Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release04 October 2017Energy ManagementErlangen
Siemens protection device offers use of the internet of things via MindSphere of energy
Siemens Siprotec 5 devices with a MindSphere interface
MindSphere, the Siemens cloud-based, open operating system for the Internet of Things (IoT), regulates communications with the connected protection devices and controls data administration. It also makes the data available to MindSphere applications, which is where the value added lies. In addition to standard data exchange formats, MindSphere also offers users a variety of services that makes it possible to create and implement in-house, vendor-neutral applications.
For example, an application could be created to monitor circuit breakers based on data collected from the protection devices. The usual data produced by circuit breakers – including short-circuit energy (I2t) and number of switching cycles – could be processed by a MindSphere application. Using this data in conjunction with values from comparable circuit breakers, grid operators could more effectively plan and optimize breaker maintenance.
For example, an application could be created to monitor circuit breakers based on data collected from the protection devices. The usual data produced by circuit breakers – including short-circuit energy (I2t) and number of switching cycles – could be processed by a MindSphere application. Using this data in conjunction with values from comparable circuit breakers, grid operators could more effectively plan and optimize breaker maintenance.
MindSphere uses technologies and mechanisms that ensure that only data from the stations and connected devices registered in the operating system are processed. This is possible thanks to a multilayer security concept that's based on modern processes, standards, and services that allow it to provide the necessary data security in line with the current state of the art. This will transform MindSphere into a powerful IoT ecosystem for the energy industry that offers an ever-increasing number of applications for power supply companies and network operators.
At Siemens, the Energy Management Division brings together its extensive IoT-portfolio of software and digital services under "MindSphere for Energy." The portfolio combines the topics of MindSphere and energy. It is designed to enable power utilities and grid operators to benefit from the impact of the Internet of Things on the energy sector. Siemens thus offers an IoT portfolio with a unique depth, breadth, and openness. This special depth of offerings is based on the outstanding domain knowledge of Siemens in terms of the ability to connect all devices, systems, and installations in power grids to MindSphere. Yet it also represents a wide range of industry-specific applications from the established EnergyIP series, with 75 million licenses for intelligent meters sold worldwide. The special range of offerings include end-to-end solutions for sector coupling and cross-industry application fields such as intelligent e-mobility network solutions or the integration into factory automation. Last but not least, an open platform and an open partner ecosystem are available so that, for example, third parties can also develop MindSphere applications.
For further information on Siprotec 5, please see www.siemens.com/siprotec5
More press material on EUW 2017 is available at www.siemens.com/press/euw2017
For further information on Division Energy Management, please see www.siemens.com/energy-management
For this press release
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 165 years. The company is active in more than 200 countries, focusing on the areas of electrification, automation and digitalization. One of the world's largest producers of energy-efficient, resource-saving technologies, Siemens is a leading supplier of efficient power generation and power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. The company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2016, which ended on September 30, 2016, Siemens generated revenue of €79.6 billion and net income of €5.6 billion. At the end of September 2016, the company had around 351,000 employees worldwide. Further information is available on the Internet at www.siemens.com.
Contact
Dietrich Biester
Siemens AG
Freyeslebenstr. 1
91058 Erlangen
Germany
91058 Erlangen
Germany
+49 (9131) 7-33559