Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release04 October 2017Energy ManagementErlangen
Siemens introduces DC transmission system for medium voltage to the market
The picture shows the direct-current transmission system MVDC PLUS from Siemens.
This makes MVDC PLUS suitable for connecting small communities in sparsely populated regions to the grid, and for connecting and stabilizing low-power distribution grids regardless of their voltage and frequency. This system enables a regulated power exchange between regional medium-voltage networks and microgrids. It also has greater independence from the high-voltage network. Cables as well as overhead lines can be used for transmission. It's also possible to use existing routes when it's necessary to increase power capacity without needing to move up to high-voltage level.
The transmission system also allows operators to set up a power link between islands or offshore platforms and the mainland in order to avoid maintenance measures and costs for a diesel generator backup. For example, the system can be used as a backup solution for medium voltage in the production industry, where it increases the availability of machines and equipment and reduces production losses. As a backup power supply for data centers, MVDC PLUS ensures, for example, classification in a quality stage ("tier"). The medium-voltage DC transmission system is also attractive because of its cost efficiency and the short implementation time for combinations at the local level with different financing models, which are increasing in importance in countries that have a growing proportion of renewable and distributed energy sources.
MVDC technology is based on the HVDC PLUS technology used in the Siemens HVDC transmission system, but is reduced to its basic functions. Like HVDC PLUS, the medium-voltage transmission system operates with voltage-source converters (VSC) in a modular multilevel converter design (MMC) that convert alternating current into direct current and vice versa. The current on the transmission route can flow in both directions. Thanks to the use of insulated-gate bipolar transistors (IGBT), the commutation processes in the converter run independent of the network voltage. Both converter stations can be operated as a static synchronous compensator (statcom). The extra high-speed control and protection intervention capabilities of the converters ensure the stability of the transmission system, which reduces network faults and malfunctions in the three-phase grid. This significantly improves the security of supply for energy suppliers and energy customers alike.
For further information on MVDC PLUS, please see www.siemens.com/mvdc
More press material on EUW 2017 is available at www.siemens.com/press/euw2017
For further information on Division Energy Management, please see www.siemens.com/energy-management
For this press release
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 165 years. The company is active in more than 200 countries, focusing on the areas of electrification, automation and digitalization. One of the world's largest producers of energy-efficient, resource-saving technologies, Siemens is a leading supplier of efficient power generation and power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. The company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2016, which ended on September 30, 2016, Siemens generated revenue of €79.6 billion and net income of €5.6 billion. At the end of September 2016, the company had around 351,000 employees worldwide. Further information is available on the Internet at www.siemens.com.
Contact
Dietrich Biester
Siemens AG
Freyeslebenstr. 1
91058 Erlangen
Germany
91058 Erlangen
Germany
+49 (9131) 7-33559