Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release28 September 2017Process Industries and DrivesNuremberg
Siemens enhances digital Coriolis flow portfolio for process optimization

The product scope has been further broadened to incorporate larger line sizes often employed by oil and gas, marine, and chemical operations. Already available in sizes DN 15 to DN 80, the Sitrans FCS400 sensor program has now grown to include sizes DN 100 and DN 150. As a result, the FCS400 portfolio is suitable for a broader spectrum of applications ranging from OEM skids and control loops in the hygienic industries to on/offshore custody transfer, bunkering and bulk chemical measurement. The FCS400 is one of the most compact Coriolis sensors on the market, featuring a robust frame immune to process noise and a variety of customizable process connectors for standard, hygienic and NAMUR applications.
Several additional advancements to the transmitter line have been implemented to provide greater flexibility in installation and simplicity in operation. The FCT030 now offers a wall-mount enclosure that enables remote configurations complemented by the option for Modbus or PROFIBUS DP/PA digital communication, an ideal protocol for processes requiring fast data exchange. The fully graphical Human-Machine Interface (HMI), which already featured an intuitive menu structure and multiple setup wizards, has been redesigned with an even easier-to-navigate layout. The innovative SensorFlash® microSD card has also been enriched with an advanced datalogging and audit trail feature, which automatically stores up to 100 records per log of process parameters, diagnostic parameters or changes made to device settings. This function allows operators to analyze the performance of each process and address any potential issues, resulting in optimized plant efficiency and higher-quality end products.
For more information, please see www.siemens.com/coriolis
For more information, please see www.siemens.com/coriolis
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 165 years. The company is active in more than 200 countries, focusing on the areas of electrification, automation and digitalization. One of the world's largest producers of energy-efficient, resource-saving technologies, Siemens is a leading supplier of efficient power generation and power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. The company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2016, which ended on September 30, 2016, Siemens generated revenue of €79.6 billion and net income of €5.6 billion. At the end of September 2016, the company had around 351,000 employees worldwide. Further information is available on the Internet at www.siemens.com.
Contact
David Petry
Siemens AG
Werner-von-Siemens-Str. 65
91052 Erlangen
Germany
91052 Erlangen
Germany
+49 (9131) 7-26616