- New Simotics HV M slipring motors provide range of power up to 4.5 MW
- Easy integration into SIDRIVE IQ applications for highest availability, serviceability, productivity and efficiency
- Easy plant integration due to 3-D Motor models to speed up complete plant integration processes
- Certified and proven Siemens MICALASTIC® VPI insulation system with extreme long lifetime
Building on more than a century of experience in manufacturing slipring motors, Siemens today announces the new Simotics HV M slipring motor. Designed and engineered for applications mainly in the cement and mining industries, the newest slipring motor is implemented in a wide range of applications including but not limited to mills, crushers, conveyors and fans. The new platform motor with its power range up to 4.5 MW completes the Siemens slipring motor family which covers now the power range from 0.5 to 8.2 MW.
- Real-time transmission over Profinet and Pulse Train
- Absolute single-turn encoder with resolution of up to 21 bits for greater efficiency
- New motor design for better connectivity
The user-friendly servo drive system Sinamics V90 from Siemens is particularly suited as a solution for highly dynamic applications. The system comes not only in the form of a high-inertia variant with 400 volts (V) for applications requiring smooth operation, but also as a 200 V version with low inertia motors where highly dynamic performance is called for. Fitted with either Pulse Train (PTI) or Profinet, the motion/process data and diagnostic data can be transmitted in real time between Sinamics V90 and Simatic PLCs. The low inertia motor now features an additional absolute single-turn encoder with a resolution of up to 21 bits, allowing it to determine unequivocal position values and so ensure the great positioning accuracy in the applications.
- Simotics SD motor series from Siemens is now consistently available in efficiency class Super Premium Efficiency (IE4)
- Exceeds increasingly stringent requirements of ErP Directive 2019/1781, which takes effect in two steps in July 2021 and July 2023
- Users can meet long-term efficiency standards, save energy, lower operating costs, and reduce CO2 emissions
Siemens is presenting the Simotics SD motor series as part of the Digital Enterprise Virtual Experience at the Hannover Messe 2021. The standard version of Simotics SD is offered in the efficiency class Super Premium Efficiency (IE4) across the entire power spectrum from 2.2 to 1,000 kW and for the number of poles 2, 4, as well as from 75 kW for 6 poles and from 55 kW for 8 poles. Simotics SD in IE4 thus exceeds the so-called ErP Directive 2019/1781 (energy-related products) – both the first stage, which will be valid by July 2021, as well as the next, which will apply from July 2023. The directive defines the eco-design requirements for electric motors and speed control systems.
- Simotics XP motors from 0.25 to 460 kW available in gas groups IIB
und IIC
- Premium efficiency class for all motors
- Chemstar: motor solution tailored for the chemical industry
The flameproof Siemens low-voltage motor series Simotics XP is now available across the entire power spectrum from 0.25 to 460 kW in gas groups IIB and IIC. Furthermore, with the availability of premium IE3 efficiency, the low-voltage motors are ready for future energy efficiency requirements. In addition, Siemens offers motors with Chemstar technology, which provide a tailored motor solution for the chemical industry with pre-configured, chemical-specific options.
- Simotics S-1FS2 in stainless steel housing with specific features for use in the pharmaceutical and F&B industries
- Servo planetary gearmotors Simotics S-1FK2 for optimum adjustment of speed, torque and mass inertia
- Simotics S-1FT2 in protection class IP67 with 26 bit encoder, higher rated speed and other selectable features
Siemens is adding new servo motors to its proven Sinamics S210 single-cable servo drive system, thereby expanding its range of applications. Specifically, for use in the pharmaceutical and food industries, the company is launching the Simotics S-1FS2, a motor version with a stainless-steel housing, the highest degree of protection IP67/IP69, and high-resolution 22-bit absolute multiturn encoders. The servo motor thus meets all hygienic conditions and can be used for mixing and stirring, air conditioning and ventilating, dosing and filling, as well as conveying, packaging and storing a wide variety of end products in the food and beverage sector and in the pharmaceutical industry.
- Siemens Large Drives Applications (LDA) to deliver a high voltage (HV) motor with 105 MW and a 40 MW starting frequency converter for an energy storage project in China
- The motor will have an efficiency of beyond 98 percent
Siemens LDA has received an order from a Chinese customer to deliver a special machine with dual shaft extension. It can be used in motor operation with a power of 105 MW and as generator with up to 129 MVA in power generation mode. The motor will have an efficiency of beyond 98 percent and will be a world-leading 2-pole electric motor.Beside the motor, the contract includes the delivery of a 40 MW Sinamics GL150 starting frequency converter. This LCI-converter (load commutated inverter) is designed for single-motor applications with variable and constant torque characteristics. As a result of the low switching losses and the low loss thyristor technology, the efficiency of the LCI converter is extremely high and lies at 99 percent.
- Analyze MyDrives Edge with new feature to optimize energy consumption
- Analyze MyDrives Edge is part of Siemens Xcelerator
- New compact DC/DC converter Sinamics DCP 250 kW
In the field of
energy-efficient and sustainable drive technology, Siemens is bringing two
innovations to this year's Smart Production Solutions (SPS) trade fair in
Nuremberg. The first innovation relates to the Analyze MyDrives Edge
application, which is already established on the market. This is equipped with
a new feature that ensures transparency regarding the energy consumption of the
entire drive system. The AI-based feature of the Edge app calculates all data
without the need for additional sensors and special measuring devices. The app
shows how efficiently the drive runs, how high energy consumption and operating
costs are and what carbon footprint the drive leaves behind. Drive settings can
thus be optimized even better to customer needs.
- Sinamics DriveSim Advanced expands the Industrial Operations X offering, part of the Siemens Xcelerator digital business platform
- Sinamics DriveSim Advanced simulation software for virtual engineering and commissioning of drive constellations
- Complete digital twin of Sinamics drives with all parameters and configurations
- Extending digitalization of drive technology continuously enables machine builders to reduce resource consumption and optimize energy efficiency
At this year's Hannover
Messe, Siemens is presenting Sinamics DriveSim Advanced, an extended simulation
software for drive constellations that can be used for both engineering and
commissioning on the basis of a digital twin. Sinamics DriveSim
Advanced thus expands the simulation portfolio for motion control drives at
Siemens, which was introduced to the market in 2021 with Sinamics DriveSim
Basic. At the same time, Sinamics DriveSim Advanced adds to the Industrial Operations X offering. With Industrial Operations X, Siemens offers a continuously growing interoperable portfolio of products and services for production engineering, execution, and optimization. This offering brings more information technology (IT) and software capabilities to automation and production operations, making industrial operations more adaptable. The Industrial Operations X portfolio is characterized by supporting an open ecosystem, being flexible with modular and scalable functions, and enabling interoperable, seamless, holistic production value chains.
- Predictive Service Analyzer provides information about anomalies in the drive system
- Increased plant availability by up to 30 percent through reduced production downtime
- AI-based algorithm for drive systems
As part of Predictive
Services for Drive Systems, Siemens is expanding its offering at the Hannover
Messe with an edge application. The Predictive Service Analyzer indicates
defects in the drive system at an early stage before they affect the entire
production. As a result, unplanned production downtime can be avoided and
maintenance times can be scheduled in good time, increasing plant availability
by up to 30 percent. By scheduling maintenance and servicing activities based
on actual demand, this increases productivity by up to 10 percent. The Predictive
Service Analyzer's AI-based solution detects early signs of anomalies, such as
those indicating mechanical damage in the motor, including bearing damage,
imbalance, and misalignment, as well as critical operating conditions of the
frequency converter. The app assesses the severity of the defect and the
expected remaining runtime and can thus predict potential future failures.
- Focus on combining the real and the digital worlds
- IIoT: Data-based algorithms increase operational efficiency of plants
- Process optimization and modularization as the key to success
At the "Achema Pulse" live digital event, Siemens will be demonstrating how the combination of the real and the digital worlds empowers industrial companies to act in a versatile and sustainable manner. Companies in the process industry are facing urgent and rapidly changing challenges. The Covid-19 pandemic in particular has transformed demand patterns and global supply chains virtually overnight. At the same time, industry-specific regulations and standards are creating new framework conditions for production. Digitalization and automation are the levers for mastering these changes. Industrial IoT solutions can exploit the resulting data to secure a competitive advantage since the intelligent analysis, understanding and utilization of the data allows companies to adapt their processes faster to changing requirements. The Siemens Digital Enterprise portfolio makes this possible by combining the real world with the digital world, thus enabling solutions for simulation, virtual processes, remote access and connectivity as well as presenting service offerings for digital transformation. Thanks to the corresponding industry-specific know-how, individual sector requirements can be taken into account.