- New Booksize Motor Modules for Sinamics S120 series
- Version with double (C-type) and triple (D-type) overload factor
- 24A devices close portfolio gap between 18A and 30A
- New variants offer compact design and higher maximum current
The Booksize Motor Module portfolio has been further developed to include compatible new C and D type Sinamics S120 Booksize Motor Modules. Siemens has added a number of new devices to the existing 3A-30A range. The 24A, 45A and 60A Motor Modules are now available with double overload factor (Continuous C-type), and the 24A modules are additionally available with triple overload factor (Discontinuous D-type). With a 33 percent narrower fit than the existing variants, the new 45A und 60A devices are extremely compact, enabling significant space savings in the control cabinet. The maximum current in the 45A devices has also been increased from 85A to 90A, while the 60A devices now come with a 120A maximum current instead of the previous 113A.A completely new addition to the series are the 24A devices, which will be available as either a C or D type. This closes the gap in the portfolio between 18A and 30A.
- Scalance W1788 ensures investment in industrial networks with WLAN Standard IEEE 802.11ac Wave 2
- Optimum implementation of wireless applications with high bandwidths
- Wide-ranging networking scope through integrated switch
- Reliable redundancy in harsh environmental conditions
Siemens is extending its portfolio of network components with Scalance W1788 Access Points, which are designed to facilitate implementation of the current WLAN Standard IEEE 802.11ac Wave 2 in industrial applications. Users will benefit from investment protection for industrial networks, and the assurance of future-proof wireless applications and projects in industrial environments. The standard will enable wireless applications with high bandwidths to be ideally implemented at gigabit data rates – for instance to transmit video data or where a high user density is involved. The integrated switch features two managed Ethernet gigabit ports offering wide-ranging networking possibilities such as link aggregation.The industrial feature (iFeature) iPRP (Industrial Parallel Redundancy Protocol) ensures reliable redundancy via WLAN even in the toughest of ambient conditions.
- 5 and 10 ampere power supply for the Simatic ET 200SP
- Flat format for use on distribution boards
- Current monitor for early fault detection and energy management
- Shutdown and isolation of the 24 V supply simplify commissioning and maintenance of the system
Siemens is bringing onto the market the Simatic ET 200SP PS, a single-phase power supply for the Simatic ET 200SP distributed I/O system. The 24 volt power supplies from the Sitop product family supply rated currents of 5 and 10 amperes, and their design, construction and functionality are optimally matched to the distributed controller. An on/off switch for the 24 volts, and plug-in terminals for three load circuits simplify the commissioning and maintenance of the system. The power supply has a current monitor that outputs the momentary output current and enables, for example, optimization of the energy management. A mounting depth of a mere 75 mm allows the power supply to be used on flat distribution boards.
- New, low-cost Sitrans FS220 clamp-on ultrasonic flow system
- User-friendly interface with setup wizards for simplified operation
- High accuracy of 1% of flow rate
- Newest addition to portfolio of next-generation digital flow systems
Siemens launched the Sitrans FS220 clamp-on ultrasonic flowmeter, the newest addition to the growing portfolio of next-generation digital flow measurement systems from Siemens. Combining the Sitrans FST020 transmitter with Sitrans FSS200 externally mounted sensors, the Sitrans FS220 offers the most commonly required measurement functions with superior accuracy, cost efficiency and ease of use. The new flow system is suitable for multiple industries requiring budget-conscious liquid flow instrumentation, including water and wastewater, power, HVAC and chemical.
- Underground to surface (drift) conveyor system with gearless drives
- New system extends existing opencast mining
- Copper ore production increased by 95,000 tons per day
Siemens is undertaking the engineering, design, production and supply of the electrical equipment for the Oyu Tolgoi copper mine conveyor system. The delivery comprises the new conveyor system with gearless and conventional drives from thyssenkrupp Industrial Solutions. The new system extends the existing opencast mining facility and is expected to bring 95,000 tons of copper ore to the surface per day. The conveyor system has to overcome a difference in height of almost 1,400 meters. Initial production is expected to commence in 2020. The order value is in the tens of millions of Euros.
- Optional I/O module for Sinamics V20 converters
- Sinamics V20 I/O module in Plug&Play design for greater flexibility
- Front and rear ports offer compatibility with additional components
For the smallest converter in its portfolio, the Sinamics V20, Siemens is now offering an extension module for the capture and output of digital and analog signals. The Sinamics V20 I/O extension module is mounted on the converter using Plug&Play technology, and provides two additional input and output interfaces, each for 400 volts., increasing both the flexibility and the scope of the Sinamics V20. Using connecting ports on the front and back, the extension module can also be combined with additional accessories from the Sinamics V20 portfolio. These include for instance the BOP (Basic Operator Panel) and the BOP interface module.
- Extended Digital Enterprise portfolio for discrete and process industries
- Machine and plant builders use digitalization to develop new business models and speed up time-to-market
- Digitalization applications enhance flexibility, efficiency and quality
- Extended "MindSphere-Lounge" over an area of 1,400 square meters
Siemens will be exhibiting at the "SPS IPC Drives" 2017 with an array of applications and examples of how machine and plant builders can sharpen their competitive edge with digitalization. Exhibiting under the banner "Discover the Value of the Digital Enterprise" in Hall 11 across an impressive 4,400 square meter exhibition space, the company will be presenting the latest additions to its Digital Enterprise portfolio. Innovations featured range from new software versions for more efficient engineering through digital drive systems to the open cloud-based IoT operating system MindSphere, which opens up scope for new business models to machine and plant builders. This allows companies across the discrete and process industries to enhance their flexibility, efficiency and speed, for instance by using a "digital twin" to simulate products, production processes or plants and optimize them across the entire value chain.
- Digitalization of low-flow measurement
- Sensor program expansion with DN100 and DN150
- Transmitter with Modbus and Profibus PA profile 4.0 communication
- Suitable for new applications in oil and gas, marine, and chemical
To extend the numerous process-optimizing advantages of the digital Coriolis flowmeter platform to low-flow applications such as batching, dosing and filling of both liquids and gases, the Sitrans FCT030 and FCT010 digital transmitters can now be paired with the Sitrans F C MASS 2100 and Sitrans FC300 Coriolis sensors for small line sizes from DI 1.5 to DN 15. With this major enhancement to the product line, a broad range of users from chemical to automotive applications can benefit from market-leading mass flow accuracy of 0.1%, density accuracy of 0.5 kg/m3 and 100 Hz signal processing. The high-speed update rate ensures the highest precision for applications such as the filling of beverage bottles.
- Digitalization allows machine manufacturers to develop new business models
- Openness of MindSphere has an important role to play for machine manufacturers
- Siemens connects 240 machine tools with "Manage MyMachines" on MindSphere across the whole exhibition site
At the EMO 2017, Siemens is demonstrating the various connection and installation options of its high-performance and open cloud-based IoT operating system MindSphere for applications in the machine tool sector. The company is connecting over 240 different machine tools from over 140 manufacturers across the whole exhibition site using its "Manage MyMachines" app on MindSphere. In addition to this, machine manufacturers such as Heller are presenting new services and business models based on MindSphere to, for example, increase efficiency and productivity.
- Memorandum of Understanding signed at EMO 2017
- Common understanding of closer, long-term partnership in integrating Siemens technology in FFG machine tools
- Introduction of the Digital Enterprise Suite and the cloud-based IoT operating system MindSphere at FFG
- Collaboration in Product Lifecycle Management (PLM), Manufacturing Operations Management (MOM) and Totally Integrated Automation (TIA)
Siemens and Fair Friend Enterprise Co., Ltd. Taiwan (FFG), which, in addition to its Industrial Equipment and Green Energy Divisions, is one of the world's leading manufacturers of machine tools, now intend to strengthen their long-standing business relationship. The aim of the extended partnership is to consolidate the integration of the Siemens Digital Enterprise Suite across the Taiwanese business and to integrate innovative Siemens digitalization and automation technologies into FFG's machine tools and machine tool technologies.