[{"name":"Home","site_name":"Press | Company | Siemens","description":"","url_str":"\/global\/","level":0,"image":"","base_root":"https:\/\/press.siemens.com","base_nid":"5","base_nodepath":"\/node\/5","base_path":"\/global\/","base_secure_url":"https:\/\/press.siemens.com\/global","children":null}]
[]
Please use another Browser
It looks like you are using a browser that is not fully supported. Please note that there might be constraints on site display and
usability.
For the best experience we suggest that you download the newest version of a supported browser:
Press Release08 November 2017Digital Factory Nuremberg
Sinamics S120 Booksize Motor Modules: new sizes (45A/60A) and new devices (24A) with reduced space requirement
New Booksize Motor Modules for Sinamics S120 series
Version with double (C-type) and triple (D-type) overload factor
24A devices close portfolio gap between 18A and 30A
New variants offer compact design and higher maximum current
The Booksize Motor Module portfolio has been further developed to include compatible new C and D type Sinamics S120 Booksize Motor Modules. Siemens has added a number of new devices to the existing 3A-30A range. The 24A, 45A and 60A Motor Modules are now available with double overload factor (Continuous C-type), and the 24A modules are additionally available with triple overload factor (Discontinuous D-type). With a 33 percent narrower fit than the existing variants, the new 45A und 60A devices are extremely compact, enabling significant space savings in the control cabinet. The maximum current in the 45A devices has also been increased from 85A to 90A, while the 60A devices now come with a 120A maximum current instead of the previous 113A.A completely new addition to the series are the 24A devices, which will be available as either a C or D type. This closes the gap in the portfolio between 18A and 30A.
New Booksize Motor Modules for Sinamics S120 series
Version with double (C-type) and triple (D-type) overload factor
24A devices close portfolio gap between 18A and 30A
New variants offer compact design and higher maximum current
The Booksize Motor Module portfolio has been further developed to include compatible new C and D type Sinamics S120 Booksize Motor Modules. Siemens has added a number of new devices to the existing 3A-30A range. The 24A, 45A and 60A Motor Modules are now available with double overload factor (Continuous C-type), and the 24A modules are additionally available with triple overload factor (Discontinuous D-type). With a 33 percent narrower fit than the existing variants, the new 45A und 60A devices are extremely compact, enabling significant space savings in the control cabinet. The maximum current in the 45A devices has also been increased from 85A to 90A, while the 60A devices now come with a 120A maximum current instead of the previous 113A.A completely new addition to the series are the 24A devices, which will be available as either a C or D type. This closes the gap in the portfolio between 18A and 30A.
Sinamics S120 is a modular drive system for high-performance motion control applications in machine and systems engineering. Users can select from a wide range of coordinated components and functions and combine them to meet their own specific requirements. The Motor Modules (power units) are an integral part of the S120 drive system.
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for 170 years. The company is active in more than 200 countries, focusing on the areas of electrification, automation and digitalization. One of the world's largest producers of energy-efficient, resource-saving technologies, Siemens is a leading supplier of efficient power generation and power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. The company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2016, which ended on September 30, 2016, Siemens generated revenue of €79.6 billion and net income of €5.6 billion. At the end of September 2016, the company had around 351,000 employees worldwide. Further information is available on the Internet at www.siemens.com.