Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release07 November 2017Process Industries and DrivesNuremberg
New Access Points for future-proof industrial networks
Scalance W1788 uses MU-MIMO (Multiuser Multiple Input Multiple Output) technology to structure data flows and achieve higher data transmission rates. The Access Points can be used outside of the control cabinet. Their high IP65 protection class and the screw-fixed M12 and N-Connect enable them to withstand harsh industrial environments. To allow flexible and easyinstallation, the Scalance W1788 Access Points are available with internal or remote antennas, and come in anumber of product variants and designs to suit the relevant application. These include variants with one or two radios for optimum data utilization, or a special EEC variant for use in enhanced environmental conditions for applications such as railways. All Access Points are available in different country variants to facilitate their application around the world. Like all Scalance W components, the new Access Points also come with the familiar parameterization interfaces and a wide range of matching accessories and antennas for every application.
For further information on Siemens at the SPS IPC Drives 2017, please see www.siemens.com/sps-ipc-drives and www.siemens.com/press/sps2017
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for 170 years. The company is active in more than 200 countries, focusing on the areas of electrification, automation and digitalization. One of the world's largest producers of energy-efficient, resource-saving technologies, Siemens is a leading supplier of efficient power generation and power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. The company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2016, which ended on September 30, 2016, Siemens generated revenue of €79.6 billion and net income of €5.6 billion. At the end of September 2016, the company had around 351,000 employees worldwide. Further information is available on the Internet at www.siemens.com.
Contact
David Petry
Siemens AG
Werner-von-Siemens-Str. 65
91052 Erlangen
Germany
91052 Erlangen
Germany
+49 (9131) 7-26616