- Higher performance and new application areas for Siplus HCS4200 Heating Control System with two new power output modules
- Versatile control of electrical heating elements in 45, 75, 110, 230/277 and 400/480 V power grid
- Current measurement integrated in output for diagnosis of heating elements connected in parallel
- Simple, easy engineering and commissioning of industrial heating processes with TIA Portal and Proneta
Siemens has equipped the flexible, modular Siplus HCS4200 Heating Control System for switching and controlling heat emitter arrays and heating elements with two new power output modules (POM). Each output is now even more powerful and it is possible to control voltages from 45 V, making this versatile heating control system even more flexible, and suitable for use in safety extra-low voltage applications, for example.
- "Realize the value of the Digital Enterprise Suite – Industrialize Additive Manufacturing" as this year's booth slogan
- Seamless integrated software and automation solutions for additive manufacturing aimed at machine builders and users
- Innovative value-add services to further speed up the industrialization of additive manufacturing
- Engineering and printing services through to complete additive manufacturing of parts by Material Solutions and Mobility Services
At this year's formnext, the leading trade fair for additive manufacturing (AM), Siemens will be showcasing its seamless integrated solutions for additive manufacturing with the Digital Enterprise Suite. At its booth stretching over an area of around 150 square meters, the company will be demonstrating its portfolio along the entire AM value chain at the show from 14 to 17 November under the banner "Realize the Value of the Digital Enterprise Suite – Industrialize Additive Manufacturing". Products featured at the show cover everything from design and engineering software, simulation tools and matching hardware for complete machine and factory automation through to machine networking with the cloud-based IoT operating system MindSphere. Designed to address the requirements of both machine builders and additive manufacturing users, this unique offering from Siemens aims to demonstrate how companies working in the field of additive manufacturing can use digitalization to significantly boost the flexibility and efficiency of their production, reduce both engineering time and time to market, and so consolidate and expand their competitive standing in the global marketplace.
As part of formnext 2017, the leading exhibition for additive manufacturing, Siemens presented its comprehensive solution portfolio for consistent digitalization of additive manufacturing, starting with the design and engineering software, via innovative simulation tools to complete machine and factory automation. In addition to this, Siemens demonstrated how the industrialization of additive manufacturing can be further accelerated by using innovative added value services.
- Industrial Ethernet switches in electrical and optical version
- Direct (24 V) and alternating (24 V) current for industry and building use
- Up to 24 electrical ports for connecting a large number of nodes
- Profinet CC-A conformity ensures reliable data transmission
With its Scalance XB-100 product line, Siemens is launching a new generation of compact unmanaged Industrial Ethernet switches designed to permit the configuration of electrical and optical line and star topologies in networks. This range of switches is particularly suited for use in industry and in building automation applications. Design features include a large number of ports and interfaces, a lightweight plastic enclosure, and a compact design making it ideal for control cabinet mounting. The switches are also approved for use in potentially explosive atmospheres (ATEX Zone 2, IECEx). As unmanaged switches with no pre-configuration, the Scalance XB-100 products are suitable for immediate use, and come with Profinet CC-A conformity to ensure the reliable transmission of Profinet data.
- Scalance SC-600 Industrial Security Appliances – offers protection at the cell level
- Stateful Inspection Firewall with data throughput of 600 Mbit/s
- Configuration via web server, TIA Portal, SNMP and CLI
- Secured remote maintenance in combination with Sinema Remote Connect
Siemens is extending its portfolio offering protection against attacks on software and hardware components at the industrial cell level: The new Scalance SC-600 Industrial Security Appliances have a firewall (Stateful Inspection Firewall) with a data throughput of up to 600 Megabits per second (Mbit/s). Depending on the variant users can also administer VPN tunnels up to 200 IPsec (Internet Protocol Security). Scalance SC-600 also provides convenient options for network structuring via virtual LANs (VLAN) and Network Address Translation (NAT/NAPT). The Scalance SC-600 is configured via the integral web server using the Simple Network Management Protocol (SNMP), Command Line Interface (CLI) or the Step 7 V15 engineering software (TIA Portal). For secured remote access, the new industrial security appliances can be connected via the Sinema Remote Connect management platform.
- New Booksize Motor Modules for Sinamics S120 series
- Version with double (C-type) and triple (D-type) overload factor
- 24A devices close portfolio gap between 18A and 30A
- New variants offer compact design and higher maximum current
The Booksize Motor Module portfolio has been further developed to include compatible new C and D type Sinamics S120 Booksize Motor Modules. Siemens has added a number of new devices to the existing 3A-30A range. The 24A, 45A and 60A Motor Modules are now available with double overload factor (Continuous C-type), and the 24A modules are additionally available with triple overload factor (Discontinuous D-type). With a 33 percent narrower fit than the existing variants, the new 45A und 60A devices are extremely compact, enabling significant space savings in the control cabinet. The maximum current in the 45A devices has also been increased from 85A to 90A, while the 60A devices now come with a 120A maximum current instead of the previous 113A.A completely new addition to the series are the 24A devices, which will be available as either a C or D type. This closes the gap in the portfolio between 18A and 30A.
- Scalance W1788 ensures investment in industrial networks with WLAN Standard IEEE 802.11ac Wave 2
- Optimum implementation of wireless applications with high bandwidths
- Wide-ranging networking scope through integrated switch
- Reliable redundancy in harsh environmental conditions
Siemens is extending its portfolio of network components with Scalance W1788 Access Points, which are designed to facilitate implementation of the current WLAN Standard IEEE 802.11ac Wave 2 in industrial applications. Users will benefit from investment protection for industrial networks, and the assurance of future-proof wireless applications and projects in industrial environments. The standard will enable wireless applications with high bandwidths to be ideally implemented at gigabit data rates – for instance to transmit video data or where a high user density is involved. The integrated switch features two managed Ethernet gigabit ports offering wide-ranging networking possibilities such as link aggregation.The industrial feature (iFeature) iPRP (Industrial Parallel Redundancy Protocol) ensures reliable redundancy via WLAN even in the toughest of ambient conditions.
- 5 and 10 ampere power supply for the Simatic ET 200SP
- Flat format for use on distribution boards
- Current monitor for early fault detection and energy management
- Shutdown and isolation of the 24 V supply simplify commissioning and maintenance of the system
Siemens is bringing onto the market the Simatic ET 200SP PS, a single-phase power supply for the Simatic ET 200SP distributed I/O system. The 24 volt power supplies from the Sitop product family supply rated currents of 5 and 10 amperes, and their design, construction and functionality are optimally matched to the distributed controller. An on/off switch for the 24 volts, and plug-in terminals for three load circuits simplify the commissioning and maintenance of the system. The power supply has a current monitor that outputs the momentary output current and enables, for example, optimization of the energy management. A mounting depth of a mere 75 mm allows the power supply to be used on flat distribution boards.
- Underground to surface (drift) conveyor system with gearless drives
- New system extends existing opencast mining
- Copper ore production increased by 95,000 tons per day
Siemens is undertaking the engineering, design, production and supply of the electrical equipment for the Oyu Tolgoi copper mine conveyor system. The delivery comprises the new conveyor system with gearless and conventional drives from thyssenkrupp Industrial Solutions. The new system extends the existing opencast mining facility and is expected to bring 95,000 tons of copper ore to the surface per day. The conveyor system has to overcome a difference in height of almost 1,400 meters. Initial production is expected to commence in 2020. The order value is in the tens of millions of Euros.
- New, low-cost Sitrans FS220 clamp-on ultrasonic flow system
- User-friendly interface with setup wizards for simplified operation
- High accuracy of 1% of flow rate
- Newest addition to portfolio of next-generation digital flow systems
Siemens launched the Sitrans FS220 clamp-on ultrasonic flowmeter, the newest addition to the growing portfolio of next-generation digital flow measurement systems from Siemens. Combining the Sitrans FST020 transmitter with Sitrans FSS200 externally mounted sensors, the Sitrans FS220 offers the most commonly required measurement functions with superior accuracy, cost efficiency and ease of use. The new flow system is suitable for multiple industries requiring budget-conscious liquid flow instrumentation, including water and wastewater, power, HVAC and chemical.