- New additive manufacturing process simulation helps predict distortion and shrinkage during the 3D printing process and helps avoid these issues by automatically generating a compensated model
- Simcenter 3D solution for additive manufacturing process simulation is fully integrated within NX software for a streamlined feedback loop with no data translation required
- Siemens' integrated digital innovation platform allows simulation data to feed the digital thread, informing each step of the industrialized additive manufacturing process
Siemens announced today a new Additive Manufacturing (AM) Process Simulation solution for predicting distortion during 3D printing. The product is fully integrated into Siemens’ end-to-end Additive Manufacturing solution, which assists manufacturers in designing and printing useful parts at scale. Building on Siemens’ comprehensive digital innovation platform and the Simcenter™ portfolio, the AM Process Simulation solution uses a digital twin to simulate the build process prior to printing, anticipating distortion within the printing process and automatically generating the corrected geometry to compensate for these distortions. This simulation is paramount for constructing a ‘first time right’ print, and necessary for achieving the efficiencies required of a fully industrialized additive manufacturing process.
- Partnership to bridge Operational Technology (OT) and Information Technology (IT) networks
- Solutions extend from factory floors to corporate offices
- Extensive interoperability testing and validated reference designs simplify deployment and maintenance based on complementary product portfolios
Siemens and Aruba, a Hewlett Packard Enterprise company, today announced a strategic partnership focused on bridging the Operational Technology (OT) and Information Technology (IT) worlds. Based on the complementary portfolios, Siemens and Aruba are able to support customers with highly reliable, secure and insightful data networks enabling high plant and network availability. Customers benefit from integrated networks with proven interoperability from factory floors to corporate offices based on Siemens' expertise as a leading provider of industrial Ethernet network components and Aruba's as a leader in wired and wireless LAN infrastructure.
- New type of active power-based dry running protection for pumps with certification according to ATEX and IEC Ex
- Current/voltage detection modules for the Simocode pro motor management system
- Previously required additional sensor technology is eliminated
- Higher levels of system availability and economic efficiency
A new type of detection technology from Siemens protects centrifugal pumps from dry running in hazardous areas. For this purpose, the corporation has developed special current/voltage detection modules for its Simocode pro motor management system. The principles and practical applicability of this technology have been investigated within the scope of a research cooperation project with the Physikalisch-Technische Bundesanstalt (National Metrology Institute of Germany) in order for it to be certified as an ignition source monitoring device corresponding to a type b1 ignition protection system according to ATEX and IEC Ex.
- New standard power supply for 12 V and 24 V applications
- High overload capability and energy efficiency
- Condition monitoring by means of diagnostics monitor and interface
- Rugged wide-range input, also suitable for direct voltage
Siemens is bringing a new line of particularly powerful and rugged power supplies to the market: The devices of the Sitop PSU6200 line can be used for a variety of purposes and offer extensive functions for targeted diagnostics, fast assembly and reliable operation. In addition, the single-phase 12 V and 24 V power supply units have a wide-range input for alternating voltage which also enables the connection to direct voltage and is particularly resistant to undervoltage and overvoltage. The high effectiveness of up to 95 percent and the efficient heat dissipation through the metal enclosure keep the heat generation low. The compact power supply units can therefore be arranged in a space-saving manner without lateral installation clearances to other devices. Typical applications include standard machine, control cabinet and system construction in the automotive, textile, food & beverage and pharmaceuticals industries, as well as the field of renewable energies.
- On a comparable basis, excluding currency translation and portfolio effects, orders rose 8% and revenue increased 2%, with the majority of the industrial businesses contributing to growth
- On a nominal basis, orders rose 6%, to €91.3 billion; revenue was up slightly at €83.0 billion; the book-to-bill ratio was 1.10
- Industrial Business profit came in lower, at €8.8 billion, as profit increases in most industrial businesses did not fully offset sharply lower profit at Power and Gas
- Industrial Business profit margin excluding severance charges of 11.3%, clearly in the guidance range of 11% to 12%; profit margin including severance charges of €0.8 billion was 10.4% with most industrial businesses within or above their target ranges
- Net income up slightly at €6.1 billion; basic earnings per share (EPS) of €7.12; excluding severance charges, basic EPS at €7.88, well within the guidance range of €7.70 to €8.00
- Free cash flow rose to €5.8 billion, up 22% year-over-year
- Siemens proposes to raise the dividend €0.10 per share, to €3.80 per share
- Successful completion of share buyback program initiated in November 2015 with a volume of €3.0 billion; new share buyback program announced with volume up to €3.0 billion until November 2021
"We again delivered what we promised and fully reached our guidance which we raised at mid-year. This shows the strength of our global team which competed convincingly in both growth markets and difficult environments, and achieved another strong performance. In fiscal 2019 we will give our businesses even greater entrepreneurial freedom, and lay the foundation for execution of Vision 2020+."
- Volume of up to €3 billion
- Share buyback to be executed by November 15, 2021
Siemens announced a new share buyback program today. The new buyback, with a volume of up to €3 billion, is to be executed in the period ending on November 15, 2021.
- Vacuum circuit breakers and "clean air" insulation replace SF6 as switching and insulating medium
- SF6-free gas-insulated switchgear (GIS) for 145 kV, 40 kA, 3,150 A
- Combination with low power instrument transformers (LPIT) ensures a compact design
Siemens Energy Management received an order from Bergenshalvøens Kommunale Kraftselskap (BKK Nett) in Norway to supply the world's first SF6-free GIS with "clean air" and vacuum interruption systems for a voltage level of up to 145 kilovolts (kV). The switchgear is part of the Koengen substation in Bergen, which shall supply electricity from renewable energy sources to Norway's largest cruise ship seaport. Non-conventional systems for measuring current and voltage allow the switchgear to have a much more compact design. The start of the collaboration was celebrated on November 5, 2018, at Siemens' headquarters in Bergen. Commissioning is scheduled for end of 2019.
- Reduction of pollutant emissions, diesel generators can remain shut down
- Parallel supply with up to 12 MVA in dock and while berthed
- Flexible 50/60-Hertz (Hz) power supply
- Siemens takes on turnkey construction and service
Siemens has received an order from MV WERFTEN Wismar GmbH to supply and install turnkey Siharbor onshore power supplies. The onshore power supply system will be used to build "Global Class" cruise ships. Measuring 340 meters in length and providing space for more than 5,000 passengers, these vessels are the world's largest cruise ships, and great amounts of energy are needed for their construction. An onshore power supply with a capacity of up to 12 MVA provides this energy simultaneously in dock and on the quay. The order covers all the necessary components for powering the ships as well as the grid connection. It includes the complete substation, transformers, and medium-voltage switchgear. Siemens will also be responsible for service for a period of five years. The systems are expected to go into operation in the spring of 2019.
- SIEAERO leverages UAVs, artificial intelligence and digital twins to improve service of transmission lines
- Reducing the time for flight execution and data analysis from weeks or even months to a few days
Siemens has launched a new service approach for overhead line inspection called "SIEAERO" at European Utility Week 2018 in Vienna, Austria. For the first time artificial intelligence and a long-range unmanned aerial vehicle (UAV) are used to bring inspection of transmission lines to the next level. SIEAERO smart analytics software is utilizing artificial intelligence (AI) and machine learning to store, manage and analyze all data in one integrated software system. To reduce the needed amount of flights and inspection efforts drastically, SIEAERO is using a unique high-resolution multi-sensor-system that can record all needed data in one go. Compared to conventional overhead line inspection, SIEAERO service is fully automated, faster and more precise. Siemens has been working closely with German and Austrian transmission system operators (TSO) TenneT and APG on the development of SIEAERO overhead line inspection service since 2016. With both TSOs Siemens has worked on test cases and the validation of a comprehensive inspection approach.
- ETCS Baseline 3 train equipment for cross-border operation
- Commissioning approved for 12-car train
- Service on the Berlin – Munich route planned for timetable change in December 2018
Germany's Federal Railway Authority (EBA) has approved the ICE 4 for operation with the European Train Control System (ETCS) in Germany. With this approval, the passenger service can begin as planned on the Berlin – Munich route, which is equipped with the system. The ICE 4 is scheduled to operate on this line when German train operator Deutsche Bahn (DB) changes its timetable on December 9, 2018.