Please use another Browser

It looks like you are using a browser that is not fully supported. Please note that there might be constraints on site display and usability. For the best experience we suggest that you download the newest version of a supported browser:

Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser

Continue with the current browser

Siemens presents SIEAERO – the next generation of overhead line inspection

Siemens presents SIEAERO – the next generation of overhead line inspection.

"SIEAERO is a gamechanger in overhead line inspection because we are using digitalization to bring services for our customers to the next level", says Mirko Düsel, CEO Transmission Solutions at Siemens' Energy Management Division. "Everything, from planning and performing inspection flights, managing and analyzing the gathered data to report generation and long-term data archiving, is more cost-efficient with SIEAERO - and it provides better and faster results on top."
Overhead line inspection is a billion Euro market. In North America and Europe alone there are more than 200,000 kilometers (km) of overhead lines transmitting power to households and industries. All of them are critical infrastructure that need regular inspection to avoid failures. Today, TSOs inspect their power lines with helicopters at least once a year. Siemens has developed the SIEAERO service concept cooperating closely with customers and introduces a series of innovations to improve transmission line inspection as it is today.
Using SIEAERO, the flights are performed with the CAMCOPTER® S-100, a high-performance long-range UAV for beyond visual line-of-sight operation with a high pay load capacity. The S-100 carries the SIEAERO high-end multi-sensor system which was specifically developed to meet the complex requirements of overhead line inspections. Since all necessary sensors and cameras are combined in one multi-sensor system, all relevant inspection data are recorded in one go. Therefore, SIEAERO is much faster and more cost-efficient compared to conventional services.
The extensive amount of multi-sensor data generated during the flights is handled by the SIEAERO smart data analytics software. The software was also developed by Siemens and is based on AI and deep learning for automated detection and assessment of faults and issues along the overhead lines. The documentation of the complete lines as well as the relevant findings and results can be directly integrated into the customers' existing asset management systems. These are relevant for trend monitoring and preventive maintenance.
SIEAERO allows not only reducing the time for flight execution and data analysis from weeks or even months to a few days, but also delivers more precise results while using sensors way above industry standard. For example, the 3D LIDAR Sensors used in SIEAERO have 120 dots per m2, while industry standard is roundabout 30 dots per m². More sensor data results in more precise analytics and results. Moreover, SIEAERO uses five cameras with 100 megapixels each, while competitors are typically working with one or two cameras and a lower resolution. On top, the SIEAERO multi-sensor system also includes infrared and corona sensors.
Schiebel Group, a Vienna-based company, is supplying the CAMCOPTER® S-100 UAVs and is also involved in R&D activities to ensure that specific requirements are met. SIEAERO is utilizing the S-100 with a flight distance up to 200km and a sensor load capacity of 50 kg. Siemens has partnered with Lufthansa Aerial Services for the operation of UAVs. Lufthansa will perform the SIEAERO inspection flights globally. Currently most countries do not allow the operation of UAVs beyond visual line of sight. Once national regulations change, SIEAERO will utilize the CAMCOPTER® S-100. SIEAERO is available utilizing helicopters from March 2019 on.

The press kit for EUW 2018 is available at www.siemens.com/press/euw2018
For further information on Division Energy Management, please see www.siemens.com/energy-management

For this press release

Event: Siemens at European Utility Week 2018

Event: Siemens at European Utility Week 2018

Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for 170 years. The company is active around the globe, focusing on the areas of electrification, automation and digitalization. One of the world's largest producers of energy-efficient, resource-saving technologies, Siemens is a leading supplier of efficient power generation and power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. With its publicly listed subsidiary Siemens Healthineers AG, the company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2017, which ended on September 30, 2017, Siemens generated revenue of €83.0 billion and net income of €6.2 billion. At the end of September 2017, the company had around 377,000 employees worldwide. Further information is available on the Internet at www.siemens.com.
Read more
Reference Number: PR2018110053EMEN

Contact

Sabrina Martin

Siemens AG

Freyeslebenstr. 1
91058 Erlangen
Germany

+49 (9131) 7-37168