Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release06 November 2018Energy ManagementErlangen
Siemens onshore power supplies to be used in construction of the world's largest cruise ships
Siemens onshore power supplies to be used in construction of the world's largest cruise ships
MV WERFTEN began to manufacture the world's largest cruise ships, known as "Global Class", in March of this year. In the past, it was customary to use external diesel generators during the first phase of construction. The generators produced energy at 60 Hz on land and transferred it to the ship. If the ship was provided with its own generator during the next phase, the latter supplied energy during the remaining fitout phase. The new onshore power supply can handle both steps simultaneously in dock and on the quay. The diesel generators can therefore remain shut down shoreside as well as on board of the ship under construction.
Unlike the German 50 Hz power grid, ships have an on-board electrical system with a frequency of 60 Hz. The 20 kV/50 Hz voltage supplied from the public grid is converted to the required voltage and frequency in the transformer substation. This frequency is 60 Hz during the first phase of shipbuilding and 440/60 Hz in the later production phase.
The combustion of ship fuels during lay time and construction is one of the main sources of air pollution in the areas around ports and wharves. Harmful emissions in the shipping industry need to be reduced: This would have an enormous impact on every port city around the world. Onshore power supplies make an important contribution to improving air quality and enable significant savings potential when it comes to nitrogen oxide and sulfur oxide emissions, fine dust, and carbon dioxide emissions. An onshore power supply is also much quieter than a diesel generator. This benefits residents as well as the employees at MV WERFTEN.
"We're using the Siharbor solution for the first time in an environment other than right in port and are implementing a parallel power supply," says Axel Mohr, head of sales of the Siemens Energy Management Division for industry and infrastructure customers, Region North. "This was an exciting challenge for us, one that will greatly benefit the customer and the environment. We're proud of this opportunity to do our part in making shipbuilding greener."
"Siemens is an outstanding partner to us," says André Machatzky, head of investments at MV WERFTEN. "The entire team is near our Wismar location and can give us immediate support for service and consulting. We'll continue to build low-emission ships in the future. The excellent collaboration led to fast planning, and we're looking forward to commissioning."
For further information on Sihabor, please see www.siemens.com/siharbor
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for 170 years. The company is active around the globe, focusing on the areas of electrification, automation and digitalization. One of the world's largest producers of energy-efficient, resource-saving technologies, Siemens is a leading supplier of efficient power generation and power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. With its publicly listed subsidiary Siemens Healthineers AG, the company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2017, which ended on September 30, 2017, Siemens generated revenue of €83.0 billion and net income of €6.2 billion. At the end of September 2017, the company had around 377,000 employees worldwide. Further information is available on the Internet at www.siemens.com.