Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release09 November 2018Process Industries and DrivesNuremberg
New power supply for a wide variety of applications

The picture shows the new line of particularly powerful and rugged power supplies Sitop PSU6200.
The connection terminals with push-in technology and their clear labelling enable fast and secure wiring. The power supply units from 10 amps inform users about the status of the device and the operating state. The diagnostics monitor indicates by means of LEDs whether the output voltage is correct, how high the load is and whether the end of its service life is approaching. In addition, via the diagnostics interface, users receive information about voltage and current values, the temperature status and the number of undervoltages and overvoltages at the output. Only one digital input of a controller (PLC) is required for the diagnostics. Free-of-charge function blocks for Simatic S7-1200 and S7-1500 evaluate the serial code and faceplates facilitate visualization in WinCC. The comprehensive condition monitoring enables users to respond promptly to critical conditions and thereby to make the supply of the control circuit even more secure.
The single-phase power supply units are available in different power classes with rated output currents from 1.3 to 20 A. The variants from 3.7 A also feature power reserves ("extra-power") which secure the power supply for up to 5 seconds, even in the event of 50 percent overload, for example during switch-on procedures. The constant current behavior limits the current in the event of higher overloads and maintains the output voltage for as long as possible. In this way, even brief short-circuits can be detected. The rugged devices continuously supply 20 percent more than their rated current, even at ambient temperatures of up to 45 ° Celsius.
The reliable Sitop PSU6200 product family is the new standard power supply that is also suitable for customers with high technical requirements. For example, the devices already comply today with the EMC standard, which will only become binding for the DC output from 2020. Users can expand the power supply units with additional modules (Sitop add-on modules) – for example, with redundancy and selectivity modules – in order to improve the reliability even further. Devices can also be expanded to form an uninterruptible 24 V power supply (DC UPS).
For further information on the Sitop PSU6200 http://www.siemens.com/sitop
For this press release

Event: Siemens at the SPS IPC Drives 2018
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 170 years. The company is active around the globe, focusing on the areas of electrification, automation and digitalization. One of the largest producers of energy-efficient, resource-saving technologies, Siemens is a leading supplier of efficient power generation and power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. With its publicly listed subsidiary Siemens Healthineers AG, the company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2018, which ended on September 30, 2018, Siemens generated revenue of €83.0 billion and net income of €6.1 billion. At the end of September 2018, the company had around 379,000 employees worldwide. Further information is available on the Internet at www.siemens.com.
Contact
David Petry
Siemens AG
Werner-von-Siemens-Str. 65
91052 Erlangen
Germany
91052 Erlangen
Germany
+49 (9131) 7-26616