Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release12 November 2018Digital Factory Nuremberg
Protecting pumps in hazardous areas easily and reliably against dry running
Simocode pro uses measuring modules to monitor the active electric power consumption of the pump motor to detect a diminishing flow rate and shut off the pump in good time at defined limit values to prevent impending dry running. Additional sensor technology otherwise required to monitor the pump for dry running can be eliminated. A menu-guided teach-in procedure in the engineering software helps the user to set the limit values. The advantages of the new type of active power-based dry running protection from Siemens are not only less hardware, early detection of faults and the avoidance of damage to the pump but also safe, reliable explosion protection, savings in time and money spent on maintenance, as well as higher system availability and economic efficiency.
Background information:
Safety has top priority wherever flammable media are used in industry. This applies in particular to the chemical industry, where flammable liquids are produced, processed and transported by pumps in hazardous areas. If the pumps start to run dry, hazardous conditions may arise inside and outside the pumps, such as air-gas mixtures, sparking and high temperatures caused by friction. The power consumption of electrically driven centrifugal pumps falls in the event of dry running, so Simocode pro switches the pumps off when consumption falls below a minimum value. This eliminates the installation of conventional monitoring devices, such as level sensors. The Simocode pro motor management system offers comprehensive protection, monitoring and control functions for the safe disconnection of motors, integration in process control systems such as Simatic PCS 7, and a large number of interfaces for system-wide communication. Simocode pro makes detailed operating, service and diagnostic data as well as process and measured values available to higher-level systems and cloud solutions.
Safety has top priority wherever flammable media are used in industry. This applies in particular to the chemical industry, where flammable liquids are produced, processed and transported by pumps in hazardous areas. If the pumps start to run dry, hazardous conditions may arise inside and outside the pumps, such as air-gas mixtures, sparking and high temperatures caused by friction. The power consumption of electrically driven centrifugal pumps falls in the event of dry running, so Simocode pro switches the pumps off when consumption falls below a minimum value. This eliminates the installation of conventional monitoring devices, such as level sensors. The Simocode pro motor management system offers comprehensive protection, monitoring and control functions for the safe disconnection of motors, integration in process control systems such as Simatic PCS 7, and a large number of interfaces for system-wide communication. Simocode pro makes detailed operating, service and diagnostic data as well as process and measured values available to higher-level systems and cloud solutions.
For this press release
Event: Siemens at the SPS IPC Drives 2018
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 170 years. The company is active around the globe, focusing on the areas of electrification, automation and digitalization. One of the largest producers of energy-efficient, resource-saving technologies, Siemens is a leading supplier of efficient power generation and power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. With its publicly listed subsidiary Siemens Healthineers AG, the company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2018, which ended on September 30, 2018, Siemens generated revenue of €83.0 billion and net income of €6.1 billion. At the end of September 2018, the company had around 379,000 employees worldwide. Further information is available on the Internet at www.siemens.com.
Contact
Andreas Friedrich
Siemens AG
Gleiwitzer Str. 555
90475 Nuremberg
Germany
90475 Nuremberg
Germany
+49 (1522) 2103967