- Approximately
2,000 kilometers of modern, safe and integrated rail system to link 60 cities for people and goods across the country
- Siemens
Mobility to provide 41 Velaro
eight car high-speed trains, 94 Desiro high-capacity four car regional train
sets and 41 Vectron freight locomotives
- Turnkey
contract includes latest rail infrastructure technology, eight depots &
yards and 15-year maintenance agreement
- Will
create sixth largest high-speed rail system in the world
- To
complete all aspects of the project the consortium will create up to 40,000
local jobs
Siemens Mobility and its consortium partners Orascom
Construction and The Arab Contractors have signed a contract with the Egyptian
National Authority for Tunnels (NAT), a governmental authority under the
jurisdiction of the Ministry of Transport of Egypt, to create the sixth largest
high-speed rail system in the world. The Siemens Mobility share of the combined
contract is 8.1 billion EUR and includes the initial contract of 2.7 billion
EUR for the first line signed September 1, 2021.
- Design, supply, testing, and commissioning of the power supply system for Jurong Region Line
A Siemens Mobility led consortium that includes Concord Corporation Pte Ltd. has been awarded a contract by the Singapore Land Transport Authority (LTA) for the design, supply, testing, and commissioning of the power supply system for the future Jurong Region Line. The system will be designed to be upgradeable, with interfaces for connecting power supply and signaling that will meet industry standards.
- Siemens supports BioNTech in converting to vaccine production at the Marburg plant
- Key parts of the new Manufacturing Execution System ready to use after only two and a half months
- Digitalization enables paperless documentation of production
The BioNTech SE biotechnology company based in Mainz has converted an existing facility in Marburg for the production of the Covid-19 vaccine in a record time with assistance from Siemens. The production plant has been producing the active substance since February and the vaccine BNT162b2 (also known as COMIRNATY®) since the end of March. BioNTech acquired a production facility for this in the fall of 2020 that was already equipped with capabilities for producing biotechnological substances. Through collaboration with Siemens and the team of experts on site in Marburg, the project timeline for converting the existing facility for the production of mRNA-vaccine was cut from around one year down to five months, whereby the implementation of key parts of the new Manufacturing Execution System (MES) was reduced to two and half months. The new system and end-to-end digitalization of production enable conversion to “paperless documentation of production”, which can immediately fulfill all documentation requirements.
- Sinumerik One is setting new standards in terms of productivity thanks to a new hardware platform and innovative technology functions
- Digital service offering supports machine users and machine manufacturers with the creation of a digital twin and with virtual commissioning
- Sinumerik One on show at EMO with more than 20 pilot customers
With the latest CNC generation, Sinumerik One, Siemens is presenting the essential component for the digital transformation of machine tools at EMO 2019. As a "digital native", the controller features versatile software for the creation of corresponding digital twins. Sinumerik One is setting new benchmarks in terms of productivity with its new hardware platform. A wide range of innovative technology functions help to improve processing speed, contour accuracy and processing quality.
- CBTC
signaling system and GoA4 operation to be implemented across a 22.8 km route, at
23 stations, and on 25 trains
- GoA4
functionality will allow for full automated driverless train operations
- The automated
signaling system will provide greater availability, enhanced operations, and
better passenger experience
Siemens Mobility, along with consortium partners ST
Engineering and Stadler, have been awarded an Electrical and Mechanical (E&M)
turnkey contract to deliver the Yellow Line for Kaohsiung Metro. Siemens
Mobility will provide its state-of-the-art CBTC signaling technology with GoA4
functionality, which will allow for full automated train operations (ATO). Furthermore,
Siemens Mobility will deliver its highly reliable and precise Airlink radio
communication system which will facilitate the communication of wayside and
onboard signaling equipment, that will be installed on the new trains.
- New Offering Seamlessly Combines Next-Generation Virtual Platform, Hardware Emulation, and FPGA Prototyping Technologies to Help Accelerate Verification Cycles
- Expansion of the Customer-Proven Veloce Family Sets New Standard in Hardware-assisted Verification
Siemens Digital Industries Software today unveiled its next-generation Veloce™ hardware-assisted verification system for the rapid verification of highly sophisticated, next-generation Integrated Circuit (IC) designs. This is the first complete, integrated offering that combines best-in-class virtual platform, hardware emulation, and Field Programmable Gate Array (FPGA) prototyping technologies, and paves the way to leverage the latest powerful hardware-assisted verification methodologies.
- Process control system Simatic PCS neo version 4.0 ready for process plants of any size
- Extended functionalities for modular systems based on MTP standard
- New hardware platform: Siemens presents new Simatic S7-4100 controller generation and Simatic CN 4100 communication node
- Siemens presents Simatic PCS neo V4.0 together with the new hardware for the first time at the SPS trade fair from November 8 to 10, 2022 in Nuremberg
Digitalization, sustainability, shortage of skilled workers: Companies
in the process industry are currently facing major challenges. To prepare their
plants for the future, Siemens believes that operators must rely on a highly
flexible process control system. Against this backdrop, Siemens has now
launched both a new software version and new hardware components for its
Simatic PCS neo web-based process control system. With version 4.0, Simatic PCS
neo is now ready for plant capacities and large-scale projects of up to 64,000
process objects and 56 controllers – making it suitable for industrial plants
of all sizes.
- VGF and Siemens Mobility to build the train control system of the future
for Frankfurt
- Major public transport infrastructure project and milestone in the
mobility transition
VGF,
Frankfurt’s public transport provider, will replace the conventional train control
system currently used in its metro and tram network with a new,
state-of-the-art digital system. The “Digital Train Control System Frankfurt” is
one of the company’s most important projects for the future. Following a public
procurement procedure initiated in early 2021, the VGF is now awarding the important
contract to Siemens Mobility.
- Siemens Mobility awarded €270 million contract to install digitalized CBTC technology across entire 94 km of track, including a new 6 km track
- Automated signalling will provide greater availability, enhanced operations, and passenger experience
- Digital maintenance and support services for the CBTC System for 25 years
Siemens Mobility has been awarded a €270 million contract by Sporveien AS in Oslo, Norway to install and maintain a Communications-Based Train Control system (CBTC) on the Oslo Metro. Siemens Mobility will completely replace the current legacy signalling with its digitalized CBTC technology which will provide greater automation and connectivity, allowing for a more efficient and centralized control of operations. Specifically, the optimization and renewal of the complete 94 km network will increase the availability, safety, and capacity of the Oslo Metro, while also equipping it to meet the future demands for mobility and the need for any potential expansions or upgrades. As part of this contract, Siemens Mobility will design, integrate, test, and commission the system, while also providing digital maintenance and support services for the CBTC system for 25 years.