- Two SGT-400 gas turbine compression packages sold for U.S. pipeline service
Siemens Gas and Power was awarded a contract to supply two SGT-400 gas turbine compression packages for Midcoast Energy, LLC’s CJ Express pipeline expansion project in east Texas. WHC Energy Services, supported by Universal Pegasus International, will be the engineering, procurement and contracting (EPC) provider for the pipeline expansion project.
- Single-phase 480-watt basic unit expands Sitop PSU8600 product line
- Four integrated monitored outputs of five amperes each (DC 24 V, 20 A/4x5)
- Modular expansion for monitoring up to 36 outputs
- Comprehensive diagnostic and maintenance information via integrated Ethernet/Profinet interfaces
Siemens is expanding its modular Sitop PSU8600 power supply system to include a new single-phase 480-watt basic unit. The new product features four integrated monitored outputs with a total of 24 volts DC at five amperes per output. Each output is flexible and can be set during operation in a range between 4 and 28 volts either manually or remotely via software. This eliminates the need for additional power supply units to supply five or twelve volt loads. The CNX8600 expansion module can be used to monitor up to 36 total outputs. Thanks to its integration into the TIA (Totally Integrated Automation) Portal engineering framework, fast implementation in to the automation is supported. In addition, the Sitop Manager provides easy parameterization and diagnostics. Comprehensive diagnostic and maintenance information are also available via the two integrated Ethernet/Profinet interfaces and via OPC UA, and can be evaluated directly in the automation systems. This means that errors can be located quickly and reduces downtime.
- Latest generation S700 low-floor light rail vehicles
- Manufactured in the Siemens Mobility Sacramento plant
Siemens Mobility has been awarded a contract from the U.S. operator Sacramento Regional Transit (SacRT) for 20 new light rail vehicles (LRVs). This is the first new order from Sacramento since the late 1980s, when SacRT ordered 36 U2A vehicles from Siemens Mobility. The contract, including the 20 trains, spare parts and tools is approximately US$100 million.
- New “Location Intelligence” software expands Simatic RTLS locating platform to include digital twin of performance
- Visualized real-time analyses create potential for optimization and facilitate rapid decision-making
- Provides customers with overview of material flow and order information
Siemens introduces new “Location Intelligence” software, which expands the Simatic RTLS (Real-Time Locating System) locating platform to include the digital twin of performance. The web-based software analyzes and visualizes dynamic data, processes events, and can be addressed directly from local ERP (Enterprise Resource Planning) or MES (Manufacturing Execution System) systems. The intelligence acquired based on position data provides the user with a comprehensive overview of material flow, order information or possible problem areas.
- Siemens Managing Board decides to form worldwide aid fund to help relieve
and combat the coronavirus pandemic
- Siemens to match all funds donated
by employees
- Fund to supplement numerous aid
programs already in place at international Siemens units
- Company and employees aim to help people stricken by the COVID-19 pandemic worldwide
- Entire Managing Board joins in donation campaign
- President and CEO lays foundation by donating €1 million
Effective immediately, the Managing Board of Siemens AG has decided to set up a COVID-19 aid fund. Under the auspices of the community-serving nonprofit organization Siemens Caring Hands e.V. (“Caring Hands”), this aid fund is to provide support, without red tape, to relief organizations and medical facilities as well as to individuals impacted by the COVID-19 crisis worldwide.
- Charter of Trust companies are helping with cybersecurity for telework
- Some 130,000 Siemens employees worldwide are working from home due to
the corona crisis
To slow the spread of the coronavirus, millions of people around the world have been working from home for about three weeks now – including more than 100,000 Siemens employees. Siemens and 16 other global companies from the Charter of Trust (CoT) initiative have developed eight tips for boosting cybersecurity so that employees can work just as securely from home as they do at the office. Their recommendations are meant to help ward off hacker attacks and enable companies to maintain business continuity. These tips range from switching off voice-controlled devices and covering webcams to not mixing personal and business use of devices. All recommendations have been published on the Charter of Trust website: bit.ly/39BB8Gv.
- Cooperation agreement on using “green hydrogen” and promoting sector coupling
- Joint projects for the conversion of power plants
- Share of “green gas” to be gradually increased
Today,
Uniper and Siemens Gas and Power signed a cooperation agreement for the
development of projects on the decarbonization of power generation and
promoting sector coupling. It extends the long-standing partnership between the
two companies. It is important to look at the energy, mobility and industry
sectors together, because they all can and must contribute to reducing
greenhouse gases. One focus of the planned cooperation is the production and
use of “green hydrogen” – in other words, hydrogen from renewable energy
sources. The companies intend to implement projects in this field together,
addressing the entire value chain.
At the Munich Security Conference 2018, Siemens and eight partners from industry signed the first joint charter for greater cybersecurity. Initiated by Siemens, the Charter of Trust calls for binding rules and standards to build trust in cybersecurity and further advance digitalization. Since 2018, the Charter of Trust has grown to 16 members. In addition to Siemens and the Munich Security Conference, the signatories include AES, Airbus, Allianz, Atos, Cisco, Daimler, Dell Technologies, Deutsche Telekom, IBM, NXP, SGS, Total and TÜV Süd.
In addition, the German Federal Office for Information Security, the CCN National Cryptologic Center of Spain and the Graz University of Technology in Austria have joined the charter as associate members. On February 19, 2019, Mitsubishi Heavy Industries (MHI) signed a letter of intent to join the Charter of Trust for cybersecurity in Tokyo, expanding the Charter’s reach into Asia. The company’s membership is expected to be finalized by the end of September 2019. MHI will be the first Asian company to join the global cybersecurity initiative.
- New Sinec software family offers a range of functions for efficient network management
- Quick and easy initialization of Scalance and Ruggedcom network components with Sinec PNI commissioning tool
- Central network services at a glance with Sinec INS
- New version V1.0 SP1 of Sinec NMS can also be used to manage security-related areas in the network
With the new Sinec software family, Siemens offers a range of functions in the field of network management. The Sinec software family meets the diverse requirements of a modern industrial network and helps users to overcome the challenges of digitalization, such as the ever-growing number of network devices as well as the security and clarity of increasingly complex networks. Alongside the Sinec NMS Network Management System, two additional Sinec tools – Sinec INS and Sinec PNI – offer even more options for comprehensive network management.