- Pipelines 4.0 is an integrated approach to the engineering, supply and life cycle optimization of pipeline assets
- The solution builds upon Siemens' extensive pipeline experience, product breadth and expertise in rotating equipment, electrification, automation and digitalization
- Key features include equipment and turnkey packages for pipeline stations, as well as data analytics, life cycle service and cyber security
Siemens has launched Pipelines 4.0, an integrated approach to the engineering, supply and life cycle optimization of pipeline assets, tailored to meet the evolving needs of North American operators. The solution combines equipment and turnkey packages for pipeline stations with data analytics, life cycle service and cyber security, building on the company's extensive pipeline experience, product breadth and domain expertise in rotating equipment, electrification, automation and digitalization.
- New power plant projects in Misrata and Tripoli West
- Contracts volume, including long-term service, in the range of 700 million euros
Siemens has signed contracts with the state-owned utility General Electricity Company of Libya (GECOL) to expand Libya’s power generation capacity by approximately 1.3 gigawatts (GW). Under these contracts Siemens will build a 650 MW open cycle power plant in Misrata, equipped with two F-class gas turbines, and a 690 MW open cycle power plant in Tripoli West, equipped with four E class gas turbines. The total volume of EPC contracts, including long-term service agreements, is in the range of 700 million euros.
- Siemens will supply four 400 kV HVDC transformers for cross-channel link
- Efficient 2,000 MW power transmission link between France and the UK will supply up to 3 million homes with electricity
Siemens will deliver four transformers, each with a capacity of 400 kilovolts (kV) and 315 megavolt amperes (MVA), on behalf of the British grid operator National Grid. The grid operator will replace the old transformers in the high-voltage direct-current (HVDC) cross-channel link. The new transformers are quieter, have lower transmission losses and will significantly improve the system's reliability. The HVDC link connects France and England and makes it possible to efficiently exchange energy in both directions. The order includes the supply, installation and commissioning of the transformers for the Sellindge converter station in England. Siemens will complete the work by mid-2019.
The regular election of seven shareholder representatives on the Supervisory Board of Siemens AG will be held at the company's Annual Shareholders' Meeting on January 31, 2018. The current Supervisory Board has decided – based on the recommendations of its Nominating Committee ‒ to propose the election of four new shareholder representatives:
Siemens has received an order from the regional grid operator EWE Netz GmbH to supply the key components of a Siharbor shore power supply system in Cuxhaven. The order includes the complete transformer station as well as the cable feed system for ro-ro (roll-on/roll-off) ships. The plant owner will be the northern German Gesellschaft für Hafeninfrastruktur Niedersachsen Ports (NPorts). With a power output of 630 kilowatts (kW), the plant will supply these ships with electricity during their lay time. They will thus be able to turn off their diesel generators, significantly lowering exhaust gas and noise pollution. The berth is located next to the new factory for wind turbines operated by Siemens Gamesa, which will be the plant's main user in the future. Siemens Gamesa will ship wind turbine components to its sister factory in Hull, UK. The Siharbor system is expected to go into operation by April 2018.
- Upgraded plants will provide safe, reliable electricity to three million people
- Plants will increase power output by over 400 MW
- Project supports Ministry of Electricity's goal to meet energy demands
In a move to help enhance Iraq's energy supply, Siemens announced today the signing of multi-million euro service contracts with the country's Ministry of Electricity. The project will see the maintenance and upgrade services of seven power generating units inside four power plants located in the areas of South Basra, Salah El Deen, Middle Region and Middle Euphrates.
- Simit Unit Administration integrated into the Simit user interface
- Simplified configuration of PLCSIM advanced coupling
- Bulk engineering using Chem Basic Library spreadsheet calculation – for chemical and pharmaceutical plant simulation
- Data transmission now also via OPC UA client coupling
Siemens has upgraded its Simit simulation platform for virtual commissioning and operator training with a new release. Version 9.1 enables Simit to also be used for virtual commissioning and operator training in modular plants, speeding up actual commissioning by as much as 60 percent and reducing unwanted standstill periods to a minimum, particularly during plant conversion and migration processes. Simit can also be used to implement a realistic operator training system. Version 9.1 comes with an array of innovations designed to improve operating convenience, support simulation modeling and contribute towards improved efficiency, openness and flexibility.
Siemens has received a contract to expand the Genelba gas-fired power station in Argentina. Working with its Argentine partner Techint, it will expand the power station for the end customer, Pampa Energía S.A. The project, known as Genelba Plus, involves converting the existing power station in Marcos Paz, Buenos Aires Province, into a combined cycle power plant. The expansion will increase the plant's electrical capacity from 168 to around 364 megawatts. The plant is scheduled to be commissioned in mid-2019.