- Russian Railways orders 13 high-speed Velaro RUS trains
- Maintenance contract for 30 years
- Order volume worth around €1.1 billion
Russian Railways (RZD) has ordered 13 high-speed Velaro RUS trains from Siemens Mobility and Ural Locomotives, a joint venture of the Sinara Group and Siemens AG. The order has a volume of around €1.1 billion. The contract also includes maintenance of the trains for a period of 30 years. RZD originally ordered eight Velaro trainsets from Siemens Mobility in 2006 and placed a follow-up order for an additional eight trains in 2011.
- Oregon’s largest regional transit provider
- Majority of project will take place in Clackamas, OR
- Enhances value sustainably over lifecycle
Siemens Mobility has won a mid-life overhaul service contract for TriMet’s Type-2 and Type-3 Light Rail Vehicle (LRV) fleet, which is made up of 79 Siemens Mobility SD660 LRVs. The project order has a volume of approximately €80 million with options for up to €25 million more. The initial project will be complete in 2025.
- Fully integrated electric-drive centrifugal compression configuration will significantly reduce footprint, capital, and operating costs
- Project marks this Delaware Basin gas plant customer's first order with Siemens
Siemens was recently awarded a contract to provide three residue compression trains for two, 250 million (500 million total) standard cubic feet per day (MMSCFD) cryogenic gas plants in the Delaware Basin. The customer, a key producer in the region and long-term user of reciprocating compression equipment, recognized the benefits of centrifugal compression and looked to Siemens for a fully integrated, turnkey solution that includes compressors, motors, variable frequency drives, and associated process equipment.
- Replacement of gas turbine from another OEM with an SGT-800
- Installation of a SIESTART battery storage solution for blackstart capability
- Customized solution requires comprehensive engineering expertise
Siemens has received an order from BASF Schwarzheide GmbH, a wholly owned subsidiary of BASF SE, to modernize the industrial power plant in Schwarzheide, Germany with key components. The Brownfield Exchange project involves replacing a gas turbine from another original equipment manufacturer (OEM) with a new, highly efficient industrial gas turbine from Siemens as well as servicing this machine for a period of 15 years. In addition, Siemens will install a SIESTART battery storage solution that will enable the entire power plant to start up independently of an external power supply.
- Sinamics Intelligent Operator Panel IOP-2 supports local operation, monitoring, setup, diagnostics and service of all Sinamics G series converters
- IOP-2 also includes applications and functions for advanced setup of the Sinamics G120X
Siemens is extending the functionality of the proven Sinamics IOP-2 for Sinamics G series converters to include the FW V2.3 SP1 firmware update. This improves local setup, operation, monitoring, diagnostics and service of all Sinamics G series converters. The FW V2.3 SP1 update also provides users with the additional benefit of transferring special application functions into the project menu. These application functions are then easily accessible from a list which simplifies the setup of the selected functions using the Quick Start or Advanced Startup options. As a result, users can run their applications without requiring any specialist knowledge of the operating parameters.
- Introducing Cerberus Portal, cloud-based online fire protection software to monitor fire systems.
- Fire panel data is transferred to the cloud via the Cerberus Connect X300 gateway using encrypted transmission technology and a built-in firewall.
- In case of system incidents, maintenance personnel receives real-time information to react promptly, inform customers and prepare site visits.
Cerberus Portal is the first stepping stone in digitalizing Siemens fire safety products. It represents the initial component of the new Cerberus Cloud Apps offering. This is a clear push towards the current fire protection industry trend: "There is an ongoing disruptive revolution in our Fire Safety industry. That revolution is called digitalization. I am deeply convinced that digitalization will change the way we do business," says Johannes Mario Kahlert, Head of Fire Safety at Siemens Smart Infrastructure.
- Siemens presents a new CNC for woodworking machines at the Ligna
- Sinumerik MC is the open CNC for customized processing machines
At the Ligna Woodworking Trade Fair 2019, Siemens is showcasing the Sinumerik MC control as a universal, open CNC system. Its optimized motion control, high-performance automation and the integrated Windows 10 operating system make it the ideal control, especially for wood, glass and stone cutting machines. With its open operating concept, the control system is also suitable for additive manufacturing, adhesive application, plate cutting, straightforward grinding, and laser or water jet cutting.
- Innovative woodworking control system
- Digitalization boosts productivity and flexibility
Under the banner "Digital Enterprise – Thinking industry further", Siemens is showcasing an extensive portfolio of innovative control and automation solutions for digitalizing the entire value chain in the woodworking and wood processing industry at the Ligna 2019 in Hannover from May 27-31, 2019 in Hall 16 at Booth C14.