Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release28 May 2019Smart InfrastructureZug
Fire protection connected to the cloud

Cerberus Portal is a cloud-based online fire protection software to monitor fire systems

Cerberus Portal is a cloud-based online fire protection software to monitor fire systems
As a cloud application, Cerberus Portal can be used from any online device – PCs, laptops and tablets running on any operating system. This allows all fire control panel information, such as faults, alarms and general system status, to be accessed remotely. A simple user interface and a clear overview of all connected sites draw the operator's focus to what is really important: have the fire protection system up and running at all times. Cerberus Portal is particularly useful in case of an incident because the real-time data can be examined in detail before dispatching service technicians. Because they know about the issue in advance, they are well prepared and have the necessary information, tools and equipment when they arrive on site. Cerberus Portal is an online application, so system operators do not need to worry about updates. This leaves them free to fully focus on providing their customers with the best service possible.
The Cerberus Connect X300 gateway makes sure all relevant data is delivered to Cerberus Portal in real time. Leveraging the power of edge computing technology, data is preprocessed locally on the gateway before it is sent to the cloud. Not only can this multi-protocol gateway be connected to both Siemens and third-party building products, it is also easy to install and commission. Encrypted transmission technology and a built-in firewall ensure the highest level of security.
Cerberus Portal and Cerberus Connect X300 are compatible with Cerberus PRO networkable panels (FC722, FC723, FC724, FC726).
Over time, more Cerberus Cloud Apps will be released to further assist maintenance companies. The Cerberus Test mobile application and Cerberus Tunnel are two examples intended to support service providers. Cerberus Test helps reduce manual effort during periodic maintenance by displaying tested detectors in real time on a smartphone. As a result, detector testing becomes more efficient and, according to initial estimates, up to 40 percent faster. With Cerberus Tunnel, a virtual version of the fire control panel can be displayed on a remote monitor via a secure connection. In combination with other tools, fire technicians will be able to remotely set and change panel configurations. The use of Cerberus Tunnel is restricted to what is legally allowed in each country.
The digitalization of fire protection systems and related maintenance activities allows service providers to save time and travel expenses. It is estimated that Cerberus Cloud Apps will enable maintenance companies to take care of up to 10 percent more customers with the same number of staff members.
Johannes Mario Kahlert adds: "Adding this new technology to our product portfolio will open doors to create new remote services, increase our customer satisfaction rate and imagine new innovative applications such as predictive maintenance. With Cerberus Portal and upcoming software products, Siemens Fire Safety is set to become a leader in the digital revolution."
For further information on Siemens Smart Infrastructure, please see
www.siemens.com/smart-infrastructure
www.siemens.com/smart-infrastructure
For further information on Cerberus Portal, please see
https://new.siemens.com/global/en/products/buildings/fire-safety/cloud/cerberus-portal.html
Siemens Smart Infrastructure (SI) is shaping the market for intelligent, adaptive infrastructure for today and the future. It addresses the pressing challenges of urbanization and climate change by connecting energy systems, buildings and industries. SI provides customers with a comprehensive end-to-end portfolio from a single source – with products, systems, solutions and services from the point of power generation all the way to consumption. With an increasingly digitalized ecosystem, it helps customers thrive and communities progress while contributing toward protecting the planet. SI creates environments that care. Siemens Smart Infrastructure has its global headquarters in Zug, Switzerland, and has around 71,000 employees worldwide.
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 170 years. The company is active around the globe, focusing on the areas of power generation and distribution, intelligent infrastructure for buildings and distributed energy systems, and automation and digitalization in the process and manufacturing industries. Through the separately managed company Siemens Mobility, a leading supplier of smart mobility solutions for rail and road transport, Siemens is shaping the world market for passenger and freight services. Due to its majority stakes in the publicly listed companies Siemens Healthineers AG and Siemens Gamesa Renewable Energy, Siemens is also a world-leading supplier of medical technology and digital healthcare services as well as environmentally friendly solutions for onshore and offshore wind power generation. In fiscal 2018, which ended on September 30, 2018, Siemens generated revenue of €83.0 billion and net income of €6.1 billion. At the end of September 2018, the company had around 379,000 employees worldwide. Further information is available on the Internet at
www.siemens.com.
Contact
Aynur Saltik
Siemens AG
1000 Deerfield Parkway
IL 60089-4513 Buffalo Grove
USA
IL 60089-4513 Buffalo Grove
USA
+1 (312) 560-3679