- Navigator combines distinct types of asset and maintenance data with performance data
- Deep analysis as the basis for new and improved Energy and Asset Performance Services
- Extended possibilities for apps and dashboards through integration into MindSphere, the cloud-based, open IoT operating system from Siemens
Navigator, the cloud-based energy and asset management platform from Siemens, has recently become even stronger thanks to a new release issued this February. With this latest version, it can aggregate a wider range of data sets, more powerfully analyze data, and create a whole new range of customized reports for easier decision making and communication. "Since we brought Navigator to the market in 2012, it has been evolving constantly to help our customers make better decisions, reduce operational expenditures, achieve sustainability targets and lower their exposure to risk. For example, Building Technologies saved 10,96 million tons CO2emissions in 2018, which corresponds to the emission of one million small cars, which are all driving once around the world." says Eike Steffen, Global Head, Solutions and Services Portfolio. Currently, Navigator processes over 625 million values per day from over 80,000 connected buildings worldwide.
The Umm Al Houl combined cycle power plant in Qatar has been inaugurated by Siemens, delivering almost a quarter of the country's installed power generating capacity and providing up to 136 million imperial gallons of drinking water per day. It is the second-largest power plant in the country.
- Strategic Partnership Agreement signed
- Technology collaboration agreement in heavy-duty gas turbines
Siemens AG and State Power Investment Corporation Limited (SPIC) signed a comprehensive Strategic Partnership Framework Agreement (SPFA). This follows a Technology Collaboration agreement on heavy-duty gas turbines between Siemens AG and China United Heavy-duty Gas Turbine Company (UGTC). The SPFA was signed by Qian Zhimin, Chairman of SPIC and Joe Kaeser, President and Chief Executive Officer of Siemens AG on March 26, 2019 in Beijing. The SPFA will further expand the cooperation in power generation in addition to the earlier agreed technology collaboration between Siemens AG and UGTC and will create a China-based supplier eco-system. Both companies will also collaborate in high-technology product demonstration e.g. in the field of digitalization of power plants or in hydrogen utilization projects and smart energy management for a decentralized energy system. Furthermore, both parties agreed to cooperate in project execution, and will jointly develop proper Gas-to-Power projects worldwide.
- Many companies and institutes from the University of Stuttgart are already participating in the "Fast Ramp-Up Challenge".
- Additional companies can join the initiative until May 23.
- Ramp-up of prototypes within only two days planned at the ARENA2036 innovation factory
- Open, cloud-based IoT operating system MindSphere in action
Siemens has launched an initiative to enable fast ramp-up and reconfiguration of production facilities together with partner companies from the mechanical engineering, automotive, robotics and information technology industries. Companies can still register and present their proposals on May 23. Prototypes will be tested at the ARENA2036 innovation factory in mid-October. As part of the "Fast Ramp-Up Challenge" competition, production cells from several companies are to be set up within just two days using MindSphere, the open cloud-based operating system for the Internet of Things (IoT) from Siemens.
- 23 Desiro HC trainsets
- Order worth around €300 million
- Service on the regional lines RE1, RE8 and RB17 in the Elbe-Spree network
- Option to increase capacity of the RE1 trains following platform extensions
- Attractive passenger experience and significant capacity increase
Ostdeutsche Eisenbahn GmbH (ODEG) has ordered 23 Desiro HC regional trains from Siemens for service on the Elbe-Spree network. The order is worth around €300 million. The multiple-unit trains are planned to be used on the regional lines RE1, RE8 and RB17 in the new Elbe-Spree network. In January 2019, ODEG was awarded the contract to operate these lines following a Europe-wide tender by Verkehrsverbund Berlin-Brandenburg (VBB). The contract includes the option to expand the capacity of the RE1 trains when the station platforms along this line are extended. Delivery of the 21 six-car and two four-car trains is scheduled to begin in the summer of 2022. The start of operations is planned for the timetable change in December 2022. The trains will be built at the Siemens plant in Krefeld, Germany.
- Higher reading rates and reading reliability
- Additional Gigabit Ethernet interface for diagnostic and service purposes
- Easy connection to cloud applications via Simatic S7-1500 and CP 1545-1
- Powerful, flexible accessories and easy handling
Siemens has introduced the Simatic MV550, the second optical reader in its new high-end Simatic MV500 series. The device is characterized by higher computing power, which allows a fast reading process and increased reading reliability – even under difficult conditions. It has an additional Gigabit Ethernet interface for diagnostic and service purposes. The Simatic MV500 can be easily and securely connected to cloud applications. This enables users to optimize production processes and supply chains, and to increase the efficiency and quality of production, logistics and asset management.
- First new gas-fired power plant project in Afghanistan since the 1970s
- Electricity generation planned for summer 2019
Siemens has received the first order for its SGT-A45 mobile unit from Bayat Power, a company of the Bayat Group. A few months from now, a complete gas-fired power plant, centered around the SGT-A45 trailer-mounted unit, will begin to provide electricity for the Jowzjan Province in northern Afghanistan. The mobile solution utilizes an aeroderivative gas turbine, which can provide capacity of up to 41 Megawatts (MW) of power at 50 Hertz (Hz). The SGT-A45 mobile unit is fully tested and pre-commissioned in the factory, and its trailer-mounted design minimizes the amount of construction work required on site. As a result, the plant can begin producing electricity in only a few months and will be capable of supplying power for approximately 200,000 homes. As the first new gas-fired power plant project in Afghanistan since the 1970s, Bayat Power Phase 1 will supply clean and reliable electricity, a first step to energy independence for the country.
- New CP 1545-1 communications processor for use with Simatic S7 1500
- New Simatic CloudConnect 7 Industrial IoT Gateway for existing systems
- Event-driven communication reduces network load and costsStandardized MQTT protocol enables transmission to various cloud platforms
The Siemens CloudConnect portfolio simplifies data transfer within the IIoT (Industrial Internet of Things) to cloud-based solutions. To this end, Siemens is offering the new Simatic CP 1545-1 communications processor, designed for use with Simatic S7-1500 in modern automation environments. For the cloud connection of existing systems, Siemens is now also offering the new Simatic CloudConnect 7 Industrial IoT Gateway. With CloudConnect, it is even easier for users to benefit from cloud-based data analyses. They can enhance machine availability by evaluating data for predictive maintenance purposes, for example, or machine manufacturers can offer new marketing models such as pay-per-use.
- New firmware V5.2 for even easier operation of Sinamics S120 drive systems
- Integration of the web server with new, responsive design and no special commissioning tools for diagnostics, maintenance and servicing
- Parallel connection of Active Line Modules (ALM) provides an extended performance range for booksize versions
- Users benefit from increased rated power without additional chassis unit and energy exchange in the DC link
Siemens offers new features in the firmware and hardware for the Sinamics S120 drive system. Operation is made much easier in firmware V5.2 through the integration of the web server. The web server in version V5.2 has a new, responsive design, which reacts via standard web browsers regardless of the end device used (notebook, PC, tablet or smartphone). For commissioning typical diagnostics and maintenance functions or servicing, no special tools are required. The web pages are available in six standard languages and feature error indicators and warning messages including meaningful help texts and suggestions for possible solutions. Users can intuitively create, manage and delete parameter lists - even across axes - and can perform firmware updates and system restores with the old firmware version. Backups of parameter settings can be stored on the clients using the web server and browser, and reloaded in the Sinamics converter using the Restore function. In order to test functions that are subject to license, it is possible to activate a temporary trial mode. In addition, a complete overview of all functions that are subject to license is clearly displayed in the web server. For optimum display on any Internet-capable end device, the best browsers are Microsoft Edge, Mozilla Firefox, Google Chrome and Safari. Navigation is via menu or breadcrumbs.
- 61 Vectron MS locomotives
- Deliveries beginning in March 2020
Austrian Federal Railways (ÖBB) has ordered 61 Vectron MS locomotives from Siemens Mobility. With this order, ÖBB is calling a further option from the framework contract signed in January 2017 for the delivery of up to 200 Vectron locomotives. This now brings the total number of locomotives ordered to date to 108. The locomotives will be operated by the Rail Cargo Group, the freight division of ÖBB, and are planned for cross-border freight service in several European countries. The locomotives will be built at Siemens Mobility's factory in Munich-Allach, and deliveries will begin in March 2020.