The regular election of seven shareholder representatives on the Supervisory Board of Siemens AG will be held at the company's Annual Shareholders' Meeting on January 31, 2018. The current Supervisory Board has decided – based on the recommendations of its Nominating Committee ‒ to propose the election of four new shareholder representatives:
Siemens has received an order from the regional grid operator EWE Netz GmbH to supply the key components of a Siharbor shore power supply system in Cuxhaven. The order includes the complete transformer station as well as the cable feed system for ro-ro (roll-on/roll-off) ships. The plant owner will be the northern German Gesellschaft für Hafeninfrastruktur Niedersachsen Ports (NPorts). With a power output of 630 kilowatts (kW), the plant will supply these ships with electricity during their lay time. They will thus be able to turn off their diesel generators, significantly lowering exhaust gas and noise pollution. The berth is located next to the new factory for wind turbines operated by Siemens Gamesa, which will be the plant's main user in the future. Siemens Gamesa will ship wind turbine components to its sister factory in Hull, UK. The Siharbor system is expected to go into operation by April 2018.
- Upgraded plants will provide safe, reliable electricity to three million people
- Plants will increase power output by over 400 MW
- Project supports Ministry of Electricity's goal to meet energy demands
In a move to help enhance Iraq's energy supply, Siemens announced today the signing of multi-million euro service contracts with the country's Ministry of Electricity. The project will see the maintenance and upgrade services of seven power generating units inside four power plants located in the areas of South Basra, Salah El Deen, Middle Region and Middle Euphrates.
- Simit Unit Administration integrated into the Simit user interface
- Simplified configuration of PLCSIM advanced coupling
- Bulk engineering using Chem Basic Library spreadsheet calculation – for chemical and pharmaceutical plant simulation
- Data transmission now also via OPC UA client coupling
Siemens has upgraded its Simit simulation platform for virtual commissioning and operator training with a new release. Version 9.1 enables Simit to also be used for virtual commissioning and operator training in modular plants, speeding up actual commissioning by as much as 60 percent and reducing unwanted standstill periods to a minimum, particularly during plant conversion and migration processes. Simit can also be used to implement a realistic operator training system. Version 9.1 comes with an array of innovations designed to improve operating convenience, support simulation modeling and contribute towards improved efficiency, openness and flexibility.
Siemens AG is preparing to list its separately managed healthcare unit on the Prime Standard segment of the Frankfurt Stock Exchange's Regulated Market. This move, which the company's Supervisory Board approved at its meeting today, is planned for the first half of 2018. "For Siemens Healthineers, the public listing is the next logical step and the foundation for expanding our strong position as a leading global supplier of healthcare technology," said Michael Sen, Chairman of the Siemens Healthineers Supervisory Board and the member of Siemens' Managing Board responsible, among other things, for healthcare technology.
Siemens has received a contract to expand the Genelba gas-fired power station in Argentina. Working with its Argentine partner Techint, it will expand the power station for the end customer, Pampa Energía S.A. The project, known as Genelba Plus, involves converting the existing power station in Marcos Paz, Buenos Aires Province, into a combined cycle power plant. The expansion will increase the plant's electrical capacity from 168 to around 364 megawatts. The plant is scheduled to be commissioned in mid-2019.
- Stand-alone Safety Instrumented System for use in critical areas in process industries
- Customized solution for functional safety for small to medium-sized plant projects
- Pre-configured packages based on proven Simatic components
- Connection to any process control system via Modbus/TCP
The Simatic SIS compact system from Siemens offers a new, stand-alone and flexible Safety Instrumented System for use in critical areas in the process industry. The combination of hardware and software components provides safety functions based on proven automation technology. The Simatic SIS compact system allows easy design of dedicated safety systems, the so called Safety Instrumented Systems (SIS), for monitoring potentially hazardous processes in the process industry and for protecting people, the environment, and the process plant. SIS monitor these processes and automatically intervene as soon as a permissible operating range is exceeded, such as too high pressure or temperature; alternatively, they can notify operating personnel to intervene. This minimizes the risk of potentially hazardous conditions.
- Faster processor and more memory space for complex applications
- Increased connectivity
- Efficient refrigeration control with inbuilt electronic expansion valves drivers
With the new Climatix C600 models the Siemens Building Technologies Division is extending its range of controllers for heating, ventilation and air conditioning (HVAC). These are designed for complex applications comprising up to 8,000 objects, for example a ventilation with integrated chiller unit. The new model series includes easy cloud connection for digitalized services for applications like chillers, heat pumps, district heating stations, air handling units and roof top units. Original equipment manufacturers (OEMs) are thereby enabled to develop new business fields or to increase service efficiency.
- New MindSphere Version 3.0 on Amazon Web Services (AWS) provides access to Siemens APIs and AWS cloud services for faster development
- Simotics IQ: New IoT concept for motors
- New partnership financing service to boost the implementation of Industrie 4.0
- Study affirms annual productivity increase due to digitalization of up to 9.8 percent
Increasing demands by consumers for individual, high-quality products at favorable prices are posing new challenges for industrial enterprises which can only be resolved by digitalization. "With the Digital Enterprise portfolio, the technical conditions have been created for Industrie 4.0. To ensure successful implementation of Industrie 4.0, what we now need is an extended model for cooperative partnership based on mutual respect: Large-scale corporations supply platforms and components, medium-sized enterprises develop their own solutions and business models on this basis, and end customers integrate these into their digital value chain," explained Klaus Helmrich, Member of the Managing Board of Siemens AG at the SPS IPC Drives. Siemens will be showcasing a range of innovations at the show designed to shorten the time to market and to improve flexibility, efficiency and quality in the process and manufacturing industries. They range from the new Version 15 of the Engineering Framework TIA Portal through the IoT concept for motors Simotics IQ to the new Version 3.0 of the open cloud-based IoT operating system MindSphere. Siemens is also offering financing services such as pay-per-use models designed to simplify the implementation of digital solutions, aimed in particular at medium-sized enterprises.